DSO Nano firmware major update

APP ver 2.4 change vs. default firmware

  1. Bug fix: Can’t trigger in SINGLE mode
  2. Bug fix: Can’t continuously trigger in NORM mode
  3. Redraw screen while pressing run/stop button, clear unexpected pixels.
  4. Change SIGN mode name to SING
  5. Keep Highlight menu items while  switch between
  6. Move X. POS on divisions (25 point)  instead of points
  7. Optimized menu navigation, left/right to navigate counter-clockwise/clockwise, up/down to adjust
  8. Save parameter to internal flash instead of TF card
  9. Press OK to display/hide reference waveform
  10. Change color scheme
  11. Add Fit mode to automatically zoom to fit human view

LIB ver 2.2

1. New Seeed Stuido Logo

Download here: http://dsonano.googlecode.com/files/DSO%20Nano%20firmware%20v2.4%20.rar

Please let us know if there is any issue/inputs for this new firmware, we will be checking forum timely. http://www.seeedstudio.com/forum/viewforum.php?f=12 Thanks for the suggestions from everybody!

About Author

2 thoughts on “DSO Nano firmware major update

  1. Is there a solution to upgrade on a non pc or a pc running on an AMD64? Just wondering if I have to find time at work, or if I can do this at home?

Comments are closed.

Calendar

August 2010
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031