DSO Quad Pre-Order available on monday

The 1st batch of DSO Quad are now on the way to their owners,  normally parcels will be delivered in coming 1 or 2 weeks. And here is another good news for our dear customers:  2nd batch of DSO Quad will be available for Pre-Order on next monday, and this time you don’t need to wait 3 months, we will ship them on May 15Th.

Pre-order from here: http://www.seeedstudio.com/depot/preorder-dso-quad-beta-test-p-736.html?cPath=174

About Author

17 thoughts on “DSO Quad Pre-Order available on monday

  1. SeeedStudio needs to do a better job on the manual (ver 91B). The calibration section is unclear, leaves too much guessing required. No place in the calibration section does it mention the three fields. It reads like there is only one. I got my unit over a week ago and still haven’t gotten it calibrated, indeed I think I messed up the original calibration GUESSING.

  2. I got mine last week. It came with 2 probes and a battery. It did not come with a USB connection for programming-recharging. It did not come with instructions-operator manual- user manual or any information… Like changing the input from DC to AC….if you can make channel 1&2 X-Y axis etc…
    No information IS disappointing.
    On the positive side.. there is a coupon for a “free probe only”

  3. Anybody know where to download the DSO QUAD User Manual? Got mine yesturday, but no user manual. And there are lots of questions.. Unanswered.

    How do we calibrate the scope probes?

  4. Hi!

    Nice, I really want one, but first 2 questions:
    -This ones comes also with the coupon to get the extra probe?
    -This “beta” is identically to the one in ebay? (~220 usd aprox) or the one in ebay is the final release?

  5. It’s the same version to the first one, no hardware change.


    Hypoon:

    Hey guys, what version of the product is this that is going up for pre-order again today? Would you consider this batch an “alpha”, “beta”, or “release”? I’m very interested in the final product, but I’d rather wait than buy something that might have hardware bugs. Thanks!

    UN:F [1.9.6_1107]
    Rating: 0 (from 0 votes)
  6. Hey guys, what version of the product is this that is going up for pre-order again today? Would you consider this batch an “alpha”, “beta”, or “release”? I’m very interested in the final product, but I’d rather wait than buy something that might have hardware bugs. Thanks!

  7. Sorry John, Our project manager will contact you soon.


    John Goh:

    Dear Sir/Mdm,

    I have e-mailed you 3 times with the following and have yet to receive a reply, it seems this blog site gets more responses than via e-mail so i am posting the following here. (if i still do not receive a response i will have to resort to calling you via phone till i do)

    I have waiting for months now for the “EasyDriver stepper motor driver V4.4 (assembled)” to be sold on your site, every time i e-mail in to check on the status of it, i am given an answer or “a few more days” or “next week” which will never be accurate, so i will simply like to know “WHEN EXACTLY WILL THE EasyDriver stepper motor driver V4.4 (assembled) BE AVAILABLE FOR SALE ON YOUR SITE?”

    Note: Pls do not ask me to buy the V3 version that is current being sold as the V4.4 is very different and i need the V4.4 only, thanks

    Yours Truly,
    John Goh

    UN:F [1.9.6_1107]
    Rating: 0 (from 0 votes)
  8. Dear Sir/Mdm,

    I have e-mailed you 3 times with the following and have yet to receive a reply, it seems this blog site gets more responses than via e-mail so i am posting the following here. (if i still do not receive a response i will have to resort to calling you via phone till i do)

    I have waiting for months now for the “EasyDriver stepper motor driver V4.4 (assembled)” to be sold on your site, every time i e-mail in to check on the status of it, i am given an answer or “a few more days” or “next week” which will never be accurate, so i will simply like to know “WHEN EXACTLY WILL THE EasyDriver stepper motor driver V4.4 (assembled) BE AVAILABLE FOR SALE ON YOUR SITE?”

    Note: Pls do not ask me to buy the V3 version that is current being sold as the V4.4 is very different and i need the V4.4 only, thanks

    Yours Truly,
    John Goh

  9. Pre-order 2nd wave will start on 18th.


    Montspy:

    I wanted to buy one but it’s out of stock, when would it be availible ?
    Montspy.
    VA:F [1.9.6_1107]Rating: 0 (from 0 votes)

  10. The probe is not compatible with Quad. You should be able to find a coupon code sticked on the box, you can get your free probe when we have them.


    air_variable:

    I live in Japan. DSO quad reached from Singapore today. Thank you.
    There is one question. one of digital probe was in the catalog on your site.
    http://bit.ly/gkULuZ
    but, it was not contain in the parcel. How should I do?
    VA:F [1.9.6_1107]Rating: 0 (from 0 votes)

  11. Does that mean Monday the 18th? Or Monday the 25th?

    Have there been any revisions on the boards between the two batches?

    pix

  12. But the product is still at beta stage, isn’t it?
    How many probes will be included in the second batch?
    What about the final price for this batch? Will it be $199.00?

Comments are closed.

Calendar

April 2011
M T W T F S S
 123
45678910
11121314151617
18192021222324
252627282930