Minibloq graphical programming environment is in Beta

image

The first Minibloq Beta version was finally released and ready for you to test!

 

We introduced the software back in May of this year, when Julián da Silva was starting a Kickstarter campaign to fund the project. Basically, Minibloq is a graphical programming environment for Arduino or other types of hardware device, such as DuinoBot or Maple. The goal is to lower the entrance of playing open hardware and bring Arduino and other platforms closer to primary schools, kids and beginners.

 

Congrats to Julián! Great idea and has almost half year hard working, the current Beta version came out with many new features and a lot of programming “blocks” beyond that was in the early stage of development. Here’s the link to Minibloq page, do check it out if you also interested in this idea.

About Author

Calendar

October 2011
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930
31