#Pebble power up guide 2nd – the initial design

We’d like to introduce the initial design we will put on xadow & pebble. before we dive into this section, let’s come back and review the concept design last time.

DSC_2855-001

This cool self replication sketch is one of the result of our brain storm.

  • pro: every brink is the same, easy to assemble
  • con: the free space between each piece is limited

DSC_2854-001

A workaround way design the shell rather than the brick itself, we place a two-brick length shell wrap up the bricks, the opposite shell will be shift by one brick to make the structure stable.

  • pro: neat
  • con: it’s impossible in practical

DSC_2852-001

We find our idea in our daily life. The connector of the loose-leaf binder inspired us, this is relatively traditional design. The following design is also so common: the zipper! It’s too much beyond our imagination, isn’t it?

DSC_2851-001

There are 3 designs in this one. The left one comes from the average watch design. The middle upper one is fastened to a surface where is connected. The right one cleverly uses a silicone parts connecting them.

DSC_2853-001

After several iterations, The “工” like connector is replaced with a “I” like, which makes more space for flexible uses.

DSC_2876

What we learn from the wearable design iteration? What is our next step? Just keep an eye on our series blog next time.

About Author

Calendar

March 2015
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031