Announcing Winners of Best Wio Project Idea Contest

Today we are announcing the result of Best Wio Project Idea Contest. In total we have received 14 entries. Most of them are Kickstarter backers who cannot wait to tinker with Wio Link once received the pledge. Below are the winners and their project idea share on Wio Forum. Actually some idea already made their own working prototyping. It was a big learning curve for some community member. We’d appreciate other member who contributed their idea to help out.  So check it the projects and if you find any interesting idea you could make it together. 

GOLD IDEA

#idea Thermostat – Final by philip.mallon

Philip had a thermostat program hosted on Beagleboard Green (BBG) with a Wio Link front end.The Wio Link is connected to a Grove Temperature and Humidly Sensor and a Grove LED. The BBG is connected to a Orvibo S20 wifi power switch that switches on when the temperature is more than 22 degC and switches off it it gets below 21 degC. He also made a node-red program on a Beaglebones Green (BBG) computer using a Debian OS.

Node-red04

SILVER IDEAS

#Idea: Industrial Garage Door Opener by  Tyler

He took some Ethernet cable and ran from the door switch into the officen and wired it up to mimic the wiring of the door switch.Then he used Relay via Wio Link to control the switch.  He even make an mobile APP to control by following Youtube video of MIT App Inventor 2.

572a7b610947a572a7b82544bc

 

 

 

 

 

 

 

 

 

 

 

 

 

#idea Weather station with LED temp without coding by markjoyner 

He monitored all of the parameters of temp & humi sensor, barometer, air quality sensors and stored the information in Initial state to see nice historical graph of the sensors. Beside, he also displayed the current temperature on the 4 digit LED display by creating a IFTTT recipe.

INI

 

BRONZE IDEAS

[idea] Garage parking assistance by uwe.fetzer 

Uwe used various Grove modules such as ultrasonic ranger, speaker and LED strip for prototyping and a Raspberry Pi as Wio Server, even shared Python script and a demo video to showcase.

 

#idea Greenhouse aquaponics monitor/controller by drstoneburg 

Drstoneburg’s idea is to build a green house aquaponics fully equipped with smart electronics, such as Fish tank monitor, plant bed monitor/controller, ambient air monitor and smart evaporative cooler.

 

#idea OpenTempescope by wassabi.time 

Tempescope is a physical display that recreates the weather forecasted inside a box. Wio-Link can use IFTTT to set up triggers on the weather for a given day. Then turn on and off relays to the 12V water pump and mist generator. Lastly, animate some RGB lamps for sunrise, lightning.

 

About Author

Calendar

May 2016
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031