Is this APP_G251 version based on pmos69 APP_G251 version with a new GUI?
DrV, I hope you won’t be disappointed too early. It has nice maybe interface, but it cannot be used for serious measurements. Actually, it doesn’t implement more than 10% functions as the original firmware. Currently I am finishing the calibration UI and I hope, in one-two months I will start implementing the rest of the UI.
glt, no, this firmware is written from a scratch and has only a little in common with the pmos62-es firmware. We just use the same build script that produces same named hex file.
alys, I really like your idea of connecting the generator to the input through a capacitor for obtaining the negative voltages. You should maybe buy this oscilloscope and help me developing it
gabonator1, not me but my colleague was dissapointed with the new release haha. It is obvious you are focusing in the interface, just the opposite from the “comunity” package. If both your interface and the functionality of the comunity release merged into a single app…
Just have in mind the title for this thread DS203 quad user interface design, for now I am expecting nothing else than a nice interface.
I like the menu layout, selecting the mode in the first tab, settings, etc. The original release is not practical for me, I really dont need to switch over ALL the options to reach one…
Just let us know how we can help you in the development of the app
Cheers.
Hello,
I have finally finished some basic calibration module and I would really appreciate it, if you would try it and give me some feedback.
Here are the instructions:
- We need to calibrate the DAC module at first, you will need some volt meter for that. Go to “User applications” menu, tab “Calib”
- Select the ADC button, here are two lines:
0.5V…0725
1.5V…2176
use the slider buttons to move between the four digit numbers. The first dac number (725) should correspond to the 0.5V voltage on wave out, and the second (2176) to 1.5V. Connect the volt meter to wave out and change the numbers to achieve the voltage as precisely as possible.
- Press the “Use values” button
- Save calib data
- Select “Analog” button
- Connect wave out to CH1 input
- Start calibration (CH1 200mV range) (it will take about 3 minutes)
- Save calib data
- Analog -> Get info and post me your results, in my case it looks like that:
Calibration data CH1: 200mV
Q0: -20 -> 46900 (-22.9)
Q1: 280 -> -774080 (377.968)
K0: -20 -> 2905 (1.418)
K1: 15 -> 2900 (1.416)
K2: 75 -> 2905 (1.418)
K3: 90 -> 2910 (1.420)
K4: 245 -> 2920 (1.425)
K5: 280 -> 2900 (1.416)
Check the calibration in oscilloscope view and for precise measurements you can use the voltmeter application (User applications->meter)
the oscilloscope calibration depends on the level of battery charge
Gabriel,
Good job on the work so far. Am I correct in thinking that a bunch of the functions are not coded yet, so it’s a GUI development ontop of a basic scope right now? It would be great to get some of this GUI merged with the community App project.
I recently bought another DS203, sourced in the UK from a Chinese importer, and it’s come with a new firmware, App (plus A1) Version 1.00 running on Hardware version 2.60 with sys version 1.51. I was really hoping it was from this forum because the UI is super improved, but the core scope functions are much better with the community APP. I am posting some screen shots because they have taken a somewhat similar approach to you. I like some of your nice features but this new DSO is actually more consistant and easier to use. Please take this as constructive review.
For Example, in this new APP the right mouse key is always navigation, and the left mouse key is always chose and left press is always select. Triangle key always and only toggles between horizontal menu and vertical menu. So it’s very easy to move around.
You have the left key as horizontal and the right as vertical, which is fine, except when you move between the two, where it’s necessary to move the vertical selection until it rejoins the horizonal by going horizontal, at which point it stops working and you have to switch keys to go horizontal, then switch again to go horizontal on the vertical key into the new menu. Proposal: have the vertical menu remember it’s last selection, and have the horizontal always work not be disabled by the vertical menu. Result: the horizontal is always horizontal and vertical is always vertical, and it’s quicker to move around both. For example, move from trigger to dY cursors is 3 keys and 14 dabs on your scheme, but it could be just one horizontal dab.
Vertical menu contains most of the functions that were so difficult to get to in the old UI eg: cursor posistions. Now it’s easy: triangle toggle then mouse keys.
You have context menus which are great, as coded on the input page. Personally I’d have them toggle which I think is more expected action of buttons and frees up circle, or more usefully free up play/hold to do just that. I keep going into sub-menus when I want to exit. I’m assuming the scope display will remain when eg: cursor boxes substitutes for input boxes otherwise it would be impossible to set them. Because you use square to close menus, you have inconsistancy again. For example, I go into CH2 menu with Play, but I close it with Square. However if I go into the sub menu Resolution, I can close it with Play (the toggle on-off I keep trying), but then have to go back to Square to close the CH2 menu. If I try the Timebase menu I can have toggle-off. But if I go into the Functions tab and select say Spectrum analyser, I must use toggle off as nothing else has any effect.
The new DSO has measurement toggled on-off by circle, and a long hold enters the menu to change measurements, where, as before, left mouse is chose, left press is select channel and right mouse is vertical move as usual. However it’s still the old terse descriptions and poor colours, and it sits on the display so I can’r recommend it. Yours are easier to read, and I think will be easier to select off the context menus. As you are coding it, it seems that maths and cursors are mutually exclusive, so you might want to consider a footer displaying two or more cursor values (eg: t1, t2, delta-v). The new DSO has fixed them at dT and dV but it’s useful to have them on display along with eg: frequency.
In learning your keys I think I have captured around 38 bitmaps. Here’s a screenshot of the functions menu on the new DSO: all these file operations are in one place (square) and as before, right vertical mouse is vertical, left mouse is chose and left press is select, so it’s completely consistant again. I think you have yet to code in the menus so you might like to consider this extended menu approach.
For info, the new App also includes
- display record length change 4k-2k-1k-512-360
- Cute function out icons with Square wave duty and up to 8MHz, others to 20k
Hope this is of some help.
Cheers,
Mike
Mikey63: Thanks for the review and for posting the pics of the newest Chinese version of the DS203; it helped me confirm the version I bought and received a few months ago on eBay. Also wanted to add my +1 to the menus and encourage Gabriel to use the same or similar.
All: Since we’re discussing UI for the DS203, here’s my playlist on Youtube with some screen shots on the various versions of the DS203.
http://www.youtube.com/playlist?list=PLRUTSitNpxYcLQXyfJgFYCanWeD8X_150
Number 3 on the playlist that has some PAWN scripting language used on the DS203, might be useful?
http://www.youtube.com/watch?v=WwzGsEINN3o&feature=share&list=PLRUTSitNpxYcLQXyfJgFYCanWeD8X_150
Gabriel: Its been a few months since I downloaded your project, but I did successfully open it in my VS2010 Ultimate…I primarily use VS for WS and UI in VB; I’m a novice when it comes to C#. I don’t have a lot of free time but if I and my VS2010 can be of assistance let me know.
Stephen
Gabriel,
I do not understand!
Calibrating Adc - OK except that “Use values” instead of “Use labels”
Calibrating analog channel:
Ground calibration - OK for CH1 and CH2
Change coeficient do not work at all on both CH1 CH2
Vin = 1.4242V = const and do not changed with K changes.
What is wrong
I really want to try Gabonator’s app for my Quad, but whenever I try and load the APP_G251.hex file, it complains that there is not enough space, it needs about another 400kb (this app is about 1mb, as opposed to around 100kb for the old one I was using). I suspect it may be because I have that frequency analyzer in the fourth app slot, but as far as I can tell, there is no way to remove it. Any ideas?
Ignore my last post, I’m idiot. I’m not familiar with github, and the .hex file I got when right clicking on the link and saving it was…different…to what I needed. Working now. For those hunting around for the link: https://github.com/gabonator/DS203
Kabron, I am sorry, there was some minor bug in calibration and triggering code. It’s fixed now, tell me whether it worked for you.
Mikey63, thank you for your extensive review. I liked the option of original firmware which allows to reduce the number of samples to lower count (2k, 1k, 360 instead of 4k) which should improve the screen redraw times (important in timebase resolution greater than 1ms). I tried to work with latest BIOS code, which should implement this feature, but for some reason I was unable to get it working. Anyway, I solved this problem in another way. Regarding the keys - the function of circle and triangle buttons is now user assignable including trigger control.
ObservativeTiger: thank you for the youtube playlist, some features of JPA’s firmware (pawn programming) and new version of original firmware I like very much. But the sad thing is, I ran out of RAM, so now I will think how to reduce the memory requirements and probably it is good time to start fixing bugs At least I would like to implement FIR filtering with user defined filters and also the slow scrolling mode for low speed sampling.
Gabriel
Nothing changed with new FW.
May be SYS/FPGA versions could affect?
Mine have SYS 1.51 while on your screen shots it’s 1.50.
What is your version in About/Firmware screen?
It should be: 1.0 rev. 85
And built date shoud be 25.12.2012
Sorry, it is 1.0 rev.84 24-Dec-2012
In a moment I’ll upgrade it.
Gabriel! Now it’s OK.
Thanks a lot!
Please Help Me!
I have the 1.0 rev. 85 New version,
And built date shoud be 25.12.2012.
I Set channel color, Y sensitivity (V / div) and the X-sensitivity.
How do I save the settings, the next time they use it?
Thanks Gabonator for excellent Firmware!
Best regards …
tacsago, these settings are stored automatically every two minutes (only when the user has made some change, to prevent wearing out of the eeprom). Just wait at least two minutes before turning the device off…
Thank You for Help Gabonator!
Super!
Dear Gabonator!
I want to save the measurement in to File No. 1 after Load from File No. 1.
The DSO write to me “Sorry…Import failed!”
What is wrong? Save/Load function not finish? Please Help Me!
My Device Config.:
HW version: V.2.7
SYS version: 1.52
DFU version: V.3.11c
Firmware version: 1.0 rev. 85
Thank You for your Help!
When it says “Sorry… import failed”, that means the file is corrupted. Can you please upload it somewhere, so I can look inside it? Or try formatting the drive…