How to find the MAC address of Wifi Bee

wireless communication and related Bees.

How to find the MAC address of Wifi Bee

by Jacket Chen » Tue Jun 18, 2013 2:56 pm

Sometimes , the supplier has not posted the MAC address tag on the Wifi Bee , so you need do something to find it:

1 Download the library of Wifi Bee and decompress it into the Arduino-->library

2 Open the demo "WebServer" , and modify the program which include local_ip , gateway_ip , subnet_mask , ssid , security_type , security_passphrase.

3 Choose the right board and upload the program to the Wifi bee , and then wait the blue LED light up.

4 Open your web browser , input the local_ip you have modified in the program and enter. Then you can see:

Hello World!!I am WiShield


5 Open your PC command terminal(Window--Win+r , MAC--Terminal) and input the command

ping 192.168.168.100
Note: input the local_ip you have modified in the program and enter

6 If the wifi bee works well , you can type a new command

arp-a


And then you can see all terminals information connected to the router , you can find the IP and MAC address of Wifi Bee.(picture 1)

Good luck!
Attachments
1.png
1.png (153.66 KiB) Viewed 2422 times
Love little, love long.
User avatar
Junior-6
Junior-6
 
Posts: 665
Joined: Thu Jun 21, 2012 4:25 pm
Location: China

Re: How to find the MAC address of Wifi Bee

by yexiaobo » Sat Jun 22, 2013 10:34 am

In Mac OS X, you must instead of cmd.exe with Terminal.app.
Pre-kindergarten
Pre-kindergarten
 
Posts: 47
Joined: Tue Dec 11, 2012 10:53 am


Who is online
Users browsing this forum: No registered users and 1 guest