DSO Quadv2.6Manual released..Include the basic operation and upgrade methed. and firmware include :logo related file, FPGA logic file, App.hex and Sys.hex.
NOTE: firmware for HWv2.2 is not compatible with HWv2.6 . DO NOT upgrade HWv2.6 with firmware for HWv2.2Latest firmware available(2012/04/12):APP: 2.53
SYS: 1.52
FPGA: 2.61
logo: logo file , do not need to upgrade as you do not want to.
And, a new designer has joined to design the UI. The following firmware available:(2012/02/14) )APP:AP3_P100
please ref the wiki to track the latest firmware: http://garden.seeedstudio.com/index.php ... mware_ListFirmwares that needs to be installed into the DSO Quad:
1. CFG_FPGA.ADR + VxxxFPGA.bin. The two files for fpga logic, you need to install the .ADR file and then the .bin file.
2. logo_00B.ADR + logo_001.bin. the logo files, need to install the .ADR file and then the .bin file.
3. APP_Bxxx.hex, the app firmware.
4. SYS_Bxxx.hex, the sys firmware.
when you want to update you firmware, for example, you want to update the app firmware to v2.35 to corrrect the calibration error ,you just need to update the app ,to 2.35, as there is no update in the sys firmware.
you should do:
1. download the app 2.35 zip from below lines.
2.upzip the app, you would see app_B235.hex and DSO Quad Calibration .pdf.
3. connect the Quad to PC via USB , and power Quad with the ">||"pressed.
4.copy the App_B235 to the virtual disk . the virtual disk will auto reset and this file changes to :APP_B235.RDY.
5. Update finished. calibrate the Quad as the DSO Quad Calibration .pdf
updated issue:
1.sys1.34 and .app2.32 can be download now, Please upgrade your DSO QuadHWv2.6 ASAP (2011/4/19)
2.Manual 0.91B added(2011/4/22)
3.Manual to calibrate the probes added(2011/4/25)
4.App 2.33 added(2011/4/27)
5.App 2.35 added,the calibration error been corrected.(2011/5/16)
6.FPGA_V2.5 added(2011/5/18)
7.Manual 0.92B added(2011/5/30)
8.Sys1.37 added(2011/06/01)
9.App2.43 added(2011/06/07)
10.Sys1.41 added(2011/06/07)
11 App2.45 added(2011/06/16)
12 App2.45(b) added(2011/06/17)
13 App2.50 and Sys1.50 added(2011/07/11)
14 New UI ,just for testing!!(2011/07/22)
15 app252/sys151/fpga2.6 released..
16.AP3_P100 released, this is not a offical Version
17. APP2.53 and Sys1.52 released(2012/04/12)
| Attachments: |
SYS_B152.zip [21.03 KiB]
Downloaded 4865 times
|
File comment: Debug the FRQ, TH and TL in Menu.c and Funtion.c
APP_B253.zip [45.57 KiB]
Downloaded 4819 times
|
File comment: UI improvement.
AP3_P100.rar [48.99 KiB]
Downloaded 3913 times
|
File comment: fpga261 file, please first install the .ADR file , and then the .BIN file
FPGA261.zip [23.31 KiB]
Downloaded 5580 times
|
File comment: sys151, must be upgraded with the fpga261 file
SYS_B151.zip [20.95 KiB]
Downloaded 2899 times
|
File comment: App2.52. mush be upgraded with the fpga261 file.
AP1_B252.zip [32.27 KiB]
Downloaded 2730 times
|
File comment: New UI ,just for testing ...if you do not like something that is not finished yet , please do not try.
DS203 new firmware testing.rar [52.85 KiB]
Downloaded 1449 times
|
File comment: 1.Re-write the fat12 file system (FAT12.c,ASM.s) 2.Modified read/write flash functions(Memory.c, EXT_flash.c) you need to format the Quad disk after upgrading as http://www.seeedstudio.com/forum/viewtopic.php?f=22&t=2112
SYS_B150.zip [20.46 KiB]
Downloaded 2304 times
|
File comment: 1. re-write the file.c and asm.s based on the new fat32 file sys. 2. Modified the TH TL measure bugs in Menu.c 3.Optimize the measuring related functions (Menu.c ,Function.c,Calibrat.c) 4. Modified the bugs in triggering with pulse width. you need to format the Quad disk after upgrading as http://www.seeedstudio.com/forum/viewtopic.php?f=22&t=2112
APP_B250.zip [30.65 KiB]
Downloaded 2337 times
|
File comment: modifyed the bug in calibration channel B in app245
APP_V245(b).rar [35.74 KiB]
Downloaded 1539 times
|
File comment: 1. Modified the bug in saving the setting 2. Modified the bug in saving the calibration data
APP_V245.rar [35.74 KiB]
Downloaded 932 times
|
File comment: 1. Read/Write file system functions added(DOSFS.C) 2. Debug the bugs in read BUFF(DOSFS.C)
sys141.rar [22.83 KiB]
Downloaded 1405 times
|
File comment: 1. Auto calibration added(calibrat.c,process.c,function.c) 2.frequency and duty measure added(Process.c,Menu.c) 3. Function to export the data in .CSV added(Main.c,files.c Menu.c) 4.Must be used with SysV1.40 or above.
App_V243.rar [35.44 KiB]
Downloaded 1680 times
|
File comment: 1. debug the saving error that may led to a black screen in sys1.34 2. dubug the function to set the offset to CH_A and CH_B
SYS_B137.rar [18.26 KiB]
Downloaded 584 times
|
File comment: 1. how to calibrate the probe added. 2. how to calibrate the waveform added
DSO Quad v2 6 Manual 0.92b.rar [2.51 MiB]
Downloaded 11481 times
|
File comment: 1. function to set sample depth added. 2. function to set trigger delay added
FPGA_V2.5.zip [23.59 KiB]
Downloaded 1112 times
|
File comment: app 2.35, the calibration error been corrected.
App2.35 and Quad calibration.zip [33.36 KiB]
Downloaded 1033 times
|
APP2.33.zip [24.46 KiB]
Downloaded 803 times
|
How to adjust the C to calibrate the probes.zip [74.25 KiB]
Downloaded 2195 times
|
File comment: DSOQuadV2.6Manual0.91B
DSOQuadV2.6Manual0.91B.zip [2.57 MiB]
Downloaded 8774 times
|
File comment: SYS1.34 and APP2.32 , please upgrade all the files include FPGA file(2011/04/19)
SYS1.34 AND APP2.32.zip [63.14 KiB]
Downloaded 1001 times
|
File comment: module to save the waveform to .bmp file or .dat file
Save wave for DSOQuad.rar [4.06 KiB]
Downloaded 3543 times
|
File comment: QuadV2.6 hardware SCH
DS203V2 6_SCH.rar [62.06 KiB]
Downloaded 16481 times
|
File comment: .sys 1.31 and .app 2.30
Quad firmware.rar [58.65 KiB]
Downloaded 1567 times
|