Relay Shield V2.0

Hi,

I just bought the seeeduino relay shield v2.0 and on the wiki page i found this note “do not operate more than 35v DC” since i couldn’t find a proper specs, can anyone kindly explain if it is possible to switch 240v AC? I’m not sure whether the 35v is operating voltage or switching.

Thanks!

Hi, the relay shield V2.0 can switch up to 250VAC or 35VDC load.

Thank you for your kind reply :slight_smile:

if it is possible to switch 240v AC? I’m not sure whether the 35v is operating voltage or switching.