Mini Soldering iron review

Moderator: weijie.han

Mini Soldering iron review

by todd.krein » Thu Jun 23, 2016 10:40 am

I bought one of the mini soldering irons, to use as a travel iron, and thought I'd post a couple thoughts about it.

First off, I do like it. It's small, heats up quick quickly, and does a pretty good job.

The only problem that I have with it is that I want it (and it seems to be aimed) as a travel iron. Unfortunately, it's not as easy to carry as one might like. You need an Allen wrench to insert a/o remove the tip, and you'll definitely want to remove that tip before you pack it to avoid breaking the unit in half. Seeed is kind enough to provide the wrench and a spare screw, but no safe way to carry them. I'd suggest a pair of threaded holes to store the extra screws, and some way to insert the Allen wrench into the handle.

The bag that's given with the unit is a nice touch, but it's just a little too small to hold the handle, tips, power supply *and* power supply cord. That makes it rather useless. It only needs to be a little bit bigger...

so, four stars out of five. Keep it up!
Posts: 1
Joined: Thu Jun 23, 2016 10:33 am

Re: Mini Soldering iron review

by kavi » Tue Jun 28, 2016 7:23 pm


Thanks for your valuable suggestion.

Thanks and Regards,
SeeedStudio Technical Support Team
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Who is online
Users browsing this forum: No registered users and 2 guests