Hey Bob thanks for you feedback here quick answers:
ALT and + key or ALT and - key change the speed on the arduino. Maybe hold the keys longer to take effect. Maybe I should add some visual feedback on processing side as well.
I still had not any time to debug this. Although non working precompiles seems to be only a problem for snow leopard macs? Would be great if anyone can report success stories on other system, by now I don’t hav any other to test with.
well I do have all file in structure like the repository is. The top mtXcontrol folder is within my sktechfolder directory, set up in processing preferences. I open mtXcontrol.pde with processing, and firmware.pde with arduino IDE. works allright.
wow right, looks all okay for my. After step i) I would only add one more step: switch to ‘Arduino: Slave’ mode (alt + ENTER) or second button form top) which allows you to display your drawing in processing in realdtime on rainbowduino to test it.
If it’s ok I’ll add those steps to the documentation, with mention your name, of course.
A proper setup screencast is indeed a good idea. I’ll see if I have time. If you or sthoneelse is interested, feel free to go for it, of course!
Hm strange, I never saw this error before. Does other sketches compile well? try some ‘bigger’ examples usering libraries as well, maybe your library path isn’t correctly set up?
From what I gather, download the “firmware” zip… Drop raindbowduino into the libraries folder…
Create a directory in your Arduino sketches directory (windows it’s documents\arduino) Something like RainbowduinoMXControl. Rename firmware.pde to RainbowduinoMXControl.pde… Then fire up Arduino 17… Sketches > RainbowduinoMXControl … Upload that
He’s hardcoded the serial port (?!) so you need to download the mxcontrol software to your desktop. Throw all the files in a directory called “mtXcontrol”. Download and unzip processing somewhere and upload up mtXcontrol.pde within processing.
Click on the tab named Arduino and look for the lines
Arduino(PApplet app) {
try {
port = new Serial(app, Serial.list()[0], BAUD_RATE);
}
catch(Exception e) {
port = null;
}
standalone = true;
}
Change serial.list()[0] to what ever com port your using… on my machine it was “COM7” (in quotes). On 'nix it may be something like /dev/usb0
is there any chance you could write a simple Arduino to Raindbowduino demo on how your “protocol” works. I’m trying to decipher your code but there’s no comments and I’m not sure how your client and server code mesh up.
I’ve just updated the SOURCE (not the binaries yet) to have an autodetection for the Rainbowduino port (only tested on Mac OS X yet) and Bitmap save and loading support. I cleaned up the code a bit and prepared quite a lot for more color support in futur. So check it out and stay tuned!
Happy new Year to all of you!
Good news right from the beginning: I’ve just pushed a new version of mtXcontrol!
On big thing is support for Novation Launchpad, but maybe way more interesting bit for you is, I’ve move the complete rainbwoduino communication into a separate library which can include into your Processing programs easily. Check: http://rngtng.github.com/rainbowduino
It now follows a proper API (likely to change) with extended functionality, including handshake and ok/error response Codes. Now, you updating the Buffer, loading/saving from EEPROM, setting the brightness or pinging the device works like charm!
As of that mtXcontrol is now way more stable, autodetects your Rainbowduino, im/exports BMP files, improved color chooser and many more. Download the latets version here:
Ok long time no hear as I was quite busy lately. But I managed to drive my rainbowduino and mtXcontrol development forward supporting multiple devices. Not yet fully finished, but good for beta test. Get a (quite nerdy) sneak preview here:
g. Close the Arduino IDE. Load the latest Processing IDE (although similar in appearance, they are not the same). Remember to leave everything connected as displayed in the blog photo.
h. Load the mtXControl application and compile and run it. The display should go blank.
What exactly do I have to load and run on Processing ?
h. Load the mtXControl application and compile and run it. <- Is this mtXcontrol.exe file ?
I currently have the LED Matrix on White, it doesn’t go blank. I get the following message on mtXControl: “No output device found, running on standalone mode”. What to do ?
Thanks in adv.
I need help. I cant make it work, windows or mac. Im stuck at the all white LEDs pattern. Could anyone make a video or screen caps of the whole process ? Im clueless. I ran mtxcontrol on mac and nothing happens, only the icon shows up. I tried running the latest processing ide while running mtxcontrol, no luck. Do I have to run anything on processing before running mtxcontrol ? thank you in advance.
I can’t get the mtXcontrol to work with the Rainbowduino through my UartSB v2.2. I got the firmware upload to work, but mtXcontrol always says “Output device not found, running in standalone mode.” I started with my UartSB set to COM8 (default), then I tried COM1. The tutorials I’ve seen say to run something in Processing, but I can’t find that. I’m using the mtXcontrol.exe file instead, and it doesn’t work.
Anyone willing to help?
mike41325 and I are experiencing the same issue. We must be missing something, I don’t know what should be running on processing when mtxcontrol is running… or if there’s any… any help much appreciated.
Connect your rainbowduino in proper way to your computer that you can program it throgh COM.(Remember to change the port to use COM1)
Unzip Rainbow_mtX.zip to your arduino code directory (no need in the arduino library), open Rainbow_mtX.pde by arduino and program it to your rainbowduino.(If it compiles failed, there may be another rainbowduino class in your arduino library, so back up and remove it).
After programmed, the rainbow Matrix will be all in white.
4.Unzip mtXcontrol_windows.zip and run mtXcontrol.exe.
If ther’s error reported, like “not found javaw.exe”, then you need to add the java path to your environment variable(On my computer is: D:\Program Files\arduino-0018\java\bin ). Am I understood?
If there’s no error reported, just enjoy controlling your rainbow!
I got it to work, but certain actions (like loading from the matrix) will freeze the program and I have to force-quit the window. Anyone have a solution?
Got it working for the first time today ! It’s awesome ! Had some problems with the COM port and app is running a bit slow but it works great ! Good work!
I have 1 more question: how do I hook up a second rainbowduino so I can write whole words ? I have 2 rainbowduinos connected but can only control 1, the other one is still running another sketch. Do I have to upload the new firmware to it individually (unplug all, upload firmware, restart mtxcontrol) ?