Grove - EMG Detector

From Wiki 来自痴汉的爱
Jump to: navigation, search

中文

Emg product.png


Contents

Introduction

EMG detector is a bridge connects human body and electrical, the sensor gathers small muscle signal then process with 2th amplify and filter, the output signal can be recognized by Arduino. You can add this signal into your control system. Note: The sensor cannot be used for medical purposes.

In standby mode, the output voltage is 1.5V. When detect muscle active, the output signal rise up, the maximum voltage is 3.3V. You can use this sensor in 3.3V or 5V system.




Features

  • Grove Compatible
  • 3.5mm Connector
  • 6 Disposable Surface Electrodes
  • Power supply voltage: 3.3V-5V
  • 1000mm Cable Leads
  • No additional power supply



Interface Function


Grove_EMG_detector.png

  • J2: grove interface, connect to analog I/O;
  • J1: EMG Disposable Surface Electrodes connector.
  • U1: INA331IDGKT, difference amplifier.
  • U2,U3: OPA333, Zero drift amplifier.




Demonstration

This demonstration will show you how to use Grove - LCD RGB Backlight, we need a Seeeduino V3.0, a Grove - LED Bar and Grove - Base Shield.

Hardware Installation

Plug Grove - Base Shield to Seeeduino, then connect Grove - LED Bar to D8, connect Grove - EMG Sensor to A0.

Finally, tack the three electrodes to your muscle, and keep a distance between each electrodes.


Emg connect.jpg



Download Code and Upload

You can download the demo code in github, click here, then extract it to anywhere.

Then upload the code to Seeeduino, if you have any problem about code uploading, please refer to Getting Start Wiht Seeeduino


Emg ide.png



Move

When finish downloading demo code, it'll take about 5s to initialize, you should keep static when initializing.

You can see that when initializing, the Led Bar will go form level 10 to level 0. When Led Bar All off, you can move now.

When you are moving, you can find that the level of Led Bar will change.

Grove emg demo 2.gif





Resource

Personal tools
Namespaces

Variants
Actions
Bazaar
Navigation
Collections
Toolbox