Grove - Encoder

From Wiki 来自痴汉的爱
Jump to: navigation, search

Encoder2.jpgEncoder back.jpg

This module is an incremental rotary encoder. It encodes the rotation signal from the axis and output the signal by electronic pulse. The Grove – Encoder is one of the Grove series and has a standard Grove interface.
When you need to add a rotary knob to your project, for example a volume knob for a speaker, a selection panel or a digital input, this will be your first choice.


Get One Now Banner.png


Contents


Features

  • Incremental encoder.
  • Grove Interface.
  • 360 degree rotary.

Specification

Item Min Typical Max Unit
Voltage 4.5 5 5.5 V
Current 10 20 30 mA
Dimension 20x 20 mm
Net Weight 12 g


Getting Started

This Grove-Encoder is very easy to use with the Encoder Lib designed by seeedstudio. Simply connect this module to the D2 connector of Base Shield and you can start using. The following is a introduction of how to make a Circular LED bar (the idea came from seeedstudio wish).

  • This Circular LED bar consists of an Encoder and a Grove-CircularLED module. Connect the two modules to Base shield as the following picture:<b

Cirhard.jpg


  • Restart the Arduino IDE and open the example by the path :File->Examples->Encoder->EncodeCircuiBar.
#include <CircularLED.h>
#include <Encoder.h>
#include <TimerOne.h>
CircularLED circularLED;
unsigned int LED[24];
int index_LED;
void setup()
{
  encoder.Timer_init();
}
void loop()
{
    if (encoder.rotate_flag ==1)
  {
    if (encoder.direct==1)
    {
      index_LED++;
      if (index_LED>23)
      index_LED=24;
      SenttocircularBar(index_LED);
    }
     else
     {
      index_LED--;
      if(index_LED<0)
      index_LED=0;
      SenttocircularBar(index_LED);
     }
    encoder.rotate_flag =0;
  }
}
void SenttocircularBar(int index)
{
  for (int i=0;i<24;i++)
  {
    if (i<index)
    {
      LED[i]=0xff;
    }
    else
    LED[i]=0;
  }
  circularLED.CircularLEDWrite(LED);
}


  • Upload it to your Arduino/Seeeduino, please refer to here to learn how to upload sketches. You can see:


Encoder&Circular LED.gif

Note: It is able to generate another signal when it’s being pressed down. However due to the limitation of the number of Grove signal cable, the module is made without output of this signal.

Resources

Personal tools
Namespaces

Variants
Actions
Bazaar
Navigation
Collections
Toolbox