Grove - Water Sensor

From Wiki
Jump to: navigation, search

Contents

Introduction

The Water Sensor module is part of the Grove system. It indicates whether the sensor is dry, damp or completely immersed in water by measuring conductivity. The sensor traces have a weak pull-up resistor of 1 MΩ. The resistor will pull the sensor trace value high until a drop of water shorts the sensor trace to the grounded trace. Believe it or not this circuit will work with the digital I/O pins of your Arduino or you can use it with the analog pins to detect the amount of water induced contact between the grounded and sensor traces.

Model:SEN113104

Twig - Water Sensor.jpg

Features

  • Grove compatible interface
  • Low power consumption
  • 2.0cm x 2.0cm Grove module
  • High sensitivity

Applications Ideas

  • Rainfall detecting
  • Liquid leakage
  • Tank overflow detector

Cautions

This device is for educational and hobby applications only. It is not intended to be used in applications where its malfunction could result in damage to property or human safety.

Specification

Item Min Typical Max Unit
Working Voltage 4.75 5.0 5.25 V
Current <20 mA
Working Temperature 10 - 30
Working Humidity (without condensation) 10 - 90  %

Usage

Connect the module to the Basic board using any of the digital pin. You can gain the value of the signal pin. When there is water on the bare conducting wires, the value is LOW. Else it is HIGH.

The following sketch demonstrates a simple application of using the Water sensor to control the buzzer. As the picture on the below indicates, the Water sensor is connected to digital port 8 of the Grove - Basic Shield and the Buzzer is connected to digital port 12. When there is water on the bare conducting wires, the SIG pin output a LOW voltage. Then the Buzzer sounds. The hardware installation is as follows:


Water Buzzer.jpg

  • Then connect Arduino to PC by using a USB cable.
  • Copy and paste code below to a new Arduino sketch.
/*macro definition of water sensor and the buzzer*/
#define WATER_SENSOR 8
#define BUZZER 12
void setup()
{
	pins_init();
}
void loop()
{
	if(isExposedToWater())
		soundAlarm();
}
void pins_init()
{
	pinMode(WATER_SENSOR, INPUT);
	pinMode(BUZZER, OUTPUT);
}
/************************************************************************/
/*Function: When the sensor is exposed to the water, the buzzer sounds	*/
/*			for 2 seonds.												*/
void soundAlarm()
{
	for(uint8_t i = 0;i < 20;i ++)
	{
		digitalWrite(BUZZER, HIGH);
		delay(50);
		digitalWrite(BUZZER, LOW);
		delay(50);
	}
}
/************************************************************************/
/*Function: Determine whether the sensor is exposed to the water		*/
/*Parameter:-void           											*/
/*Return:	-boolean,if it is exposed to the water,it will return ture. */
boolean isExposedToWater()
{
	if(digitalRead(WATER_SENSOR) == LOW)
		return true;
	else return false;
}
  • Upload the code, Please click here if you do not know how to upload.
  • Then the buzzer sounds when the sensor is damp or completely immersed in water. Have a try!

Resources

Support

If you have questions or other better design ideas, you can go to our forum or wish to discuss.

Personal tools
Namespaces

Variants
Actions
Seeed Products
Support
Toolbox