TOP

Grove - Chainable RGB LED

From Wiki 来自痴汉的爱
(Redirected from Twig - Chainable RGB LED)
Jump to: navigation, search

[中文]

Chanbalelednb1.jpg

Contents

Introduction

Chainable RGB LED is based on P9813 chip which is a full-color light source LED driver chip, and can provide constant current drive and modulated output of 256 gray. Transmission by wire (DATA and CLK), built-in recycling, can enhance the transmission distance.

Model: COM53140P

Specification

  • Operating Voltage: 5V
  • Operating Current: 20mA
  • Communication Protocol: Serial

Usage

With Arduino

When you get Grove - Chainble RGB LED, you may think how I can light up it. Now we will show you this demo: all colors of RGB cycles in an uniform way.
The hardware installation like this:
Picture

To complete this demo, you can use one or more Grove - Chainable RGB LED. Note that the IN interface of one Grove - Chainable RGB LED should be connect to D7/D8 of Grove - Base Shield and its OUT interface connect to IN interface of another Grove - Chainable RGB LED, chainable more LED in this way. Jasa seo, Jasa seo jakarta

/* 
 * Example of using the ChainableRGB library for controlling a Grove RGB.
 * This code cycles through all the colors in an uniform way. This is accomplished using a HSB color space. 
 */
#include <ChainableLED.h>

#define NUM_LEDS  5

ChainableLED leds(7, 8, NUM_LEDS);

void setup()
{
}

float hue = 0.0;
boolean up = true;

void loop()
{
  for (byte i=0; i<NUM_LEDS; i++)
    leds.setColorHSB(i, hue, 1.0, 0.5);
    
  delay(50);
    
  if (up)
    hue+= 0.025;
  else
    hue-= 0.025;
    
  if (hue>=1.0 && up)
    up = false;
  else if (hue<=0.0 && !up)
    up = true;
}

You can observe this scene: colors of two LED will gradient consistently.

Extend application:
Based on Chainable LED Library, we have designed this demo: RGB color varies with the temperature measured by Grove - temperature. The RGB color vary from green to red when the temperature is from 25 to 32. The test code is shown below. Do it if you are interested in it.

// demo of temperature -> rgbLED
// temperature form 25 - 32, rgbLed from green -> red
// Grove-temperature plu to A0
// LED plug to D7,D8

#include <Streaming.h>
#include <ChainableLED.h>

#define TEMPUP 32
#define TEMPDOWN 25

ChainableLED leds(7, 8, 1); // connect to pin7 and pin8 , one led

int getAnalog() // get value from A0
{
    int sum = 0;
    for(int i=0; i<32; i++)
    {
        sum += analogRead(A0);
    }
    
    return sum>>5;
}

float getTemp() // get temperature
{
    float temperature = 0.0;
    float resistance = 0.0;
    int B = 3975; //B value of the thermistor
    
    int a = getAnalog();
    
    resistance = (float)(1023-a)*10000/a; //get the resistance of the sensor;
    temperature = 1/(log(resistance/10000)/B+1/298.15)-273.15; //convert to temperature via datasheet ;
    return temperature;
}

void ledLight(int dta) // light led
{

    dta = dta/4; // 0 - 255
    
    int colorR = dta;
    int colorG = 255-dta;
    int colorB = 0;

    leds.setColorRGB(0, colorR, colorG, colorB);
}

void setup()
{
    Serial.begin(38400);
    cout << "hello world !" << endl;
}

void loop()
{
    float temp = getTemp();
    int nTemp = temp*100;
    
    nTemp = nTemp > TEMPUP*100 ? TEMPUP*100 : (nTemp < TEMPDOWN*100 ? TEMPDOWN*100 : nTemp);
    nTemp = map(nTemp, TEMPDOWN*100, TEMPUP*100, 0, 1023);
    ledLight(nTemp);
    delay(100);
}

With Raspberry Pi

1.You should have got a raspberry pi and a grovepi or grovepi+.
2.You should have completed configuring the development enviroment, otherwise follow here.
3.Connection

  • Plug the sensor to grovepi socket D7 by using a grove cable.

4.Navigate to the demos' directory:

   cd yourpath/GrovePi/Software/Python/
  • To see the code
   nano grove_chainable_rgb_led.py   # "Ctrl+x" to exit #
import time
import grovepi

# Connect first LED in Chainable RGB LED chain to digital port D7
# In: CI,DI,VCC,GND
# Out: CO,DO,VCC,GND
pin = 7

# I have 10 LEDs connected in series with the first connected to the GrovePi and the last not connected
# First LED input socket connected to GrovePi, output socket connected to second LED input and so on
numleds = 1  

grovepi.pinMode(pin,"OUTPUT")
time.sleep(1)

# Chainable RGB LED methods
# grovepi.storeColor(red, green, blue)
# grovepi.chainableRgbLed_init(pin, numLeds)
# grovepi.chainableRgbLed_test(pin, numLeds, testColor)
# grovepi.chainableRgbLed_pattern(pin, pattern, whichLed)
# grovepi.chainableRgbLed_modulo(pin, offset, divisor)
# grovepi.chainableRgbLed_setLevel(pin, level, reverse)

# test colors used in grovepi.chainableRgbLed_test()
testColorBlack = 0   # 0b000 #000000
testColorBlue = 1    # 0b001 #0000FF
testColorGreen = 2   # 0b010 #00FF00
testColorCyan = 3    # 0b011 #00FFFF
testColorRed = 4     # 0b100 #FF0000
testColorMagenta = 5 # 0b101 #FF00FF
testColorYellow = 6  # 0b110 #FFFF00
testColorWhite = 7   # 0b111 #FFFFFF

# patterns used in grovepi.chainableRgbLed_pattern()
thisLedOnly = 0
allLedsExceptThis = 1
thisLedAndInwards = 2
thisLedAndOutwards = 3

try:

    print "Test 1) Initialise"

    # init chain of leds
    grovepi.chainableRgbLed_init(pin, numleds)
    time.sleep(.5)

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set led 1 to green
    grovepi.chainableRgbLed_pattern(pin, thisLedOnly, 0)
    time.sleep(.5)

    # change color to red
    grovepi.storeColor(255,0,0)
    time.sleep(.5)

    # set led 10 to red
    grovepi.chainableRgbLed_pattern(pin, thisLedOnly, 9)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 2a) Test Patterns - black"

    # test pattern 0 - black (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(1)


    print "Test 2b) Test Patterns - blue"

    # test pattern 1 blue
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlue)
    time.sleep(1)


    print "Test 2c) Test Patterns - green"

    # test pattern 2 green
    grovepi.chainableRgbLed_test(pin, numleds, testColorGreen)
    time.sleep(1)


    print "Test 2d) Test Patterns - cyan"

    # test pattern 3 cyan
    grovepi.chainableRgbLed_test(pin, numleds, testColorCyan)
    time.sleep(1)


    print "Test 2e) Test Patterns - red"

    # test pattern 4 red
    grovepi.chainableRgbLed_test(pin, numleds, testColorRed)
    time.sleep(1)


    print "Test 2f) Test Patterns - magenta"

    # test pattern 5 magenta
    grovepi.chainableRgbLed_test(pin, numleds, testColorMagenta)
    time.sleep(1)


    print "Test 2g) Test Patterns - yellow"

    # test pattern 6 yellow
    grovepi.chainableRgbLed_test(pin, numleds, testColorYellow)
    time.sleep(1)


    print "Test 2h) Test Patterns - white"

    # test pattern 7 white
    grovepi.chainableRgbLed_test(pin, numleds, testColorWhite)
    time.sleep(1)


    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 3a) Set using pattern - this led only"

    # change color to red
    grovepi.storeColor(255,0,0)
    time.sleep(.5)

    # set led 3 to red
    grovepi.chainableRgbLed_pattern(pin, thisLedOnly, 2)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 3b) Set using pattern - all leds except this"

    # change color to blue
    grovepi.storeColor(0,0,255)
    time.sleep(.5)

    # set all leds except for 3 to blue
    grovepi.chainableRgbLed_pattern(pin, allLedsExceptThis, 3)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 3c) Set using pattern - this led and inwards"

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set leds 1-3 to green
    grovepi.chainableRgbLed_pattern(pin, thisLedAndInwards, 2)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 3d) Set using pattern - this led and outwards"

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set leds 7-10 to green
    grovepi.chainableRgbLed_pattern(pin, thisLedAndOutwards, 6)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 4a) Set using modulo - all leds"

    # change color to black (fully off)
    grovepi.storeColor(0,0,0)
    time.sleep(.5)

    # set all leds black
    # offset 0 means start at first led
    # divisor 1 means every led
    grovepi.chainableRgbLed_modulo(pin, 0, 1)
    time.sleep(.5)

    # change color to white (fully on)
    grovepi.storeColor(255,255,255)
    time.sleep(.5)

    # set all leds white
    grovepi.chainableRgbLed_modulo(pin, 0, 1)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 4b) Set using modulo - every 2"

    # change color to red
    grovepi.storeColor(255,0,0)
    time.sleep(.5)

    # set every 2nd led to red
    grovepi.chainableRgbLed_modulo(pin, 0, 2)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)


    print "Test 4c) Set using modulo - every 2, offset 1"

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set every 2nd led to green, offset 1
    grovepi.chainableRgbLed_modulo(pin, 1, 2)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 4d) Set using modulo - every 3, offset 0"

    # change color to red
    grovepi.storeColor(255,0,0)
    time.sleep(.5)

    # set every 3nd led to red
    grovepi.chainableRgbLed_modulo(pin, 0, 3)
    time.sleep(.5)

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set every 3nd led to green, offset 1
    grovepi.chainableRgbLed_modulo(pin, 1, 3)
    time.sleep(.5)

    # change color to blue
    grovepi.storeColor(0,0,255)
    time.sleep(.5)

    # set every 3nd led to blue, offset 2
    grovepi.chainableRgbLed_modulo(pin, 2, 3)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 4e) Set using modulo - every 3, offset 1"

    # change color to yellow
    grovepi.storeColor(255,255,0)
    time.sleep(.5)

    # set every 4nd led to yellow
    grovepi.chainableRgbLed_modulo(pin, 1, 3)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)


    print "Test 4f) Set using modulo - every 3, offset 2"

    # change color to magenta
    grovepi.storeColor(255,0,255)
    time.sleep(.5)

    # set every 4nd led to magenta
    grovepi.chainableRgbLed_modulo(pin, 2, 3)
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 5a) Set level 6"

    # change color to green
    grovepi.storeColor(0,255,0)
    time.sleep(.5)

    # set leds 1-6 to green
    grovepi.write_i2c_block(0x04,[95,pin,6,0])
    time.sleep(.5)

    # pause so you can see what happened
    time.sleep(2)

    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    time.sleep(.5)


    print "Test 5b) Set level 7 - reverse"

    # change color to red
    grovepi.storeColor(255,0,0)
    time.sleep(.5)

    # set leds 4-10 to red
    grovepi.write_i2c_block(0x04,[95,pin,7,1])
    time.sleep(.5)


except KeyboardInterrupt:
    # reset (all off)
    grovepi.chainableRgbLed_test(pin, numleds, testColorBlack)
    break
except IOError:
    print "Error"

  • Notice that there's something you have to concern of:
pin = 7         #setting up the output pin
numleds = 1     #how many leds you plug
  • Also all methods you can see in grovepi.py is:
storeColor(red, green, blue)
chainableRgbLed_init(pin, numLeds)
chainableRgbLed_test(pin, numLeds, testColor)
chainableRgbLed_pattern(pin, pattern, whichLed)
chainableRgbLed_modulo(pin, offset, divisor)
chainableRgbLed_setLevel(pin, level, reverse)

5.Run the demo.

   sudo python grove_chainable_rgb_led.py


6.This demo may not work if your grovepi dosen't have the newest firmware, update the firmware.

cd yourpath/GrovePi/Firmware
sudo ./firmware_update.sh

With Beaglebone Green

To begin editing programs that live on BBG, you can use the Cloud9 IDE.
As a simple exercise to become familiar with Cloud9 IDE, creating a simple application to blink one of the 4 user programmable LEDs on the BeagleBone is a good start.

If this is your first time to use Cloud9 IDE, please follow this link.


Step1: Set the Grove - UART socket as a Grove - GPIO Socket, just follow this link.

Step2: Click the "+" in the top-right to create a new file.

C9-create-tab.png

C9 newfile.jpg

Step3: Copy and paste the following code into the new tab

import time
import Adafruit_BBIO.GPIO as GPIO
 
CLK_PIN = "P9_22"
DATA_PIN = "P9_21"
NUMBER_OF_LEDS = 1
 
class ChainableLED():
    def __init__(self, clk_pin, data_pin, number_of_leds):
        self.__clk_pin = clk_pin
        self.__data_pin = data_pin
        self.__number_of_leds = number_of_leds
 
        GPIO.setup(self.__clk_pin, GPIO.OUT)
        GPIO.setup(self.__data_pin, GPIO.OUT)
 
        for i in range(self.__number_of_leds):
            self.setColorRGB(i, 0, 0, 0)
 
    def clk(self):
        GPIO.output(self.__clk_pin, GPIO.LOW)
        time.sleep(0.00002)
        GPIO.output(self.__clk_pin, GPIO.HIGH)
        time.sleep(0.00002)
 
    def sendByte(self, b):
        "Send one bit at a time, starting with the MSB"
        for i in range(8):
            # If MSB is 1, write one and clock it, else write 0 and clock
            if (b & 0x80) != 0:
                GPIO.output(self.__data_pin, GPIO.HIGH)
            else:
                GPIO.output(self.__data_pin, GPIO.LOW)
            self.clk()
 
            # Advance to the next bit to send
            b = b << 1
 
    def sendColor(self, red, green, blue):
        "Start by sending a byte with the format '1 1 /B7 /B6 /G7 /G6 /R7 /R6' "
        #prefix = B11000000
        prefix = 0xC0
        if (blue & 0x80) == 0:     
            #prefix |= B00100000
            prefix |= 0x20
        if (blue & 0x40) == 0:     
            #prefix |= B00010000
            prefix |= 0x10
        if (green & 0x80) == 0:    
            #prefix |= B00001000
            prefix |= 0x08
        if (green & 0x40) == 0:    
            #prefix |= B00000100
            prefix |= 0x04
        if (red & 0x80) == 0:      
            #prefix |= B00000010
            prefix |= 0x02
        if (red & 0x40) == 0:      
            #prefix |= B00000001
            prefix |= 0x01
        self.sendByte(prefix)
 
        # Now must send the 3 colors
        self.sendByte(blue)
        self.sendByte(green)
        self.sendByte(red)
 
    def setColorRGB(self, led, red, green, blue):
        # Send data frame prefix (32x '0')
        self.sendByte(0x00)
        self.sendByte(0x00)
        self.sendByte(0x00)
        self.sendByte(0x00)
 
        # Send color data for each one of the leds
        for i in range(self.__number_of_leds):
            '''
            if i == led:
                _led_state[i*3 + _CL_RED] = red;
                _led_state[i*3 + _CL_GREEN] = green;
                _led_state[i*3 + _CL_BLUE] = blue;
            sendColor(_led_state[i*3 + _CL_RED], 
                      _led_state[i*3 + _CL_GREEN], 
                      _led_state[i*3 + _CL_BLUE]);
            '''
            self.sendColor(red, green, blue)
 
        # Terminate data frame (32x "0")
        self.sendByte(0x00)
        self.sendByte(0x00)
        self.sendByte(0x00)
        self.sendByte(0x00)
 
 
# Note: Use P9_22(UART2_RXD) and P9_21(UART2_TXD) as GPIO.
# Connect the Grove - Chainable RGB LED to UART Grove port of Beaglebone Green.
if __name__ == "__main__":
    rgb_led = ChainableLED(CLK_PIN, DATA_PIN, NUMBER_OF_LEDS)
 
    while True:
        # The first parameter: NUMBER_OF_LEDS - 1; Other parameters: the RGB values.
        rgb_led.setColorRGB(0, 255, 0, 0)
        time.sleep(2)
        rgb_led.setColorRGB(0, 0, 255, 0)
        time.sleep(2)
        rgb_led.setColorRGB(0, 0, 0, 255)
        time.sleep(2)
        rgb_led.setColorRGB(0, 0, 255, 255)
        time.sleep(2)
        rgb_led.setColorRGB(0, 255, 0, 255)
        time.sleep(2)
        rgb_led.setColorRGB(0, 255, 255, 0)
        time.sleep(2)
        rgb_led.setColorRGB(0, 255, 255, 255)
        time.sleep(2)

Step4: Save the file by clicking the disk icon and giving the file a name with the .py extension.

Step5: Connect Grove Chainable RGB LED to Grove UART socket on BBG.

Step6: Run the code. You'll find the RGB LED is changing color every 2 seconds.

Resources

Personal tools
Namespaces

Variants
Actions
Navigation
Support
Navigation
Collections
Toolbox