Something's Happening Here...

Most Recent

More...
mpu-9150
The MPU-9150™ is the world’s first 9-axis MotionTracking device desi...
I2C LCD
Hope this wish being granted
1279047098367[1]
1、I have a wireless local net work(WLAN); 2、the TV can‘t use the W...

Wishes Granted

More...
pcb
There is an OBD-II Shield, as the name implies, it was used in obd syste...
sensor
Just found the sensor on a chineese web page. Or any other garden soil h...
1
This is a BH1750FVI light intensity sensor module with built-in a 16 bit...

Wishes In Process

More...
12688922280[1]
Hello, I’d love to see more to see either the screw shield come ba...
LittleBits to Grove adaptator
Make a grove shield adapator to connect Bittlebits for kids activity ! T...
CapWizSW
I work on a lot of monitors – LCD, arcade, TV – and, an inex...

Most Popular

More...
wish3
DSO443
Seeed Studio and Bure (aka Chai Xiaoguang, the designer of DSO Nano) nev...
RGB LED Coffetable – Rainbow Carnival 2010 Entry
My entry for the Rainbowduino Carnival 2010 by seeedstudio A standalone ...
ECG2_AM1
The ECG2_AM1 is a fully functional implementation of a 2-lead electrocar...
Home Automation Node
I’m looking for the ultimate home automation node. Constraints: Sm...
IMG_4844
Overview A quadrature encoder outputs two square waves 90 degrees apart....