Special offer on this weekend

Last weekend we had 3 products on special, and they were sold out in few hours!  Today i am bringing you another 3 exciting products to this weekend :

Electronic Brick – Starter Kit:

This is a Starter kit of electronic brick; it includes  basic components and sensors. You can build many interesting projects even if you don’t know anything about soldering, and that makes it the best choice for beginners.
Parts list:

  • Arduino/Seeeduino sensor Chassis V1.1  X1
  • LCD 16*2 Characters X1
  • Rotary angle sensor (Analog) X1
  • Big button switch  X1
  • Buzzer X1
  • Tilt switch X1
  • Lighting emitting diode X2
  • Light sensor X1
  • Temperature sensor X1
  • 2pin plugable terminal module X1
  • Fully buckled 3 wire cable X5
  • 10 pin colorful ribbon cable with 2*5 IDC connector X1

Regular price:  $49 Sale price: $30

Available QTY: 10 Units

Electronic Brick – ADXL330 Acceleration Sensor(Analog)

This module included the same  Acceleration Sensor (ADXL330) as wiimote has, and it’s Electronic Brick compatible.

Features

  • 3 axis sensing
  • Small, low-profile package
  • 4×4×1.45mm LFCSP
  • Low power 180µA at 1.8V (typical)
  • Single-supply operation 1.8 to 3.6V
  • 10,000 g shock survival
  • Excellent temperature stability
  • BW adjustment with a single capacitor per axis
  • RoHS/WEEE lead-free compliant

Regular price:  $24.5 Sale price: $16

Available QTY: 20 Units

Electronic Brick – Real Time Clock Module(DS1307)

A Electronic Brick compatible module includes the DS1307 RTC module, it can be also used as a shield for Arduino.

Regular price:  $13.5 Sale price: $7

Available QTY: 20 Units

Please note that the special price will be available on 0:00 AM , 26th June -0700GMT,  ends on 24:00 PM, 27th June.

About Author

6 thoughts on “Special offer on this weekend

  1. Just saw this early this morning. I had the RTC in my shopping cart and when I added something else the price had changed to 13.50. 🙁 I was going to but the “Real Time Clock Module” the “Electronic Brick – Starter Kit” a second Arduino and the iPodEXT Assembled version! I can’t believe I missed out on this by just a few minutes this morning. Is there any chance this deal could be extended? Please please?

  2. Yes!!! I got it!!! Electronic Brick – Starter Kit! woooooohoooo!!!, long waiting, couse time diference!!! Thanks a lot! (I miss rainbowduino and LED MAtrix offer, but I keeep “hunting for” LOL).

  3. Which product? I think it’s just started, you should be able to purchase them now! Come on! be hurry.

Comments are closed.

Calendar

June 2010
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
282930