Introducing XIAO ESP32S3 for Meshtastic, The Smallest LoRa Dev Kit in The World
Since we released the Wio Tracker 1110 Dev Kit and SenseCAP Card Tracker T1000-E, we’ve gotten a lot of feedback from the community to include a smaller, more affordable Meshtastic powered product. And our answer is the XIAO ESP32S3 for Meshtastic & LoRa. Sized as small as your thumb, and priced at only $9.9, it‘s the smallest dev kit for prototyping your first Meshtastic and LoRa/LoRaWAN projects.
XIAO ESP32S3 + Semtech SX1262 LoRa
Featuring the powerful thumb-sized XIAO ESP32S3 Dev Board and a Wio-SX1262 Extension Board, the XIAO ESP32S3 Dev Kit for Meshtastic & LoRa is a super mini LoRa dev kit supporting LoRa (862-930MHz) with a 5km LoRa range. It also supports WiFi, BLE for wireless communication with a range of 100m+. Built on the XIAO ESP32S3, the kit comes with a built-in power management systems, and can be expanded via IIC, UART, and other GPIO interfaces. Compatible with Arduino IDE, it’s available for pre-order now at $9.9, with an estimated shipping in November, 2024.

Key Features of XIAO ESP32S3 for Meshtastic and LoRa Dev Kit
- Meshtactic works out of the box: Pre-flashed with Meshtastic firmware, it is ready to work once powered on.
- Outstanding RF performance: Supports LoRa(862-930MHz) 2.4GHz Wi-Fi and BLE 5.0 dual wireless communication, support 2~5km(LoRa) and 100m+(Wi-Fi/BLE) remote communication when connected with U.FL antenna.
- Thumb-sized Compact Design: 21 x 18mm, adopting the classic form factor of Seeed Studio XIAO, suitable for space-limited projects.
- Powerful MCU Board: Incorporate the ESP32S3 32-bit, dual-core, Xtensa processor running at up to 240MHz, mounted multiple development ports, Arduino / MicroPython supported.
- Elaborate Power Design: Includes a Type-C USB interface and lithium battery charge management.
- Same Hardware for Multiple Applications: Can be developed as a Meshtastic node or router, a single-channel LoRaWAN gateway, or a LoRa & LoRaWAN sensor.

Applications of XIAO ESP32S3 for Meshtastic & LoRa
1. Tap into Meshtastic for Off-Grid Communication
Meshtastic is an open-source, off-grid, decentralized LoRa mesh network designed for affordable, low-power devices. This XIAO ESP32S3 Dev Kit offers a flexible and cost-effective solution for Meshtastic developers. You can build a Meshtastic device at an affordable price and use it as an emergency communication tool, similar to the SenseCAP T1000-E, but simpler in function. Moreover, thanks to the amazing Seeed Studio XIAO Product Ecosystem, it’s compatible with the XIAO Expansion Board and the Grove Expansion Board for adding screens, sensors, and over 300+ Grove modules, allowing you to customize your unique Meshtastic devices. You can even design your own casing.
2. Configure It as a LoRa/LoRaWAN Sensor Node
It can be set up as a LoRa node, enabling the XIAO ESP32S3 Dev Kit to connect with various sensors and transmit data using LoRaWAN. This offers flexibility for different applications, like home automation. Essentially, the XIAO ESP32S3 Dev Kit can serve as a data collection and transmission node, allowing for communication and control among smart home devices.
3. The Most Cost-Effective Single-Channel LoRa/LoRaWAN Gateway
Thanks to the powerful Semtech SX1262 LoRa Chip, you can turn it into a single-channel gateway, making it the most cost effective single-channel LoRaWAN gateway in the world. It receives LoRa packets on a specific setting and share them with the LoRaWAN network. By using the XIAO ESP32S3 Dev Kit, you can set it up to connect to The Things Network or Chripstack. This kit is great for those who want to learn about LoRa technology and connect to a LoRa Network Server (LNS).
Some Useful Links
Here are some guides for you to get started:
Pre-Order Now at $9.9
Available for pre-order now at just $9.9, the XIAO ESP32S3 Dev Kit is one of our solutions to provide the community more affordable and flexible products for you to build your LoRa-based IoT projects. Stay tuned for more updates on our Meshtastic-powered and LoRaWAN products. If you have any ideas or suggestions about our Meshtastic-compatible products, feel free to share them in the comments!
Sometimes, you just don’t have the time to write everything yourself, and that’s when I decided to buy nursing papers from this service. The experience was surprisingly straightforward. I uploaded my requirements, and they immediately assigned a writer with expertise in my topic. What impressed me most was how quickly they grasped what I needed. Even though I was a little late with my instructions, they adapted without any complaints. The final result was not just well-written but actually helped me understand the topic better, which I didn’t expect. If you’re juggling a million things like I was, this might be the smartest move to keep your grades intact without losing sleep.
Subject: Partnership Opportunity: Promoting LoRa and Meshtastic Technologies via YouTube Review Channel
Dear Seeed Studio,
I hope this message finds you well. My name is Robert Lock, and together with my son, we are in the process of launching a YouTube review channel focused on educating and raising awareness about innovative communication technologies—specifically LoRa and Meshtastic. Our mission is to highlight the transformative potential of these technologies, showcase their practical applications, and help users understand how they can leverage them in real-world situations.
We are currently working on a channel name, but we are thinking along the lines of “Father and Son: Next Level Communications.” This channel will not only serve as a platform for reviews and tutorials but also as a way for us to bond over a shared passion for technology. My son has a keen interest in this field, and through this project, we hope to create something lasting that we can both be proud of and that I can leave behind as a legacy.
We are very ambitious and eager to work with companies like yours that are developing LoRa and Meshtastic-based solutions. To help bring our vision to life, we are seeking product donations or samples that we can feature and review on our channel. Once we establish our audience and begin generating traction, we would be glad to reimburse your company for contributions made at the start.
As a family, we are deeply committed to professionalism and integrity. We are 100% open to working with any requirements or expectations you may have. Your support would go a long way in helping us raise awareness of these cutting-edge technologies and introduce them to a wider audience.
I also want to mention that, unfortunately, our previous startup was destroyed by the recent hurricane. This new venture is a dream we are working hard to rebuild, and we are grateful for any support that can help us get started again. Thank you for your time, consideration, and for the opportunity to potentially collaborate with you.
Blessings from our family to yours, and we sincerely appreciate your thoughts and prayers as we work towards this new chapter.
Thank you again for your time and contemplation.
Best regards,
Robert Lock
165 South French Broad Ave, Apt 1B
Email: [email protected]
[Your YouTube Channel Name] (TBD)
1WIN-ə qoşulmaq qərarına gəldiyim andan bəri burada keçirdiyim hər dəqiqədən zövq alıram. Platformaya qoşulduğumda ilk depozitdə mənə 500%-lik bonus təklif etdilər ki, bu da oyunları sınaqdan keçirmək üçün əla fürsət oldu. Klassik slotlardan, maraqlı turnirlərə və canlı dilerlərlə oyunlara qədər müxtəlif seçimlər var, bu da hər zaman yenilik və həyəcan təmin edir. Platformanın rəsmi səhifəsi olan http://www.1wins-az.net üzərindən qeydiyyatdan keçib bu gözəl təkliflərdən faydalana bilərsiniz. Pul çıxarışlarında problem yaşamamışam, hər əməliyyatım cəmi bir neçə dəqiqə içində baş verir.