Particle Boron IoT Development Board (Cellular+Mesh+Bluetooth)

SKU
113990598

Particle Boron IoT Development Board (Cellular+Mesh+Bluetooth),mesh networking,end to end,a standalone cellular endpoint or LTE enabled gateway,u-blox SARA R410 LTE modem,LTE CAT M1/ NB1 module,Particle Device Cloud,Thread,Bluetooth 5,BLE

$49.00
In stock
  • 50+: $48.00
-
+

Pls kindly noted that the first 10pcs shipped out will be Kits which including:

  • Boron LTE dev board
  • Mini breadboard
  • Cellular flex antenna
  • USB cable
  • Starter project includes two resistors (220 ohm), one red LED, and one photodiode

Note: Particle’s MVNO will provide support for LTE M1 connectivity in the US upon initial release. Not in the region? Check out the Boron 2G/3G Kit. See the cellular FAQ for details.

The Boron LTE is a powerful LTE CAT-M1/NB1 enabled development board that can act as either a standalone cellular endpoint or LTE enabled gateway for Particle Mesh networks. It is based on the Nordic nRF52840 and has built-in battery charging circuitry so it’s easy to connect a Li-Po and deploy your local network in minutes.

The Boron is great for connecting existing projects to the Particle Device Cloud or as a gateway to connect an entire group of local endpoints where Wi-Fi is missing or unreliable.

All Particle hardware is designed from the ground up to work with the Device Cloud; a powerful set of tools and infrastructure to build, connect, and manage your IoT fleet. The Device Cloud for Particle Mesh is priced by network. All Particle customers get 3 free months of Device Cloud access for micro networks using a cellular gateway. A micro network is defined as a network with 10 total devices and a single gateway. Please refer to our pricing documentation for more information.

Features:

  • u-blox SARA R410 LTE modem 

    - LTE CAT M1/ NB1 module with global hardware support (MVNO support for US only) 

    - 3GPP Release 13 LTE Cat M1

  • Nordic Semiconductor nRF52840 SoC 

    - ARM Cortex-M4F 32-bit processor @ 64MHz     

    - 1MB flash, 256KB RAM 

    - IEEE 802.15.4-2006: 250 Kbps 

    - Bluetooth 5: 2 Mbps, 1 Mbps, 500 Kbps, 125 Kbps   

    - Supports DSP instructions, HW accelerated Floating Point Unit (FPU) calculations   

    - ARM TrustZone CryptoCell-310 Cryptographic and security module    

    - Up to +8 dBm TX power (down to -20 dBm in 4 dB steps)    

    - NFC-A tag     

  • On-board additional 2MB SPI flash

  • 20 mixed signal GPIO (6 x Analog, 8 x PWM), UART, I2C, SPI

  • Micro USB 2.0 full speed (12 Mbps)

  • Integrated Li-Po charging and battery connector

  • JTAG (SWD) Connector

  • RGB status LED

  • Reset and Mode buttons

  • Dual SIM support: Nano 4FF (unpopulated) and MFF2

  • U.FL connector for external antenna

  • Meets the Feather specification in dimensions and pinout

  • FCC and PTCRB certified

  • RoHS compliant (lead-free)

           

           

Technical details

Dimensions 51mm x23mm x11mm
Weight G.W 18g
Battery Exclude

Part List

Boron LTE dev board 1
Cellular flex antenna 1

ECCN/HTS

ECCN 5A991.b
HSCODE 8517709000
USHSCODE 85177000
UPC 841454121695
FCC 1
CE 1

BUILDING PARTICLE MESH WITH OPENTHREAD

While planning Particle Mesh, we did so with the view that current IoT networks connect only a portion of the interesting places and spaces that developers want to reach. From remote pipelines without an existing Wi-Fi infrastructure to subterranean syste

PARTICLE MESH 102: SELECTING A ROLE FOR YOUR DEVICE

In a Particle Mesh network, there are three types of roles a device can take: a gateway, a repeater, or an endpoint. A previous post, Particle Mesh 101, introduces the basic concepts of roles but stops short of suggesting which role a particular device in

HOW TO BUILD A WIRELESS MESH NETWORK

In the past, building beyond a single-point connection required high-cost hardware solutions and software implementations to connect the in-between spaces needed for device to device communication. As IoT platforms have matured, they have started to embra

Write Your Own Review
Only registered users can write reviews. Please Sign in or create an account

Product Faqs


Sort by   
    There are no faqs for this item.