Grove - Speech Recognizer

SKU
101020232
Rating:
67% of 100
Use voice to interact with things around you can always be one of the most interesting things of IoT application, we want to make something more different and cooler
$19.50
In stock
  • 10+: $17.50
  • 20+: $16.50
  • More
  • 50+: $15.50
  • Less
-
+

Use voice to interact with things around you can always be one of the most interesting things of IoT application, we want to make something more different and cooler. Recently we just launched the voice control solution “Respeaker” on Kickstarter and it becomes the blockbuster. However not everybody needs a Respeaker to build voice control project, sometimes people only need a simple solution, here we would like to introduce the first generation of grove speech recognizer to realize your dream of smart home easily and fast.


Grove speech recognizer is a designed for voice control application such as smart home, smart toy, voice control robot, anything you would like to control through voice, it worth a try. The board includes a Nuvoton ISD9160, a microphone, 1 SPI flash, 1 grove connector,1 speaker connector and 1 led to reflect to your voice.


Nuvoton ISD9160 is (SoC) Chipcorder that based on Cortex™-M0, it provides strong and economic solution for voice control applications. ISD9160 is not the only amazing thing in this grove. Let’s look at the microphone. Remember the uncomfortable moment when you have to speak directly and closely to the voice recognizer device to make sure it can hear you? It won’t happen this time! The microphone on grove-speech recognizer is Omni-directional, which means that whether a user speaks into the microphone from the front, back, left or right side, the microphone will record the signals all with equal gain.


This speech recognizer can recognize 22 pieces of commands including 'start', 'stop', 'Play music' and so on. Every time it recognizes a command, it will return a value and then the loudspeaker that connected to it will repeat the command. This value can be used to control other devices like motor, music player. We have tested it for hours to make sure it possesses a high recognition rate and a very low false trigger.

How to use it

  • Awaken Word: Hicell (Please pronounce it as one word)

  • When it recognizes the awaken word, LED turn red, then you can say the command word, if it recognize the command word, LED will turn blue.

Notes

  • The package does not include speaker.

  • The power of speaker should be lower than 1w to avoid any damage to the chip.


Features

  • Local Voice Recognition

  • Very low rate of false triggering

  • Speaker connector(JST2.0, speaker is not include)

  • Built-in microphone

  • 3.3/5V working voltage

  • 22 recognition entry

  • Default Baudrate: 9600



Technical details

Dimensions 0mm x0mm x0mm
Weight G.W 11g
Battery Exclude

Part List

Grove - Speech Recognizer 1
Grove - Cable 1

ECCN/HTS

ECCN EAR99
HSCODE 9031900090
USHSCODE 8518900090
UPC 841454118794

Grove - Speech Recognizer

Wiki of Grove - Speech Recognizer

Write Your Own Review
Only registered users can write reviews. Please Sign in or create an account
Customer Reviews
  1.  
    Rating
    20%
    not works for me..

    Review by

    Posted on

  2.  
    Rating
    80%
    Don't checked yet.

    Review by

    Posted on

  3.  
    Rating
    100%
    Excellent Seller and Product !!! THANKS !!! ++++++++++++

    Review by

    Posted on

Product Faqs


Sort by