Seeedstudio Grove - TF Mini LiDAR

SKU
114991434
Rating:
98% of 100

LiDar RPLiDAR rplidar lidar

$39.95
In stock
  • 2+: $35.95
-
+

The TF Mini LiDAR is based on ToF (Time of Flight) principle and integrated with unique optical and electrical designs, so as to achieve stable, precise, high sensitivity and high-speed distance detection.

ToF is the abbreviation of Time of Flight technology, and its operating principle is as follows: a modulated near-infrared light is sent from the sensor and reflected by an object; the distance to the object to be shot can be converted with the sensor by calculating the time difference or phase difference between the light sending and the light reflection, so as to produce the depth information. 

Applications:

• Drone altitude holding and terrain following

• Machine control and safety sensor

• Robot distance detection

If you are using Seeeduino Lite then just put it straight into the Grove Serial Interfaces.
IMG_4409a.JPG

1.1 TF mini optical simulation of the optical path:

雷达1.jpg

1.2 Measurement range schematic diagram:

雷达2.jpg

1.3 Line sequence description:

雷达3.jpg

1.4 Product Size Specifications

雷达4.jpg

Technical details

Dimensions 42mm x15mm x16mm
Weight G.W 4.7g
Battery Exclude
Operating range 0.3m-12m
Maximum operating range at 10% reflectivity 5m
Average power consumption 0.6W
Applicable voltage range 4.5V-6V
Acceptance angle 2.3°
Minimum resolution ratio 1cm
Frequency 100Hz
Accuracy 1% (less than 6m), 2% (6m-12m)
Distance detection unit cm
Laser Wavelength 850nm
Operating temperature -20℃-60℃
Light sensitivity 70,000lux
Communication interface UART
Laser Safety Class FDA Class Ⅰ
LED peak current 800ma
Electromagnetic Compatibility(EMC) EN 55032 Class B

Part List

TF Mini LiDar 1
Grove Cable 1

ECCN/HTS

ECCN ERA99
HSCODE 9015100000
USHSCODE 9015900130
UPC 841454121336

Seeedstudio Grove - TF Mini LiDAR

This is the wiki page for this product, which will show you how to use the product, as well as details about the software and hardware.

Write Your Own Review
Only registered users can write reviews. Please Sign in or create an account

Product Faqs


Sort by   
  • In reference to TF Mini LIDAR ref. 114991434 I need to know price for 10 or more units. Thank you.
    Question by: Raimundo Alfonso on 2019-02-27 12:29:51

    Hi, Raimundo, Please write an email to our customer service. qi.liao@seeed.cc. Regards

    Answer by: admin on 2019-02-28 12:00:15
  • Question by: admin on 2018-12-18 02:30:26

    Hi Dear Customer, The Grove-TF Mini LiDAR’s UART baud rate is 115200 and the SoftwareI2C can’t support it. So if we use 1 hardware UART to hook up the sensor and other hardware UART for Serial Port display, we need at least 2 hardware UART platforms, such as arduino mega, seeeduino lite and so on. If we only have 1 UART platform(ie. seeeduino v4.2, arduino uno), we can use the I2C LCD as display. Bill

    Answer by: admin on 2018-12-18 02:30:26
  • Question by: admin on 2018-12-18 02:30:25

    Hi there~ You can check our wiki # http://wiki.seeed.cc/Grove-TF_Mini_LiDAR/ # Regards

    Answer by: admin on 2018-12-18 02:30:25
  • Question by: admin on 2018-12-18 02:30:12

    Hi there~ We are glad that it works fine with you.Regards

    Answer by: admin on 2018-12-18 02:30:12
  • Question by: admin on 2018-12-18 02:29:58

    Hi khan~You can find the software in the vedio at our wiki,or you can just use Arduino's serial plotter to show the graph.For your convenience,you can download the software by the link below. =========================================================================== https://github.com/SeeedDocument/Grove-TF_Mini_LiDAR/raw/master/res/Grove-TF-Mini-LiDAR%20Master%20Computer%20Software.zip

    Answer by: admin on 2018-12-18 02:29:58
  • Question by: admin on 2018-12-18 02:29:53

    Hi Lawewnce, Please email us with the code you use and a picture to show the hardware connection. That will be helpful, thanks. =====================================dividing line============================= techsupport@seeed.cc

    Answer by: admin on 2018-12-18 02:29:53
  • Question by: admin on 2018-12-18 02:29:37

    Hi there ~ You can use this product continuously for two years . Regards

    Answer by: admin on 2018-12-18 02:29:37
  • Question by: admin on 2018-12-18 02:29:37

    You can use this product continuously for two years

    Answer by: admin on 2018-12-18 02:29:37
  • Question by: admin on 2018-12-18 02:24:12

    Hi there, we simulate the issue and suspect you select the pixmode, please do not select the pixmode and test it again. thanks.

    Answer by: admin on 2018-12-18 02:24:12
  • Question by: admin on 2018-12-18 02:23:38

    Hi there, we do not have the analog laser sensor, the tf mini support software serial, here is the library, **https://github.com/TFmini/TFmini-Arduino** thanks.

    Answer by: admin on 2018-12-18 02:23:38
  • Question by: admin on 2018-12-18 02:21:10

    <p style="margin:0in"><a href="http://publicholidays2018.net/"><span style="font-family:Arial;font-size:9.0pt">best holiday apk</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://publicholidays2018.net/2018-federal-holidays-usa-uk/"><span style="font-family:Arial;font-size:9.0pt">list best holiday apk</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/"><span style="font-family:Arial;font-size: 9.0pt">calendar's management</span></a><span style="font-family:Calibri; font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-liturgico-catolico-2018/"><span style="font-family:Arial;font-size:9.0pt">Verify services</span></a><a href="http://calendario-2018.info/calendario-febrero-2018/"><span style="font-family:Arial;font-size:9.0pt">Analysis of data</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-janeiro-2018/"><span style="font-family:Arial;font-size:9.0pt">Designs modes</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-diciembre-2017/"><span style="font-family:Arial;font-size:9.0pt">Incentive hiking</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-noviembre-2017/"><span style="font-family:Arial;font-size:9.0pt">Garbage collection</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://jacketsformenguide.com/"><span style="font-family:Arial; font-size:9.0pt">Modes of Jobs</span></a></p> <p style="margin:0in;font-family:Calibri;font-size:11.0pt">&nbsp;</p> <p style="margin:0in;font-family:Calibri;font-size:11.0pt">&nbsp;</p>

    Answer by: admin on 2018-12-18 02:21:10
  • Question by: admin on 2018-12-18 02:21:10

    <p style="margin:0in"><span style="font-family: Verdana;font-size:7.5pt">Thanks for sharing you have a very nice post&nbsp;<a href="http://howtokodi.co/">How to apply this pattern</a></span><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/install-setup-kodi-on-windows/"><span style="font-family:Verdana;font-size:7.5pt">Welcome all UK</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/upgrade-an-android-tv-box-on-kodi/"><span style="font-family:Verdana;font-size:7.5pt">Updating app weekly</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/enable-automatic-subtitles-on-kodi/"><span style="font-family:Verdana;font-size:7.5pt">best user app</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/install-covenant-on-kodi/"><span style="font-family: Verdana;font-size:7.5pt">how to achieve that goal</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/install-exodus-on-kodi/"><span style="font-family: Verdana;font-size:7.5pt">add feature</span></a><span style="font-family:Calibri; font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/upgrade-kodi-on-android-tv-box/"><span style="font-family:Verdana;font-size:7.5pt">Best Design for suit</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/install-a-vpn-with-kodi-on-amazon-fire-tv-stick/"><span style="font-family:Verdana;font-size:7.5pt">Best design shoes</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://howtokodi.co/guide-to-kodi-and-streaming-movies-or-tv-shows/"><span style="font-family:Verdana;font-size:7.5pt">Download pics</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://jacketsformenguide.com/jacket-for-women/"><span style="font-family: Verdana;font-size:7.5pt">High Quality&nbsp;Videos</span></a></p> <p style="margin:0in;font-family:Calibri;font-size:11.0pt">&nbsp;</p> <p style="margin:0in;font-family:Calibri;font-size:11.0pt">&nbsp;</p>

    Answer by: admin on 2018-12-18 02:21:10
  • Question by: admin on 2018-12-18 02:21:09

    <p style="margin:0in"><a href="http://publicholidays2018.net/"><span style="font-family:Arial;font-size:9.0pt">Loads of games</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://publicholidays2018.net/2018-federal-holidays-usa-uk/"><span style="font-family:Arial;font-size:9.0pt">highest rating app</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/"><span style="font-family:Arial;font-size: 9.0pt">latest project design</span></a><span style="font-family:Calibri; font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-liturgico-catolico-2018/"><span style="font-family:Arial;font-size:9.0pt">calendar view mode</span></a><a href="http://calendario-2018.info/calendario-febrero-2018/"><span style="font-family:Arial;font-size:9.0pt">Garbage Pattern</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-janeiro-2018/"><span style="font-family:Arial;font-size:9.0pt">Web services</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-diciembre-2017/"><span style="font-family:Arial;font-size:9.0pt">None of these</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://calendario-2018.info/calendario-noviembre-2017/"><span style="font-family:Arial;font-size:9.0pt">Enterprenure of company</span></a><span style="font-family:Calibri;font-size:11.0pt">&nbsp;</span><a href="http://jacketsformenguide.com/"><span style="font-family:Arial; font-size:9.0pt">Start-up</span></a></p> <p style="margin:0in;font-family:Calibri;font-size:11.0pt">&nbsp;</p>

    Answer by: admin on 2018-12-18 02:21:09
  • Question by: admin on 2018-12-18 02:21:06

    According to the pin mappings there are two at D10 and D9, and another at D7 and D8 but i'm struggling with what values to put into SoftwareSerial serial1(x,y). Can you suggest values?

    Answer by: admin on 2018-12-18 02:21:06
  • Question by: admin on 2018-12-18 02:20:55

    Hi again, The sensor is not in pixmode. See listing with the setupsequence. No commands for Enter/Exit configmode are used. (I also use setupcode to force middle distance mode. Not included in listing. ) Two Lidarsensors connected to a MEGA 2560 But I have to use a slight delay between each setupcommand. It works fine now. So I&#39;m happy. But it would be interesting to know why I can&#39;t follow the procedure described in manual ? Serial.println (&quot;Initializing...&quot;); // Step 2: Initialize the data rate for the SoftwareSerial port Serial1.begin(TFMINI_BAUDRATE); Serial2.begin(TFMINI_BAUDRATE); // Step 3: Initialize the TF Mini sensor tfminiLeft.begin(&amp;Serial1); tfminiRight.begin(&amp;Serial2); pinMode(10, INPUT_PULLUP); // Halt measurement pinMode(13, INPUT_PULLUP); // Unit cm or mm delay(100); tfminiLeft.setStandardOutputMode(); delay(100); tfminiRight.setStandardOutputMode(); delay(100); // Step 4: Initialize single measurement mode with external trigger tfminiLeft.setSingleScanMode(); delay(100); tfminiRight.setSingleScanMode(); delay(100); tfminiRight.setUnitOfDistanceTomm(); delay(100); tfminiLeft.setUnitOfDistanceTomm(); delay(100); }

    Answer by: admin on 2018-12-18 02:20:55
  • Question by: admin on 2018-12-18 02:20:36

    Hi~Unfortunately, the measure range is 30cm--12m, it can not get an accurate date within 30cm.Regards

    Answer by: admin on 2018-12-18 02:20:36
  • Question by: admin on 2018-12-18 02:20:35

    HI there~One more question,did those boards you use have two hardware UART, because the baud rate is 115200,and the software UART can not support it.So please make sure the boards have two hardware UART.regards

    Answer by: admin on 2018-12-18 02:20:36
  • Question by: admin on 2018-12-18 02:20:28

    Hi there~ We've got your point. However here is the process-- you need to send the email to the ### order@seeed.cc ### for sample application. So, could you please copy your last reply to our email. Sorry for the inconvenience. Regards

    Answer by: admin on 2018-12-18 02:20:28
  • Question by: admin on 2018-12-18 02:20:26

    Hi, based on Benewake manual I did: (1) Get in configuration mode: 0x42 0x57 0x02 0x00 0x00 0x00 0x01 0x02 (2) Change output from 10ms to 1s 0x42 0x57 0x02 0x00 0xE8 0x03 0x00 0x07 (3) Exit from configuration mode 0x42 0x57 0x02 0x00 0x00 0x00 0x00 0x02 Best regards

    Answer by: admin on 2018-12-18 02:20:26