Back to Playground

Prayer Times

InkSalah

Turn reTerminal Sticky into an offline-first prayer-window display with native touch settings.

Author 作者
limengdu
0.1.1 Beta Learn More
InkSalah portrait interface on reTerminal Sticky showing the Asr prayer window and daily times in Dongguan

Step 1

Version and setup

Turn reTerminal Sticky into an offline-first prayer-window display with native touch settings.
  • Device connection: Connect reTerminal Sticky with a USB-C data cable and use desktop Chrome or Edge.
  • Clean installation: Accept the erase prompt when moving from another firmware so InkSalah can create a clean settings store.
  • Wi-Fi onboarding: On first boot, connect a phone to the Sticky-Salah setup network, choose a nearby Wi-Fi network, and complete the captive setup page.
  • Prayer settings: Confirm location and time zone on the device, then choose the calculation method, Asr school, per-time adjustments, reminder, and Qiyam display.

Step 2

Flash to device

Both modes verify and write the complete firmware package described by the selected manifest. Full flash erase only runs in the erase mode.

Flash device 0%

Connect your reTerminal Sticky with a USB data cable first.