Connect the board
Connect an ESP32 series XIAO and choose its port; the page detects the model and starts monitoring automatically.
Use desktop Chrome or Edge and open this page over HTTPS or localhost.
Trouble connecting?
1. Try another data-capable USB-C cable — some cables only carry power. 2. Hold BOOT while plugging in USB, or hold BOOT and tap RESET, to enter download mode and retry. 3. No driver is needed on macOS or Windows; if no port shows up, try another USB port or plug straight into the computer instead of a hub.