One-stop multi-factor environmental monitoring solutions for agricultural greenhouses
Too many IoT devices in greenhouse seem not smart enough and hard to manage?
One device, one solution for real-time monitoring of multi-factor environmental data in greenhouses to cut costs and improve yields.
Challenges
Greenhouse management requires timely and accurate measurement of temperature, humidity, light, carbon dioxide
and other basic environmental factors for plant growth in the greenhouse.With the development of IoT and sensor technology, a wide variety of environmental sensors suitable for use
in agricultural greenhouses have been developed. However, sensors from different manufacturers require a lot of manpower for deployment, management,
and subsequent maintenance.
Seeed's Solution
Key scenario: Seeed Studio’s One-stop multi-factor environmental monitoring solutions combines the advantages of simplicity, intelligence, compactness, stability, power saving and the most important cost advantage, which is very suitable for greenhouse greenhouses, providing accurate and stable solutions for greenhouse environmental monitoring, and greatly saving manpower cost, which will turn the ordinary greenhouses into intelligent greenhouses.
One device, complete all the greenhouses multi-element environmental monitoring:
The device supports multiple measurement elements such as temperature, humidity, dew point, light, carbon dioxide, barometric pressure, etc. It also supports up to 10 Modbus RTU RS485 sensor extensions, providing access to most sensor types on the market. If the communication signal is weak or lost, tens of thousands of sensor readings can be cached locally until communication is restored and then uploaded to the server or exported locally, greatly reducing the risk of data loss.
Features
One device supportsmultiple measurement elements such as temperature, humidity, dew point, light, carbon dioxide, barometric pressure,
Ready to use right out of the box, can access most types of sensors on the market,the device supports hanging or cradle mounting, allowing quick installation and deployment even for inexperienced users.
The device can withstand Harsh Environmentsin greenhouse environments. water-proof, robust and durable,
Ultralow power consumption, when power failure,the device can work normally for more than two weeks.
Combined with tracable data management and analysis system