Seeed Studio Announces Support for NVIDIA Jetson Orin Nano 2 — Expanding Scalable Physical AI and Robotics Ecosystem

Shenzhen, China – Aug. 25, 2026 – Seeed Studio, an NVIDIA Elite Partner, today announced support for the new NVIDIA Jetson Orin Nano 2, a new robotics computer for entry-level edge AI. NVIDIA’s latest entry-level edge AI platform. As AI models grow smaller and more capable, edge devices are increasingly becoming autonomous systems that interpret language, understand images, and act in real time. The Jetson Orin Nano 2 is built for these demands, and Seeed Studio is delivering carrier boards, hardware kits, and developer resources to accelerate product development.

A Major Leap for Entry-Level Edge AI

NVIDIA Jetson Orin Nano 2 delivers 78 TOPS of AI compute, 8GB of memory, and an 8-core ARM CPU. It achieves 2× the inference performance of the previous Orin Nano Super, thanks to improved Tensor Cores and higher memory bandwidth, while maintaining the same compact size. In 15W mode, it consumes 40% less power for equivalent performance. Supported by NVIDIA’s open software stack and rich AI ecosystem, it runs memory-efficient LLMs and VLMs – including NVIDIA Cosmos, Nemotron, Gemma 4, and Qwen 3. With over 3 million developers already using NVIDIA robotics tools, Seeed is also building around agentic robotics with Cosmos3-Edge, enabling closed-loop perception, real-time execution, and dynamic recovery for reBot arm.

Seeed’s Robotics and Edge AI Hardware Portfolio

As an NVIDIA Elite Partner, Seeed Studio offers a comprehensive lineup of carrier boards and industrial computing systems built across the NVIDIA Jetson platform — designed to serve the full spectrum of robotics and Physical AI applications, from entry-level prototyping to production-grade deployment.

What’s New in 2026 on the Seeed-Jetson Shelf

reComputer Robotics J50 Series

Industrial-grade edge AI platform for robotics and Physical AI, powered by NVIDIA Jetson AGX Orin 32/64GB with up to 275 TOPS. With CAN-FD, up to 5× Ethernet, and support for 8× GMSL2 cameras, it’s built for humanoids, AMRs, and multi-modal autonomous robots.

reComputer Rugged J40 Series

IP66-rated rugged edge AI computer with passive cooling, CAN-FD, PoE, 5G/GPS, and waterproof interfaces – ideal for outdoor, marine, and industrial inspection.

reComputer J601 Carrier Board

Compact board for NVIDIA Jetson Thor T4000 and T5000 modules, with CAN, EtherCAT, up to 4× 2.5/10GbE, and 8× GMSL cameras – enabling real-time robot control and high-bandwidth multimodal perception and decision-making for following actions.

reComputer Classic J50 Series (J5012)

NVIDIA Jetson AGX Orin 64GB developer platform with 275 TOPS, 10GbE, PCIe x16, 16-lane MIPI CSI-2, and full JetPack7.2 support – ideal for Physical AI prototyping and scalable deployment.

A Complete Developer Ecosystem and Tutorials

Beyond hardware, Seeed Studio provides a full ecosystem of resources to help developers build, deploy, and scale their Physical AI and robotics development:

Beginner Course — The reComputer’s NVIDIA Jetson course for beginners offers a structured learning path for developers new to the Jetson platform, covering setup, AI model deployment, and real-world project building: reComputer- NVIDIA Jetson-for-Beginners (GitHub)

Developer Tools — The Seeed-Jetson-DevelopTool on GitHub provides developers with essential tools for flashing, configuration, and deployment across Seeed’s NVIDIA Jetson product line: Seeed-Jetson-DevelopTool (GitHub)

Sim-to-Real VLA Curriculum with reBot Arm & NVIDIA Isaac — The latest Physical AI dev tutorial guiding developers from simulation environment setup and teleoperation data collection through VLA model training and real-world deployment. The hands-on curriculum covers URDF asset preparation, domain randomization, policy training, and sim-to-real transfer — bridging the gap between virtual training and physical robot execution. Learn more about this tutorial.

NVIDIA Jetson Orin Nano 2 Availability

The NVIDIA Jetson Orin Nano 2 module and developer kit will be available in the first half of 2027. Seeed Studio’s full portfolio of Jetson-based products — including the reComputer Robotics J50, reComputer Rugged J40, reComputer J601 carrier board, and reComputer Classic J50 series — is available now through the Seeed Studio website.

About Seeed Studio

Seeed Studio is a global provider of open hardware and AI solutions, empowering developers and enterprises to build and deploy edge AI, IoT, and robotics applications at scale. As an NVIDIA Elite Partner, Seeed Studio provides a comprehensive ecosystem of carrier boards, industrial computing systems, developer tools, and educational resources built on the NVIDIA Jetson Orin platform — from entry-level edge AI to production-grade robotics. For more information, visit seeedstudio.com about reComputer Jetson.

About Author

Calendar

August 2026
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930
31