PCBA Component Sourcing: From BOM to Assembly

Your BOM lists the components your board needs. Before those parts can go into production, their availability, price, order quantity, and delivery dates need to be checked. Any parts that cannot be purchased as specified need a solution.

Seeed Fusion handles component sourcing as part of its one-stop PCBA service, alongside PCB fabrication and assembly. Our supplier network and engineering support help your team address sourcing problems and reduce the work of finding suppliers, tracking orders, and sending parts to the factory.

📋Start with Clearly Identified Parts

When preparing your BOM, identify the exact component you need. A description such as “10 kΩ resistor” leaves several details open, including package size, tolerance, and power rating. The manufacturer part number (MPN) identifies the specific part, while the reference designator and quantity show where it belongs and how many are needed.

Enter the MPN in the part-number field. For Seeed’s own products, you can use the corresponding Seeed SKU. If a component cannot be matched, include a product link to help the purchasing team identify it. The link serves as a reference; it does not determine where the part will be purchased.

For file formats and required fields, see the PCBA File Preparation Checklist.

🌐How a Network of 600+ Suppliers Supports Your BOM

Seeed’s broader supply chain includes more than 600 qualified suppliers across electronics and product manufacturing. Fusion draws on this network and local component resources to find parts for your BOM and review pricing, available quantities, and lead times.

Sourcing a BOM yourself can involve several suppliers, each with different purchasing conditions. One may offer a suitable price but insufficient stock. Another may have the part available, but require a minimum order far above your project’s needs.

Our supplier network gives us more places to look when a source cannot meet your requirements. Fusion checks stock, pricing, minimum order quantities, and lead times for the parts in your BOM. We’ll contact you if a part is unavailable, requires buying more than you need, or has a long lead time.

🔎From Sourcing Challenges to Practical Support

The cost of sourcing includes more than the components themselves. Extra quantities, separate shipments, and time spent checking suppliers and following up on orders all add to the work.

Fusion looks for suitable purchasing options through its supplier network, checks incoming parts, and follows up on procurement issues. Your team has one point of contact for sourcing questions, without having to collect parts from different suppliers and forward them to the factory.

If you are still choosing components, check the Open Parts Library (OPL) for suitable options. Choosing locally available parts can reduce overseas purchasing and shipping delays. Reviewing availability during design also gives you more time to adjust your selection before the BOM is finalized.

🔎When a Part Is Unavailable

A part may be out of stock, discontinued, or available only with a lead time or minimum order quantity that does not suit your project. When we encounter a sourcing issue, we explain it so you can decide how to proceed.

If the specified part cannot be sourced, we will ask you to provide an alternative where possible. Your team knows the design requirements and any testing already completed. If you need help identifying an alternative, our engineers can offer guidance.

A replacement must suit the design as well as be available to buy. Package dimensions, pin assignments, and electrical characteristics need to be checked. Some changes may also require testing or design adjustments. Any proposed replacement requires your approval before it is used.

📷Sourcing Support in Practice: Poetry Camera

The Poetry Camera team needed to deliver 75 cameras within two weeks, but some specialized components had lead times beyond the project deadline. Fusion reviewed the BOM, proposed locally available alternatives, and coordinated production resources. The team completed the batch in 14 days.

The project shows how local sourcing resources and engineering support can help a team address component shortages under a tight deadline.

✅Get Your BOM Ready for Sourcing

A clear BOM helps us identify your parts and resolve purchasing questions sooner.

  • Use exact part numbers. Include the MPN, reference designators, and quantities. Use Seeed SKUs only for Seeed’s own products.
  • List the components you want Fusion to source and assemble. Leave out parts you plan to install yourself.
  • Add useful references. Include a product link for a part that cannot be matched, and flag any known availability issues or approved alternatives.

Ready to start? 👉Upload your Gerber files and BOM to get a Seeed Fusion PCBA quote.

About Author

Calendar

September 2026
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
282930