SenseCraft Robotics: Start Robot Arm Training with 1,000 Credits

Explore SenseCraft Robotics’ robot arm training workflow, usage-based GPU credits, and the 1,000-credit benefit available to new users.

Robot arm development often involves switching between different tools for device setup, calibration, data collection, model training, and validation. This fragmented workflow can increase preparation time and make experiments harder to manage.
SenseCraft Robotics brings these stages into one ready-to-use robot arm training platform. Users can prepare data on a desktop, run training and inference validation in the cloud, and track projects through a more connected workflow.
New users can also claim 1,000 credits on their first login. Each account can claim the benefit once, and the credits remain available for long-term use.

What Is SenseCraft Robotics?

SenseCraft Robotics is designed to support robot arm training projects through a guided workflow covering:
  • Device setup and calibration
  • Robot arm operation and data collection
  • Dataset preparation
  • Cloud-based model training
  • Training result review
  • Inference validation
By bringing these steps together, the platform reduces the need to manage separate tools and local training environments.
It is designed for several practical scenarios, including education and laboratory activities, R&D proof-of-concept projects, and early-stage integration validation.

Get 1,000 Credits as a New User

Every new SenseCraft Robotics account can claim 1,000 credits after its first login.
The benefit:
  • Is available once per account
  • Can be used for eligible cloud training and inference validation tasks
  • Remains valid for long-term use
These credits provide a starting point for exploring the platform, testing the workflow, and running an initial robot arm experiment before purchasing additional credit packs.

How the SenseCraft Robotics Credit System Works

SenseCraft Robotics uses a credit package plus actual GPU usage model for cloud training and inference validation.
  1. Configure Your Training Task

Before starting a task, users select the available GPU option and configure the required number of training steps.
  1. Review the Estimated Credit Usage

The platform estimates the required credits based on the selected GPU, training steps, and expected runtime. This allows users to review the expected consumption before the task begins.
  1. Pay According to Actual GPU Usage

Once the task starts, credits are settled according to the actual GPU running time. If the task uses fewer credits than estimated, the unused estimated credits are returned automatically.
This approach helps users understand and manage cloud computing costs more clearly.

When Credits Are Not Deducted

SenseCraft Robotics does not deduct credits when:
  • A task is waiting in the queue
  • A task fails to start
  • A platform-related error prevents the task from running
If the account balance becomes insufficient while a task is running, the task stops automatically without creating a negative balance.
Users can also review their recharge history, credit consumption, and abnormal return records in the platform.

Choose a Credit Package for Your Project

Users can purchase credit redemption packages through designated e-commerce channels. After receiving a redemption code, enter it in the SenseCraft Robotics desktop application to add the credits to your account.
Available package types are designed for different levels of usage:

Light Task Package

Suitable for personal testing, classroom exercises, and small-scale parameter adjustments.

Project Training Package

Suitable for repeated training, inference validation, and multiple rounds of experimentation.

Professional Training Package

Suitable for teams and projects that require more frequent or long-term use.
Specific package values and purchasing information should be checked through the current official sales channel.

A More Transparent Way to Manage Robot Arm Training

The credit system is designed to make cloud resource usage easier to understand:
  • Estimated consumption is shown before training
  • Final settlement is based on actual GPU usage
  • Unused estimated credits are returned
  • Queue time and failed starts do not consume credits
  • Recharge, consumption, and return records can be reviewed
Combined with the guided robot arm training workflow, this gives educators, developers, and researchers a clearer way to plan and manage experiments.

Start Your First Robot Arm Training Project

SenseCraft Robotics provides a connected workflow for preparing data, training models in the cloud, and validating results without requiring users to build and maintain a high-performance local training environment.
New users can begin by claiming 1,000 credits on their first login.

Frequently Asked Questions

How many credits can a new user claim?

New users can claim 1,000 credits. Each account can claim the benefit once.

Do the new-user credits expire?

The 1,000 credits remain available for long-term use.

Are credits deducted while a task is waiting?

No. Tasks waiting in the queue do not consume credits.

What happens if a training task uses fewer credits than estimated?

Credits are settled according to actual GPU usage time. Any unused estimated credits are returned automatically.

What happens if my balance runs out?

The running task stops automatically, and the account does not enter a negative balance.

About Author

Calendar

September 2026
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
282930