Mobile Robot Full-Stack Development in Practice: An Open-Source Course from Jetson to Autonomous Robotics

If you are learning mobile robotics, ROS 2, Jetson, SLAM, AI vision, or robotic manipulation, it is easy to end up with a collection of separate tutorials and algorithms without a clear picture of how they work together.

Mobile Robot Full-Stack Development Course banner featuring a mobile robot powered by Jetson, with callouts for RGB camera, multi-sensor fusion, mobile chassis, and ROS 2, plus a development roadmap covering visual perception, LiDAR sensing, SLAM mapping, path planning, semantic understanding, grasping and manipulation, and deployment.

Mobile Robot Full-Stack Development in Practice is an open-source, hands-on course from Seeed Studio designed to provide that complete picture.

Built around the reComputer Robotics J501 with NVIDIA Jetson AGX Orin, the course takes developers step by step from hardware and development environment setup to visual perception, multi-sensor fusion, SLAM, autonomous navigation, semantic understanding, robotic manipulation, and deployment.

The idea is simple:

Don’t just learn individual robotics algorithms. Learn how to connect them and build a real robotics system.

⭐ Start with the open-source course on GitHub

reComputer Robotics J501 Series edge AI computing platform for mobile robotics and embodied AI development.

The reComputer Robotics J501 Series is an edge AI computing platform designed for mobile robotics and embodied AI development. Powered by NVIDIA Jetson AGX Orin, it combines high-performance AI computing with a rich set of robotics interfaces. From visual perception and multi-sensor fusion to SLAM, navigation, and AI inference, the J501 Series can serve as the robot’s core “brain,” helping developers build complete robotic systems step by step—from interface integration to real-world applications.

Main Capabilities:

  • High-Performance AI Computing: Up to NVIDIA Jetson AGX Orin 64GB, delivering up to 275 TOPS
  • Rich Robotics Interfaces: USB, Ethernet, CAN, RS-232/422/485, I²C, SPI, and more
  • Multi-Sensor Integration: Supports LiDAR, 3D cameras, IMU, GNSS, and other sensors for multi-source data fusion
  • Vision AI Support: Supports up to 8 GMSL2 cameras, suitable for applications such as BEV, SLAM, and Occupancy Grid

🛒 Explore the reComputer Robotics J501 Series

Mobile Robot Course roadmap diagram showing the progression from M1 Platform and Environment through M2 Vision System and M3 Multi-Sensor Fusion, leading to M4 AI Perception, M5 SLAM and Reconstruction, M6 Autonomous Navigation, M7 Semantic Navigation, M8 Active Vision, M9 Robotic Arm Manipulation, M10 Integrated Projects, and M11 Engineering Deployment.

What Will You Learn?

The course follows the way a mobile robot gradually gains new capabilities.

It starts with reComputer J501, JetPack, Docker, and ROS 2, establishing the computing and software foundation. From there, cameras and other sensors are introduced so the robot can begin collecting information from the physical world.

The next stages move into AI vision, LiDAR, sensor fusion, and SLAM, covering technologies such as YOLO, 6D pose estimation, ORB-SLAM3, Fast-LIO, R3LIVE, and 3DGS.

Once the robot can perceive its environment and understand its position, the course moves into Nav2, path planning, dynamic obstacle avoidance, and Vision-Language Navigation (VLN).

The final stages bring in active vision and robotic manipulation, using technologies such as MoveIt 2, hand-eye calibration, and GraspNet, before moving toward model optimization and deployment with ONNX, TensorRT, DeepStream, monitoring, and OTA.

In other words, the course gradually connects:

Perception → Spatial Understanding → Navigation → Semantic Understanding → Manipulation → Deployment

Each stage builds on what came before, so the focus stays on understanding how the pieces fit together inside a real robot.

Start Small, Build Step by Step

You don’t need to build a fully equipped robot before starting.

The early modules can begin with a J501 and a single camera. As you progress, you can gradually add the mobile chassis, LiDAR, IMU, GNSS, PTZ, and robotic arm.

This makes it possible to start with a manageable system and expand it as your understanding grows.

First, get the platform running.

Then make the robot see.

Add sensors and build its spatial understanding.

Teach it to navigate.

Then give it the ability to interact with the physical world.

This step-by-step approach is one of the core ideas behind the course.

Who Is This Course For?

The course is designed for developers and learners at different stages of their robotics journey.

ROS 2 and robotics beginners can use the structured roadmap to build their foundation step by step.

AI, computer vision, and edge computing developers can explore how existing AI skills translate into real-world robotic systems.

AMR, AGV, inspection, and service robot developers can use individual modules as references for perception, navigation, manipulation, and deployment.

Students, educators, and robotics labs can use the open-source project as a practical foundation for robotics learning, experiments, and research.

Basic knowledge of Linux, Python, Git, and linear algebra is recommended. ROS 2, Docker, and Jetson fundamentals are introduced progressively throughout the course.

An Open-Source Course That Grows with the Community

Illustration of the “Mobile Robot Full-Stack Development” open-source course, showing a mobile robot and a step-by-step development workflow from visual perception and LiDAR sensing to SLAM mapping, path planning, semantic understanding, grasping and manipulation, and deployment, with Jetson Edge AI, ROS 2, and open-source development elements.

This is not intended to be a course that is published once and then left unchanged.

Mobile Robot Full-Stack Development in Practice is being developed as an fully open-source project, with course materials and practical resources released progressively.

The project will include:

  • Course documentation and experiments
  • ROS 2 source code and configurations
  • Dockerfiles and installation scripts
  • Deployment and testing tools
  • Integrated project code
  • Demo resources and troubleshooting notes

The current release covers the foundational modules, with additional modules continuing to be developed and released according to the roadmap.

Follow the latest course updates on GitHub

And because the project is open source, developers can do more than follow the lessons.

Found a problem? Open an Issue.

Built something interesting? Share it.

Improved the code? Contribute it.

Using different hardware? Show us how you made it work.

The goal is to make the course more useful with every experiment, contribution, and piece of feedback from the community.

Learn, Build & Create with Seeed Studio

We also want the learning process to be interactive.

As you work through the course, you can earn points through learning check-ins, hands-on practice, project sharing, and community contributions.

Complete a practical task, share your Demo, or help another developer solve a problem — and you can accumulate points along the way.

Redeem Your Points

PointsReward
100Seeed Custom Tumbler
150Manual Screwdriver Set
300Electric Screwdriver
550SO-ARM101 Robotic Arm Kit

Outstanding projects may also be selected for community showcases.

The point system is not simply about completing lessons. It is designed to encourage developers to build something of their own, share what they learn, and contribute back to the community.

Learn → Build → Share → Contribute

Start Building Your Mobile Robot

You don’t need to understand the entire robotics stack before you begin.

Start with a Jetson.

Connect a camera.

Run ROS 2.

Make the robot see.

Add LiDAR.

Build a map.

Plan a path.

Add semantic understanding.

Then connect perception to manipulation and deployment.

One step at a time. One capability at a time. Build them into a complete robotics system.

If you are exploring mobile robot development, Jetson robotics, ROS 2, SLAM, autonomous navigation, or embodied AI, we invite you to learn with us, build your own projects, and help shape the course as it grows.

⭐ Star the Mobile Robot Full-Stack Development project on GitHub

Build it. Share it. Improve it. Let’s build robots together. 🤖

Join the Robotics Community

Building robots is more fun when you don’t have to build alone.

If you are learning mobile robotics, Jetson, ROS 2, AI vision, SLAM, navigation, or robotic manipulation, join the Seeed Studio robotics community to share your projects, exchange ideas, ask questions, and learn from other developers.

🌐 Join us here:

Build your robot, share what you learn, and let’s make the open-source robotics ecosystem better together. 🤖

About Author

Calendar

September 2026
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
282930