Product Details
Wiki & Learn
Reviews
Download PDF

Description


Grove Starter Kit for LaunchPad is a co-branded quick starter kit for Texas Instruments LaunchPad Development Kits. This kit carries one Grove Base BoosterPack and 10 carefully selected Groves modules. It enables users of the Texas Instruments Launchpad to rapidly prototype and hack together fun microcontroller-based projects. Grove Base BoosterPack is an expansion module that can plug on to the various LaunchPad development kits that TI offers. On the BoosterPack, there are 13 Grove connects, which feature a 4-pin standardized interface for enabling you to easily connect with Seeed's huge offering of Grove modules!


Grove Starter Kit for LaunchPad makes it an enjoyable experience to dive into the world of electronics. The kit also includes 11 interesting examples that will guide you through on how to work with the TI LaunchPad, as well as 2 additional advanced demos that can inspire you for further project building.


NOTE

This Starter Kit is not compatiable with CC3200-LAUNCHXL, if your Launchpad is this version, please don't buy the Grove Starter Kit. 


11 Projects and 2 Cool Demos

  • Getting Started - (Blinking LED)

  • Playing Music - (Buzzer)

  • Control the Electric - (Relays)

  • Display- (4-Digital Display)

  • Potentiometer - (Rotary Angle Sensor)

  • Sensing the Light - (Light Sensor)

  • Hearing - (Sound Sensor)

  • Is anybody there- (PIR Sensor)

  • Taking care of your plants- (Moisture Sensor)

  • Sensing the Distance - (Ultrasonic Ranger Sensor)

  • Feeling the Environments - (Temperature Humidity Sensor)


NOTE: 

You can find all the projects in the wiki of every corresponding grove modules.


PROJECT ONE: Intelligent Tulip Water Device

WHAT WE’VE GOT HERE

Decorate your room with tulips, and make your home a pleasant space. But what if I am too busy to take care of the lovely tulips? Now imagine your tulips will remind us when they are thirsty! We can set up a “conversation” with the help of Moisture Sensor, which can detect the electric resistance of the soil, and thus can show us the soil moisture by the 4-Digital-Display.

When the moisture is below the value you have set, the buzzer will respond in a blast of sound of “DEE DEE”, reminding you of their need of water. At this moment, the Relay will initiate the motor to water your Tulips.

THE CIRCUIT

List

  • Grove - Moisture Sensor

  • Grove - Buzzer

  • Grove - Relay

  • Grove - 4-Digital-Display

  • Grove - Base-BoosterPack x 1

  • LaunchPad MSP430G2 x 1

Result

When the soil turns dry and its moisture index is below the value you have set, the Buzzer will ring and the Relay will initiate the motor automatically until the moisture of soil reaches the parameter you set in the device.


PROJECT TWO: Intelligent Lamp

WHAT WE’VE GOT HERE

Have you ever had this idea? When someone gets closer or the night falls, the lamp of your room will turn on automatically. When someone leaves or the day dawns, it will turn off. Now we can work out the magic by Grove PIR sensor and Grove Relay.

THE CIRCUIT

List

  • Grove - Light Sensor

  • Grove - Relay

  • Grove - PIR sensor

  • Grove - Base-BoosterPack x 1

  • LaunchPad MSP430G2 x 1

Result

When someone gets closer, the Relay will interact with the “lamp” on LaunchPad for 10 seconds, and at the same time the light will be turned on. When it becomes darker, the device works in a similar way.


SOFTWARE ENVIRONMENT

Energia is an open-source and community-driven development environment for the TI LaunchPad development kits. It is based on the popular Wiring framework, which offers a collection of simple functions and APIs for programming a microcontroller easily. Energia support is available on many of TI’s LaunchPad development kits, featuring the MSP430, TM4C, C2000, CC3200 and other microcontroller devices.



Certification

HSCODE9023009000
USHSCODE9023000000
UPC841454107262
EUHSCODE9023001000
COOCHINA

Technical Details

Technical details

Dimensions0mm x0mm x0mm
WeightG.W 287g
BatteryExclude

Part List

Part List

Grove - Ultrasonic Ranger1
Grove - Light Sensor1
Grove - Buzzer1
Grove - Temperature&Humidity Sensor Pro1
Grove - 4-Digit Display 1
Grove - Relay1
Grove - PIR Motion Sensor 1
Grove - Moisture Sensor1
Grove-Sound Sensor1
Grove - Rotary Angle Sensor1
Grove Base BoosterPack1
Guidebook1

Grove Starter Kit for LaunchPad

SKU 110020004
Co-branded kit with Texas Instruments Compatible with various LaunchPad development kits Expansion board provides up to 13 Grove ports 10 specially selected Grove modules Detailed guidebook with 11 getting-started examples
USD$64.90
Discontinued
  • Free Insurance Included On Us
  • Flexible Payments with PayPal Pay Later
  • Avoid Import Fees: Ship Tax-Free from Local Warehouses
  • 1 on 1 Support | 12-Month Warranty | 30-Day Return Policy