Join the TinyML Challenge 2022 to Create Smart Weather Stations to Win $8000 in Prizes

Hey community,

A piece of exciting news to share is that Seeed Studio is honored and happy to join the tinyML Challenge, organized by United Nations’ ITU in conjunction with the tinyML Foundation, as a partner together with tinyMLEdu, International Centre for Theoretical Physics, and Edge Impulse. The first edition of the tinyML Challenge, which is also one of the AI for Good events, aims to create a low-cost, low-power, reliable, accurate, easy to install and maintain weather station, with no mechanical moving parts for measuring all weather conditions with a focus on rain and wind, based on TinyML, that can be deployed locally. This weather station could be deployed on a farm, for example, to provide local conditions and assist farmers in deciding when to plant crops.

Timeline of the tinyML Challenge (Smart Weather Station)

Prize of the tinyML Challenge (Smart Weather Station)

  • 1st place prize: $3,000
  • 2nd place prize: $2,000
  • 3rd place prize: $1,000

Being a partner of the tinyML Challenge, we’ll sponsor a SenseCAP S1000 10-in-1 Compact Weather Sensor with CO2 Measurement as an additional prize to the 1st place winning team. It’s a compact powerful and precise CO2 emission-ready weather station valued at $2,199. It measures air temperature, relative humidity, barometric pressure, light intensity, rainfall (optical), PM2.5, PM10, wind speed, wind direction (ultrasonic), and CO2. It is ideal for applications for carbon and environment monitoring. More details about the prize product can be found here.

Moreover, in order to support all challenge participants to develop a fully functioning rugged, and cost-effective weather station, we’re also offering all of our TinyML-native products at a special discount (20% off for all products listed on this landing page). In this way, you can use these Seeed products to build your smart weather station solution to detect all weather parameters including TPH (temperature, pressure, and humidity), wind, and rain. Click here to explore what possible smart weather station you can build with Seeed’s TinyML-native products (Please use the coupon code “AI4GOOD” to get your project ideas supported.).

Getting excited about the tinyML Challenge? Click here to join the challenge! After registration, you can either create a project team or join the existing teams to work on your smart weather station solution!

Note: Create an account on ITU and then log in to the account to get the full description and register to the tinyML Challenge (Smart Weather Station).

Some Useful Links:
1. On June 29, the tinyML Foundation also hosted a talk to introduce the 2022 tinyML Challenge. If you’d love to learn more about how you can participate in this Challenge, click here to watch the recap video.

2. Want to get more inspiration for your smart weather station project? Click here to explore our Project Hub on Hackster, where you can find tons of project tutorials!

3. Still new to tinyML technology? Our team has published a 46-page PDF tutorial on No-Code Programming to Get Started with TinyML and a 64-page PDF tutorial on TinyML with Wio Terminal Using Edge Impulse. Feel free to download and start your journey with tinyML.


As always, we can’t wait to see what you make with Seeed tinyML products. Shoot us a tweet @seeedstudio, or let us know on LinkedIn, Discord, or publish your project on our Project Hub on Hackster. Please be safe out there, be kind to one another, and we’ll see you next time!

About Author

Calendar

July 2022
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031