Seeed Studio Launches reBot Arm B601: A Fully Open-Source Robotic Arm Built for Physical AI

Physical AI enables autonomous systems to perceive, reason, and act within complex real-world environments. Yet for developers, progress will be slowed by fragmented hardware ecosystems and limited transparency.  In practice, bringing physical AI to life on a robotic arm remains challenging—hardware selection, extensive parameter tuning, and navigating supply chain complexity.

That’s the whole point. So, we launched reBot Arm B601, a fully open-source robotic arm designed to bring more structure and clarity into this process. Built as a developer-first platform, reBot emphasizes standardized design, a transparent BOM, and a tightly integrated software stack, enabling developers to move from assembly to data collection and algorithm development in a more predictable, streamlined workflow—bridging research-grade capability with real-world usability. More than just hardware, it delivers a complete, ready-to-use stack for embodied AI development.

Positioning it as the “Getting Started Robot Kit of Physical AI”—fast to start, reliable to run, and open for innovation.

Where Did We Start This Project?

Over the past year, our AI robotics team has traveled globally, co-hosting hackathons with partners like NVIDIA and Hugging Face, building alongside developers exploring embodied AI in the real world. While we saw rapid innovation—from robotic arms playing music to performing complex tasks—we consistently heard the same challenge:

  • existing solutions forced a trade-off between precision, affordability, and openness.
  • Low-cost arms lacked stability,
  • High-performance systems were prohibitively expensive,
  • Truly open platforms were rare.

After exploring existing projects and industry options, we have not found a clear answer.

So, we decided to build one.

Built for Developers: Open, Accessible, and Reproducible

The reBot Arm B601 is part of Seeed Studio’s broader effort to democratize robotics hardware.

The GitHub project provides:

  • Complete CAD files and mechanical design
  • Full Bill of Materials (BOM)
  • Assembly guides and tutorials
  • Software SDKs and integration examples

With a target build cost of under $1,000, the B601 significantly lowers the cost barrier compared to traditional industrial robotic arms, making it accessible to:

  • Robotics researchers
  • AI developers
  • Educators and students
  • Maker communities
  • Robot solution integration

Designed for the Next Generation of Embodied AI

Unlike traditional industrial robotic arms that rely on fixed trajectories, embodied AI systems require adaptability, perception, and learning in dynamic environments. The reBot Arm B601 is engineered with this paradigm in mind.

The platform features a 6+1 Degree-of-Freedom (DoF) architecture, enabling dexterous manipulation across a wide range of tasks—from pick-and-place to human-robot interaction workflows.

With a reach of over 767 mm and a rated payload of up to 1.5 kg, the B601 is capable of handling meaningful real-world workloads while maintaining a compact desktop footprint.

Its repeatability of ±0.2 mm ensures consistent precision, making it suitable for both research experiments and light industrial prototyping scenarios.

High-Performance Actuation with Physical Transparency

At the core of the reBot Arm B601 lies a high-torque brushless actuator system, designed to deliver both strength and controllability.

Unlike conventional servo-based educational arms, the B601 integrates advanced motor solutions (e.g., DAMIAO / RobStride Dynamics – compatible systems) to achieve:

  • Smooth motion control with reduced backlash
  • Enhanced torque output for stable manipulation
  • Improved physical transparency for force-sensitive applications

This architecture enables advanced capabilities such as:

  • Gravity compensation
  • Force-aware manipulation
  • Dynamic trajectory execution

The system has been validated through extensive internal testing, including 24/7 endurance runs, overload conditions, and stability verification, ensuring robustness for continuous development cycles.

Full-Stack Software Integration for Robotics & AI

A key differentiator of the reBot Arm B601 is its deep integration with modern robotics and AI frameworks, allowing developers to move seamlessly from simulation to deployment.

Native Ecosystem Support

The platform supports a comprehensive robotics software stack, including:

  • ROS 1 / ROS 2 (Humble) for motion control and system orchestration
  • MoveIt for motion planning
  • NVIDIA Isaac Sim for physics-based simulation and digital twin workflows
  • Hugging Face LeRobot for learning-based manipulation pipelines
  • Pinocchio for forward/inverse kinematics and dynamics modeling
  • Python API for rapid prototyping and scripting

This enables developers to:

  • Simulate robotic tasks before hardware deployment
  • Train policies using imitation learning or reinforcement learning
  • Deploy perception-action loops with real-time feedback

From Simulation to Real-World Deployment

The reBot Arm B601 is designed to support the full development lifecycle of embodied AI:

  • Modeling & Simulation: Build and validate algorithms in NVIDIA Isaac Sim with accurate physics and collision modeling
  • Algorithm Development: Leverage ROS1/ROS2/Pinocchio/LeRobot for robot control and model training pipeline
  • Real-World Execution: Deploy pre-trained policies directly onto the physical arm with consistent behavior

This seamless workflow significantly reduces iteration cycles and lowers the barrier for robotics experimentation.

Modular Design for Flexible Expansion

To support diverse use cases, the B601 adopts a modular hardware architecture

  • Interchangeable end-effectors (grippers, custom tools)
  • Force-sensing gripper options for precision manipulation
  • Enrich teleoperation methods of leader+follower, and VR control on the way
  • Expandable interfaces for vision systems and sensors
  • Support for multi-payload scenarios (50g–750g typical working range)

You can adapt the platform for:

  • Adaptive pick-and-place systems
  • Human-robot interaction
  • Teleoperation and remote control
  • Research in manipulation and model verification, and more!

Accelerating Embodied AI Innovation

We envision reBot Arm B601 as enabling developers to move faster from idea to implementation in embodied AI. By combining high-performance hardware, full-stack software compatibility, and open modular design, the reBot serves as a foundational platform for building the next generation of intelligent machines that can perceive, learn, and act in the real world much more easily than ever.

Get Started Now

The reBot Arm B601 is now available with full documentation, tutorials, and source files on GitHub. You can also buy the whole BOM kit at the Seeed Studio store, or get the assembled kit.

From unboxing to learning—within minutes.

We’re glad to invite more developers to join this journey, to explore, build, and contribute to the robotics ecosystem—pushing the boundaries of what embodied AI can achieve, testing its limitations, identifying appropriate application scenarios, and making AI robotics much easier to use and further develop.


Seeed Studio AI Robotics Ecosystem

Seeed Studio has been the AI hardware partner for global developers since 2008, providing sensing, networking, and edge AI hardware.  Seeed AI Robotics team is dedicated to making physical AI accessible to everyone. By offering a comprehensive hardware portfolio, spanning from sensing and perception to robust computation and control. Through deep community collaboration and open-source integration, Seeed is empowering developers to scale embodied AI from prototype to deployment.

About Author

Calendar

April 2026
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
27282930