Elctronic Brick :Analog and Digital
Analog signals are continuous where digital signals are discrete. Analog signals are continuously varying where
Analog signals are continuous where digital signals are discrete. Analog signals are continuously varying where
Have you ever played Toy brick when you were kids? It is the most common
We finally got those chips and produced our new seeeduino board: seeeduino V328. It kept
Rainbowduino isn’t only used to drive the LED matrix but also can be used to
I should post this message through Twitter but seems like it was blocked by GOV.
When time comes to 8th july,2009, the anniversary of seeedstudio has arrived. It is a
The Rainbowduino have not the USB connector and cannot use the Arduino IDE to program
The Seeeduino Mega is as small as the seeeduino which is about 2/3 of the
The RTC module is a conventional module in many circuits. You can used it to
As the Rainbowduino sell like hot cakes, more and more Email comes to ask how
After several times correcting, now the Rainbowduino V1.11 is on sale. In the hardware world,