Huge! Waterproof and dustproof button!
These buttons are from our OEM order, they are mistakenly produced as non-ROHS model thus
These buttons are from our OEM order, they are mistakenly produced as non-ROHS model thus
UartSB V2.1 adds USB connectivity to your project easily. It’s pluggable to computer USB port
If you want to remove some solder,here is a tool you should have one-L135A Desoldering pump ,
Multiple Usage Programing Adapter Features: ● Compatible with AVR STK200 programming interface ● Compatible with Altera
This is a deluxe pack for Arduino users; it includes Seeeduino, basic components and prototyping platform, various Input and sensors, visual and
Funnel I/O (FIO) is an Arduino compatible board designed by Shigeru Kobayashi, based on
Since many developers asked about if Seeeduino is RoHS compliant, we replaced all the components
2008 is a very special year for all Chinese people, not just because of the Beijing Olympic Games. On May 12th, a huge disaster came and took thousands of people’s life in Sichuan. Many countries lent their helping hand, just like Michael Jackson songs: We are the one. On the last day of 2008, we would state that we are proud to contribute to open source hardware, participate in the community of generosity and inspirations. Thanks to all the friends who supported Seeed Studio, your supporting made us grown. ^^ 2009 is about to come, we will do our best in supporting open source hardware development. On the occasion of the New Year, Please allow us to congratulate you on the arrival of the New Year and to extend to you all our best wishes for your perfect health, your career greater success and lasting prosperity. -Fan on behalf of Seeed Studio
>> Click to Keep touched. ^^
Last month of 2009! Almost time to party and acting lazy! Here are some note
Finally, 2008 is about to end. Forget the many terrible events, a fresh new year
Intro UartSB adds USB connectivity to your project easily. It’s pluggable to computer USB port