TPGmini v2: A Tiny AR Wearable Companion Powered by XIAO ESP32S3 Sense
In a world where wearables often prioritize form over function, TPGmini v2 is redefining what
In a world where wearables often prioritize form over function, TPGmini v2 is redefining what
In recent years, artificial intelligence has transformed various industries, with vision AI being at the
日本の広大で高度に専門化された電気機器産業において、安全は最優先事項です。毎日、数千件の設置作業が実施され、変圧器からリレーコイルまで、工場、建物、インフラストラクチャーにわたる電力の安定した供給が確保されています。しかし、これらの設置作業において最も基本的で重要な作業の一つが、しばしば見落とされています:正しい配線極性です。 数十年にわたり、パナソニック(旧ナショナル)が製造した独自のアナログブザー装置は、日本の電気分野で静かに定番品となっていた。誤配線検出を目的としたものではなかったが、3Vの開放電圧と20mAの短絡電流、そしてアナログ発振回路の組み合わせにより、変圧器やリレーコイルのインピーダンス差を検知することが可能となった。電池駆動でシンプル、かつ精密機器にも安全なこの装置は、全国の技術者や電気技師にとって欠かせない存在となった。 しかし2010年代に入り、パナソニックはこの装置の製造を中止したため、市場には適切な代替品が存在しなくなった。新型のデジタルテスターは中核となる検出能力を欠いていた。抵抗値のしきい値は測定できたものの、複雑な電気部品における誘導性の誤配線を検出することはできなかった。明らかだった:このレガシーデバイスは生まれ変わる必要があった——21世紀にふさわしい改良を加えて。 専門知識を駆使したゼロからのハイブリッド再設計 そのギャップを埋めるため、日本のエンジニアチームはベテランの回路設計者である下間憲行氏(通称「居酒屋ガレージ」)と協力しました。下間氏は、日本において回路設計とプログラミングの専門家として知られ、数十年にわたり『トランジスタ・テクノロジー』誌(https://toragi.cqpub.co.jp/)に技術記事を寄稿し、日本のエンジニアの間で広く読まれています。現代のマイクロコントローラーベースの導通テスターを基盤に、彼らは失われたACベースの検出原理を再導入する作業を進めました。発振回路を統合し、さまざまな周波数をテストすることで、再設計されたデバイスは、現代のアナログメーターや小型リレーコイルのような低インダクタンス部品でも検出可能になりました。 結果:コンパクトでバッテリー駆動のAC/DCハイブリッドテスター。端子短絡時に自動で起動し、現場での使用に安全で、日常の点検に非常に効率的です。 オリジナルのブザーの独自の能力が、AC発振によるインピーダンス検出にあることを認識したチームは、下間氏にACとDCの両モードを組み合わせたハイブリッドデバイスを開発するよう依頼しました。一連の迅速な設計反復を経て、彼は発振回路を追加し、周波数を1kHzから5kHzまで調整しました。これにより、これまで検出できなかった部品の検出が可能になりました。 このデバイスは巧妙に効率化されたスリープモード設計💤を採用し、テスト端子が短絡されると⚡自動的に起動します。さらに180秒のタイマー⏱️を搭載し、スリープ状態へ復帰するため電源スイッチ🔌が不要。スリープ時の消費電流は さらに180秒のタイマー⏱️を搭載し、電源スイッチ🔌が不要なままスリープ状態へ復帰。2本の単三電池で駆動するスリープ電流は1μA未満のため、放置されても数週間持続可能。これにより新型ブザーは、先代機が愛された現場での実用性を確実に継承している。 👉 詳細を見る・注文する 試作から量産へ — Seeed Fusion
What is Everything Presence Lite? Designed and developed by Everything Smart Home and manufactured with
At Seeed Studio, we’re constantly pushing the boundaries of what’s possible with edge computing. The
XIAO Soil Moisture Sensor is a capacitive soil moisture sensor built for smarter gardening. Powerd by XIAO ESP32-C6, it integrates seamlessly with Home Assistant.
As long as your PCBA design includes any LoRa module developed by Seeed, you’ll receive an exclusive 30% discount on Fusion PCBA services, and the lowest global prices for LoRa modules.
Hey community, we’re super excited to share something special with you today – our brand
Introducing CM5 MINIMA R3, a compact and versatile carrier board built around the latest Raspberry Pi Compute Module (CM5) and designed for developers, makers and professionals.
We’re thrilled to introduce the Vibration Anomaly Detection Kit for XIAO ESP32-S3—a compact, efficient, and
On July 23, 2025, the classroom of St. Augustine’s Girls Higher Secondary School transformed into
We’re excited to introduce the newest member of the XIAO nRF family — XIAO nRF54L15 (Sense), powered by Nordic Semiconductor’s nRF54L15 SoC. With a 128 MHz Arm Cortex-M33 core,1.5 MB NVM, ultra-low-power performance, and multi-protocol connectivity (including BLE 6.0, Matter, Thread, Zigbee, and Amazon Sidewalk), this compact board brings next-level performance to your embedded and IoT applications.