How to Build a Real-Time AI Voice Assistant with SenseCAP Watcher and OpenAI
By Liyan Gong 6 months agoThis project first published by our engineer Mengdu on Hackster, is shared here to help more people discover how simple it can be to build a real-time LLM voice chat.
The Internet of Things (IoT) has brought us incredible possibilities, and when combined with advancements in artificial intelligence, the potential becomes even more exciting. Meet the SenseCAP Watcher, a compact and powerful device powered by the ESP32-S3 MCU. Recently, I experimented with the integration of the latest OpenAI API (as outlined in Espressif’s OpenAI API documentation) to build a real-time voice chat demo.
This blog will walk you through this experience—how I set up the SenseCAP Watcher, integrated voice input and output, and created a conversational assistant that feels natural and intuitive. Let’s dive in!
What is the SenseCAP Watcher?
The SenseCAP Watcher is part of the SenseCAP family of IoT devices. SenseCAP Watcher is built on ESP32S3, incorporating a Himax WiseEye2 HX6538 AI chip with Arm Cortex-M55 & Ethos-U55, excelling in image and vector data processing. Equipped with a camera, microphone, speaker, SenseCAP Watcher can see, hear, talk. Plus, with LLM-enabled SenseCraft suite, SenseCAP Watcher understands your commands, perceives its surroundings, and triggers actions accordingly. It features:
- ESP32-S3 MCU: A dual-core processor with built-in AI acceleration and low-power capabilities.
- Onboard Microphone: Perfect for audio input, such as voice commands or speech recognition.
- Wi-Fi and Bluetooth: Provides seamless connectivity to the cloud and other devices.
- Compact Design: Designed for IoT applications with minimal space requirements.
Its powerful ESP32-S3 chip makes it ideal for AI applications, especially those that require real-time processing, such as voice recognition and natural language understanding.
The Idea: Real-Time Voice Chat with OpenAI
The goal of this project was to create a real-time voice assistant using the SenseCAP Watcher, leveraging the OpenAI API to handle conversational interactions. With the latest updates to Espressif’s esp-iot-solution, integrating OpenAI’s capabilities into ESP32-based devices has become remarkably straightforward.
The workflow for this demo is as follows:
1. Use the SenseCAP Watcher microphone to capture voice input.
2. Send the audio to the OpenAI API for conversational processing.
3. Receive and process the API response, then convert the text back to speech for real-time audio output.
Step-by-Step: Building the Voice Chat Demo
Step 1: Setting Up the Development Environment
To get started, I set up the development environment for the ESP32-S3:
1. Install ESP-IDF v5.2.1: Download and install the version 5.2.1 of the ESP-IDF from Espressif’s official website. This is the SDK needed to program ESP32-based devices.
2. Clone Watcher Firmware Code: The firmware code for the SenseCAP Watcher real-time OpenAI integration can be found at the following GitHub repository:SenseCAP-Watcher-Firmware/examples/openai-realtime
This repository contains example code for creating a real-time voice chat application using the SenseCAP Watcher, ESP32-S3, and OpenAI API.
3. Hardware Setup:
- Connect the SenseCAP Watcher to your computer using a USB-C cable.
- Ensure the device is detected by your system and ready for programming.
Step 2: Integrating the OpenAI API
Configure Wi-Fi
To set up the Wi-Fi connection, use the wifi_sta command:
wifi_sta -s <SSID> -p <PASSWORD>
Replace <SSID> with your Wi-Fi network name.
Replace <PASSWORD> with your Wi-Fi password.
Configure OpenAI API Key
To set up the OpenAI API key, use the openai_api command:
openai_api -k <API_KEY>
Replace <API_KEY> with your OpenAI API key.
Once these configurations are complete, the SenseCAP Watcher will be ready to connect to the internet and interact with the OpenAI API for real-time applications.
Step 3: Running the Demo
With all components in place, I ran the demo:
1. Start a Conversation: I spoke into the SenseCAP Watcher, giving it a prompt like, “When did the world war happen?”
2. Processing: The device converted my voice to text, sent it to the OpenAI API, and received a response.
3. Playback: The response was converted to speech and played back in real-time:
– “There have been two major world wars in history: World War I (The Great War) Dates: July 28, 1914 – November 11, 1918…”
The latency was impressively low, and the conversation felt natural and intuitive.
Challenges and Solutions
1. Latency: While the ESP32-S3 is powerful, network latency could occasionally cause delays. To mitigate this, I optimized the API request size and ensured a stable Wi-Fi connection.
2. Audio Quality: Fine-tuning the microphone and speaker settings improved the overall audio input and output quality.
Key Takeaways
This project demonstrated how the SenseCAP Watcher and the OpenAI API can be combined to create an engaging and practical real-time voice assistant. The ESP32-S3’s AI capabilities and Espressif’s seamless OpenAI integration make it an excellent choice for developers looking to build IoT devices with conversational AI.
Future Possibilities
This demo is just the beginning! Here are some ideas for expanding this project:
1. Smart Home Assistant: Control IoT devices in your home with voice commands.
2. Multilingual Support: Use OpenAI’s models to translate between languages in real-time.
3. Edge AI Improvements: Implement more on-device processing for faster responses and reduced dependence on the cloud.
The world of IoT and AI is growing rapidly, and tools like the SenseCAP Watcher and OpenAI API are paving the way for smarter, more interactive devices. If you’re excited about turning your IoT ideas into reality, this is the perfect time to explore!