Beyond Home Automation – LLM on the Edge Makes Your Smart Home Smarter

Imagine what would happen if a large language model and Home Assistant were combined? Yes, we would get a smart home assistant. It’s not just the popular voice chatbot of recent times, but also functions as a smart furniture controller. Here, we’ll discuss how to build your own smart home assistant!

Basic Concepts

Chatbots

Chatbots are automated dialogue systems based on artificial intelligence technology, capable of mimicking human communication methods. They interact with users through text or voice, offering a variety of services such as information retrieval, customer service, and entertainment. These bots can understand and respond to user queries or commands, making the conversation process more natural and efficient.

Home Assistant

Home Assistant is an open-source smart home automation platform. It allows users to connect and control a wide range of smart devices, from lighting and temperature control to security and entertainment systems. It provides highly customizable and automated home management solutions, enhancing the convenience and smartness of home living.

Implementation Process

The diagram above illustrates the hardware and software devices and workflows involved in the entire project. The hardware includes reComputer J4012 and reSpeaker, while the software primarily consists of Riva, Langchain, OpenAI, and Home Assistant.

The main workflow is as follows:

  • After the microphone receives the user’s audio input, the Riva ASR Server converts this input into text format.
  • The Langchain tool calls the OpenAI API to obtain chat content from the large language model.
  • Intelligent furniture control commands are generated based on the chat content and executed using the Home Assistant API.
  • The Riva TTS Server converts the content generated by the large language model into audio signals, which are then output through the speaker.

We have uploaded the relevant code to GitHub. Please refer to the tutorial on GitHub to complete the installation.

Application Example

In the application example, we use the large language model to understand and execute voice commands, controlling the indoor lighting system.

In fact, this project has tremendous potential. It can control not just the lighting, but also all smart devices in the home, thereby creating a more advanced integrated smart home solution. You are just one reComputer away from completing this project.

Summary

By integrating large language models with Home Assistant, we can achieve not only home automation but also a more intelligent, interactive, and personalized home assistant experience. As technology continues to advance, the future of smart homes will become increasingly intelligent and human-centric, bringing greater convenience and enjoyment to our lives.


Seeed: NVIDIA Jetson Ecosystem Partner

Seeed is an Elite partner for edge AI in the NVIDIA Partner Network. Explore more carrier boards, full system devices, customization services, use cases, and developer tools on Seeed’s NVIDIA Jetson ecosystem page.

Join the forefront of AI innovation with us! Harness the power of cutting-edge hardware and technology to revolutionize the deployment of machine learning in the real world across industries. Be a part of our mission to provide developers and enterprises with the best ML solutions available. Check out our successful case study catalog to discover more edge AI possibilities!

Take the first step and send us an email at [email protected] to become a part of this exciting journey! 

Download our latest Jetson Catalog to find one option that suits you well. If you can’t find the off-the-shelf Jetson hardware solution for your needs, please check out our customization services, and submit a new product inquiry to us at [email protected] for evaluation.

About Author

Calendar

2024 年 2 月
 1234
567891011
12131415161718
19202122232425
26272829