Building Robots Made Easy: Introducing Bus Servo Driver Board for Seeed Studio XIAO
Experience the next evolution in servo control with the Bus Servo Driver Board for Seeed Studio XIAO. Unlike traditional PWM that requires one signal line per servo, this compact powerhouse uses efficient bus control to manage multiple servos through a single communication line, offering real-time feedback and precise synchronization. Whether you’re building robotic arms or multi-legged robots, transform your projects with advanced features like torque monitoring, programmable acceleration, and simplified wiring architecture.

There is an issue with this board and the wiki: it’s write” For UART: Jumper Setting (Critical): Locate the solder jumper near the UART pins. For direct UART communication, you must ensure that the two pads are connected (soldered together).” And For USB Connection it’s write “Step1: Locate the soldering jumper on the back of the board. For USB communication, you must ensure that the two pads are connected (there is a solder bridge between them). So exactly same config…aka solder blob between pad… And in the FAQ: “What happens if I set the jumper incorrectly?
The board won’t communicate properly. For direct UART communication, ensure the two pads are connected (soldered together), and for USB communication, ensure the two pads are disconnected (no solder bridge between them). You must solder/desolder the jumper pads to match the selected mode.” so again anothzer instruction. I spend more than 300 dollar to order the SO-ARM100 Low-Cost AI Arm Servo Motor Kit Pro and despite multiple email I still have no working Servo bus driver board. This piece doesn’t work for USB direct connction. MAx voltage is 12V and power in the PRO kit give 12.26v ! not serious. Don’t buy this board it doesn’t work.
Hi Prigent, I sincerely apologize for the delayed response to your concerns. First, given the timing of your comment, I wanted to check if you have already resolved this issue with our technical support team?
Let me clarify the confusion: Based on your feedback, you purchased the SO-ARM100 Pro Kit, which includes a Bus Servo Driver Board. The board in the SO-ARM100 Pro Kit comes pre-configured in USB connection mode by default – you can refer to this Kit’s dedicated wiki (https://wiki.seeedstudio.com/lerobot_so100m/) and use it directly without any additional configuration.
The wiki content you referenced is actually for the standard Bus Servo Driver Board for XIAO, which is a different version with UART connection mode by default. However, you raised a valid point about the inconsistencies in that wiki page. Our Application Engineering team has reviewed and confirmed these documentation errors. We are already working on correcting these inconsistencies. Thank you for bringing this to our attention.
Please let me know if you still need any assistance with your SO-ARM100 Pro Kit. We’re here to help ensure you get the best experience with our products.