Build the Robots of Tomorrow with NVIDIA Jetson Thor
NVIDIA has unveiled the NVIDIA® Jetson Thor™ series, a groundbreaking platform for physical AI and
NVIDIA has unveiled the NVIDIA® Jetson Thor™ series, a groundbreaking platform for physical AI and
Explore how to pick the right Home Assistant Display among esphome epaper display, and home assistant touch screen. You can also expect to learn how to build a beautiful, functional lovelace dashboards for your smart home setup.
Explore how to pick the right Home Assistant Display among esphome epaper display, and home assistant touch screen. You can also expect to learn how to build a beautiful, functional lovelace dashboards for your smart home setup.
On 2nd August 2025, Mar Athanasius College of Engineering (Autonomous), Kothamangalam transformed into a vibrant
The first edition of the Interactive Signage Contest was a huge success! This year, we
From AI-powered smart glasses and health-monitoring rings to gesture-controlled gloves and LED fashion accessories, Seeed Studio XIAO is powering the next generation of wearable technology. This blog showcases a diverse collection of community projects and reference designs where XIAO delivers compact size, low power, and versatile connectivity to bring innovative, real-time wearables to life.
Home Assistant Connect ZWA-2 is now available at Seeed Studio! This powerful device serves as your gateway to building a robust Z-Wave network through Home Assistant’s Z-Wave Integration.
Hey community, Welcome to our June and July 2025 newsletter! From a series of groundbreaking
We’re thrilled to announce the launch of the XIAO Showdown, an exciting developer competition that
In a world where wearables often prioritize form over function, TPGmini v2 is redefining what
At Seeed, we’re diving into the exciting world of voice AI with our Microphone Arrays
日本の広大で高度に専門化された電気機器産業において、安全は最優先事項です。毎日、数千件の設置作業が実施され、変圧器からリレーコイルまで、工場、建物、インフラストラクチャーにわたる電力の安定した供給が確保されています。しかし、これらの設置作業において最も基本的で重要な作業の一つが、しばしば見落とされています:正しい配線極性です。 数十年にわたり、パナソニック(旧ナショナル)が製造した独自のアナログブザー装置は、日本の電気分野で静かに定番品となっていた。誤配線検出を目的としたものではなかったが、3Vの開放電圧と20mAの短絡電流、そしてアナログ発振回路の組み合わせにより、変圧器やリレーコイルのインピーダンス差を検知することが可能となった。電池駆動でシンプル、かつ精密機器にも安全なこの装置は、全国の技術者や電気技師にとって欠かせない存在となった。 しかし2010年代に入り、パナソニックはこの装置の製造を中止したため、市場には適切な代替品が存在しなくなった。新型のデジタルテスターは中核となる検出能力を欠いていた。抵抗値のしきい値は測定できたものの、複雑な電気部品における誘導性の誤配線を検出することはできなかった。明らかだった:このレガシーデバイスは生まれ変わる必要があった——21世紀にふさわしい改良を加えて。 専門知識を駆使したゼロからのハイブリッド再設計 そのギャップを埋めるため、日本のエンジニアチームはベテランの回路設計者である下間憲行氏(通称「居酒屋ガレージ」)と協力しました。下間氏は、日本において回路設計とプログラミングの専門家として知られ、数十年にわたり『トランジスタ・テクノロジー』誌(https://toragi.cqpub.co.jp/)に技術記事を寄稿し、日本のエンジニアの間で広く読まれています。現代のマイクロコントローラーベースの導通テスターを基盤に、彼らは失われたACベースの検出原理を再導入する作業を進めました。発振回路を統合し、さまざまな周波数をテストすることで、再設計されたデバイスは、現代のアナログメーターや小型リレーコイルのような低インダクタンス部品でも検出可能になりました。 結果:コンパクトでバッテリー駆動のAC/DCハイブリッドテスター。端子短絡時に自動で起動し、現場での使用に安全で、日常の点検に非常に効率的です。 オリジナルのブザーの独自の能力が、AC発振によるインピーダンス検出にあることを認識したチームは、下間氏にACとDCの両モードを組み合わせたハイブリッドデバイスを開発するよう依頼しました。一連の迅速な設計反復を経て、彼は発振回路を追加し、周波数を1kHzから5kHzまで調整しました。これにより、これまで検出できなかった部品の検出が可能になりました。 このデバイスは巧妙に効率化されたスリープモード設計💤を採用し、テスト端子が短絡されると⚡自動的に起動します。さらに180秒のタイマー⏱️を搭載し、スリープ状態へ復帰するため電源スイッチ🔌が不要。スリープ時の消費電流は さらに180秒のタイマー⏱️を搭載し、電源スイッチ🔌が不要なままスリープ状態へ復帰。2本の単三電池で駆動するスリープ電流は1μA未満のため、放置されても数週間持続可能。これにより新型ブザーは、先代機が愛された現場での実用性を確実に継承している。 👉 詳細を見る・注文する 試作から量産へ — Seeed Fusion