E Ink Display vs LCD: Which One is Right for Your Next Project?

The performance, readability, and power efficiency of your product can all be greatly impacted by the display you choose when building your next DIY or IoT device. The argument over E Ink versus LCD (and even E Ink versus OLED) is more pertinent now than it has ever been.

We’ll discuss the differences between E-paper and LCD, their respective functions, and how to choose the best display for your project in this post.

eink vs lcd
reTerminal E1001 & Wio Terminal

What Is an E Ink (E-paper) Display?

E Ink, also known as electronic paper (E-paper), is a display technology that mimics the appearance of ink on paper. Instead of emitting light, it reflects ambient light, making it comfortable to read in all lighting conditions — even direct sunlight. E Ink displays contain millions of microcapsules filled with black and white particles that move under an electric field. Once arranged, the image remains visible without consuming power until it’s refreshed.

reTerminal E1001 Monochrome ePaper Display
reTerminal E1001 Monochrome ePaper Display

Key Features of E Ink Displays:

  • Ultra-Low Power Consumption: Displays hold images without continuous power.
  • Readable in Sunlight: Perfect for outdoor and handheld devices.
  • Paper-Like Appearance: Great for text-heavy applications.
  • Limited Refresh Rate: Not suitable for animation or video.
the principle of epaper
From The Principle and Advantage of E-paper Display on Good Display

E Ink Displays from Seeed:

eink display by Seeed
reTerminal E1002(full color version) & E1001(black and white version)

What Is an LCD Display?

An LCD (Liquid Crystal Display) is a flat-panel display that uses a backlit layer of liquid crystals to create an image. When an electric current is applied, the liquid crystals twist to block or allow light to pass through, with the help of polarizing filters and color filters, to form the colors and shapes you see on the screen. These displays are used in TVs, monitors, smartphones, and calculators because they are thin, lightweight.

1.69 inch LCD SPI Display
1.69 inch LCD Display

Key Features of LCD:

  • High Refresh Rate: Ideal for animations, videos, and dynamic UIs.
  • Bright and Vivid Colors: Excellent for colorful interfaces or outdoor visibility (with backlight).
  • Wide Availability: A vast range of sizes and resolutions available.
  • Low Cost: Suitable for budget-sensitive projects.
From What is LCD? on Electronicsforu

LCD Displays from Seeed:

Grove-LCD RGB Backlight connected to Arduino

E Ink Display vs LCD: Technical Comparison

FeatureE Ink Display (E-paper)LCD Display (Liquid Crystal Display)
Core TechnologyUses electrophoretic microcapsules that rearrange charged pigment particles. The display holds the image even without power.Uses liquid crystals and a backlight to control the passage of light through color filters. Requires continuous power to maintain visibility.
Power ConsumptionExtremely low – only during updates. Perfect for battery- or solar-powered devices.High – needs constant power for backlight and pixel refresh.
Visibility in SunlightExcellent – fully reflective, works perfectly outdoors.Moderate to poor – readability depends on brightness and anti-glare coatings.
Refresh RateSlow (mostly around 1 Hz to 15Hz) – suitable for text, sensors, or dashboards that refresh occasionally.Fast (30–120 Hz) – ideal for data visualization, animation, or touch UI.
Color RangeMonochrome(black/white) or limited color options (3-color or 6-color Spectra variants)Full RGB color with high contrast and saturation.
Display TypeReflective – uses ambient light, similar to paper.Transmissive/Transflective – relies on LED backlighting.
Eye ComfortNon-glare and natural, great for prolonged viewing.Bright and vivid, but can cause more eye strain over time.
Best Use CaseStatic information, IoT dashboards, shelf labels, e-readers, or energy-efficient trackers.Dynamic interfaces, media, and real-time IoT visualization (like Home Assistant panels).

E-paper vs LCD: When to Choose Each Display

Choose E Ink (E-paper) if you’re building:

  • Battery-powered IoT devices
  • Outdoor signage or trackers
  • E-book readers or smart labels
  • Minimalist displays that update infrequently

Choose LCD if you need:

  • Real-time data visualisation
  • Smooth animations or videos
  • Interactive user interfaces
  • Projects with continuous power supply

Projects that utilise e-ink & LCD

· ESticky: a Tiny Paperless Way to Keep Your Thoughts Organized by Gokux

hand holding an e-ink device called ESticky
Project Link: https://www.instructables.com/ESticky-a-Tiny-Paperless-Way-to-Keep-Your-Thoughts/

ESticky offer a fantastic way to keep your notes, reminders, and to-do lists organised—without the mess of traditional sticky notes. Imagine having a reusable, low-power sticky note that updates through Wi-Fi!

This project turns the 2.9-inch e-paper display and the Seeed Studio XIAO ESP32C3 into a sleek, always-visible sticky note that you can easily update using a web app. Whether you’re jotting down daily tasks, sharing motivational quotes, or displaying fun images, this e-paper note keeps your space tidy and your ideas front and centre.

· ESP32-Based Wireless Smartwatch by RoboticWorx

DIY ESP32-Based Wireless Smartwatch
Project Link: https://www.instructables.com/ESP32-Based-Wireless-Smartwatch-LiDAR-Distance-Sen/

This is a “Gateway” smartwatch project! It acts as a compact wireless access key to control all your IoT devices from the comfort of your arm! It also features exchangeable MAC addresses, the ability to scan WiFi networks, has a built-in LiDAR for distance sensing, and provides you with real-time temperature, altitude, humidity, pressure, gas resistance, tilt, and acceleration.

The display being used for this project is a 280×240 resolution 1.69″ 262K RGB LCD driven by an ST7789 via Serial Peripheral Interface or SPI. Perfect for illuminating high-resolution images.

E Ink Display vs OLED: A Quick Comparison

OLED Yellow & Blue Display 0.96
Seeed Studio Grove – OLED Yellow & Blue Display 0.96 (SSD1315)

While OLED displays are known for their vibrant color and flexibility, they consume much more power compared to E Ink. If your project requires a colorful and responsive UI, OLED might be the better choice. However, for ultra-low-power and sunlight-readable applications, E Ink wins.

Final Thoughts

Both e-ink and LCD technologies have distinct advantages. If your project needs clarity under sunlight and ultra-low power, E-Ink is unbeatable. But if you’re building something dynamic or colorful, LCD remains the go-to choice.

Explore Seeed Studio to find the perfect match — whether it’s a low-power ePaper for outdoor devices or a vivid LCD for data-rich dashboards.

Start your next project today — with the right display for your vision.

>> Read more about E ink

About Author

Calendar

November 2025
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930