XIAO Debug Mate: A Plug-and-Play Dev Multi-Tool for $19.9

TL;DR: Community feedback shaped every feature of the Seeed Studio XIAO Debug Mate—an ESP32-S3 powered multi-tool combining DAPLink debugging, serial monitoring, and power profiling with a built-in LCD display. Professional capabilities, hobby-friendly price.

If You've Ever Done This, We Built This For You

Picture this: You’re deep into your embedded project when a mysterious bug appears. No debugger? Time to sprinkle Serial.print() statements everywhere, recompile, reflash, cross your fingers, repeat.

Or maybe you need to monitor UART communication between your XIAO and a sensor. Disconnect the sensor, grab a USB-to-TTL adapter, rewire everything… wait, you need to see both serial streams? Now you need two adapters and a cable management PhD.

And don’t get us started on power consumption mysteries. Your battery drains too fast, but measuring current means either manually recording multimeter readings or dropping $100+ on a professional power profiler.

The result? A workbench drowning in cables, tools you rarely use, and the lingering thought: embedded development shouldn’t be this hard.

We agree. That’s why we built Seeed Studio XIAO Debug Mate.

Three Essential Tools. One Device. Under $20.

Meet Seeed Studio XIAO Debug Mate, our answer to these frustrations. It’s an open-source ESP32-S3 based multi-tool that puts professional capabilities in your hands for under $20.

XIAO Debug Mate

This all-in-one device features a standalone 2.01 inch TFT LCD display, LED status matrix, and native Seeed Studio XIAO support. It combines three essential functions that previously required separate tools: DAPLink chip-level debugging, built-in serial monitoring with UART passthrough, and accurate power consumption measurement. Plug-and-play design eliminates complex wiring for streamlined development.

While purpose-built for the XIAO ecosystem with direct plug-and-play support for any pre-soldered XIAO board, the Debug Mate’s open-source design extends compatibility to most of popular embedded systems via standard SWD (for DAPLink debugging any ARM Cortex-M microcontroller) and UART (for serial monitoring) interfaces. It’s optimized for XIAO but not limited to it.

How This Came to Be: Community-Driven Development

This project started with a simple GitHub discussion. In July 2024, community member @rei-vilo opened Discussion #20 in our repository with an observation that resonated with many developers: “A programmer-debugger probe is a very useful and ‘must have’ tool for embedded system development. Today, there is no affordable offer.”

The conversation highlighted a real problem. The J-Link Edu Mini had jumped from $20 to $70, putting professional debugging tools out of reach for many hobbyists and students. The Raspberry Pi Debug Probe offered great value but didn’t integrate seamlessly with the XIAO ecosystem. Existing XIAO expansion boards relied on fragile pogo pins and only worked with certain boards.

We listened, and we acted. Over the following months, we shared preliminary designs and collected feedback from the community. Together, we decided on OpenOCD support, refined the form factor, and added features like the power profiler and standalone display that went beyond basic debugging. The software development proved more challenging than expected, but the community’s enthusiasm kept us motivated through multiple revisions. 

XIAO Debug Mate V0.1
XIAO Debug Mate V0.1
XIAO Debug Mate V0.1

XIAO Debug Mate V0.1 (we used to called it Debugger for XIAO)

This is the XIAO Open Roadmap in action. It’s our community-driven product development initiative where users don’t just provide feedback—they actively shape what we build. In July 2025, we shipped out 20 early samples of XIAO Debug Mate V0.1 to 20 XIAO users for alpha testing. Based on all the feedback that we collected, our team made an upgrade on the hardware and software, which shaped the final look of the gadget we released today. Debug Mate exists because you told us what you needed, and we built it together.

Our mission has always been to make technology accessible for more people. Seeed Studio XIAO Debug Mate embodies this philosophy by being not just a debugger, but also a serial monitor and energy profiler. It’s not just a tool that requires a PC all the time—it has standalone visualization (for serial monitoring and power profiling) built right in. It’s not just for experts—the plug-and-play design welcomes beginners. And most importantly, it’s not expensive—professional features come at a price anyone can afford.

Thank you to everyone who contributed ideas and feedback throughout this journey. A special big shout-out to rei-vilo, Chris, PJ, Hendra, Ernesto, Benjamin, Pete, NitekryDPaul for insightful feedback during v0.1 testing.

Order Now & Join XIAO Open Roadmap

Seeed Studio XIAO Debug Mate is now available for order at $19.9 via our official store Bazaar and AliExpress Store (listing approval in progress, which should be available soon) with shipment from our CN warehouse (the stock for our EU and US warehouses will be available in late December or early January). Ready to simplify your embedded workflow? Grab your XIAO Debug Mate while the first batch of stock lasts!

Beyond just buying the product, we’d also love to invite you to join the XIAO Open Roadmap and help shape what we build next. The XIAO ecosystem thrives because of community input like the discussion that led to XIAO Debug Mate. Share your ideas in our GitHub Discussions, vote on proposed features, contribute to open-source designs, or simply help us spread the word. Every XIAO product is better because of feedback from developers like you. Whether you’re a hobbyist building your first IoT device or a professional prototyping the next big thing, your voice matters.

Notes at the end.

Hey community, we’re curating a monthly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with:

🤖️ Cool Projects from the Community to get inspiration and tutorials
📰 Product Updates: firmware update, new product spoiler
📖 Wiki Updates: new wikis + wiki contribution
📣 News: events, contests, and other community stuff

Please click the image below👇 to subscribe now!

About Author

Calendar

November 2025
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930