Home Assistant Soil Moisture Sensor Recommendation and Build Guide in 2026

home assistant soil moisture sensor

Looking for a plant soil moisture sensor that integrates well with Home Assistant?

Then you’ll definitely want to check out the XIAO Soil Moisture Sensor—a compact, low-power soil moisture monitor powered by the XIAO ESP32-C6. It seamlessly integrates with Home Assistant, keeping you connected to your soil’s condition in real time.

Below, I’ll explain in detail why this sensor is a solid option. After that, we’ll guide you through setting it up with Home Assistant to monitor your plant’s soil moisture and even automate watering when the soil becomes dry.

Why You Should Choose the XIAO Soil Moisture Sensor?

✅ Native ESPHome & Home Assistant Integration

The XIAO Soil Moisture Sensor features pre-flashed ESPHome firmware with auto-detection, giving you seamless Home Assistant integration right out of the box.

But it’s also fully compatible with YAML and the Arduino IDE, unlocking limitless possibilities for custom firmware and advanced automation control.

Comprehensive Three Level Soil Moisture Monitoring and Alert System

✅ Designed for Real Plant Growing Conditions

  • Uses capacitive sensing with a resin-coated probe and splash-resistant housing for accurate, corrosion-resistant performance in real garden conditions.
  • Built-in LED and multifunction button allow quick status checks and manual resets.
  • Pre-calibrated and supports custom soil calibration for different environments.
  • Powered by a single AA battery for a simple, wire-free setup.

✅ Cost-Effective

Buy directly from the Seeed Studio official store for only $9.90.

⚠️ Limitation

It is a great Home Assistant indoor plant moisture sensor. However, since the 3D printed enclosure is not waterproof, it is usually not recommended for outdoor use.

It protects against side splashes so that you can use it indoors with complete confidence.

How to Build a Soil Moisture Monitor and Irrigation System with Home Assistant

Seeed has created a hands‑on tutorial for the XIAO Soil Moisture Sensor. It walks you through a quick start and also shows advanced options like tweaking the firmware logic and flashing your own customized version straight from Home Assistant. For the full details, check out the Wiki guide.

Besides, Seeed engineer Mengdu used the XIAO Soil Moisture Sensor to build both a plant soil moisture monitor and an automated irrigation system, complete with detailed step‑by‑step instructions you can follow.

Plant Soil Moisture Monitor System

This project creates a fully wireless, solder‑free smart plant monitor, making it easy to check your plant’s soil condition at a glance via a desktop e‑paper display.

The hardware setup utilizes two integrated ESP32‑based devices:

  • XIAO Soil Moisture Sensor: Staked directly into the plant pot, it measures moisture levels and transmits the data over Wi‑Fi.

  • XIAO 7.5‑inch e‑Paper Display: Placed on your desk, this serves as a compact command center. It pulls the plant’s status, local weather forecasts, and your daily calendar directly from Home Assistant, presenting them in a clean, distraction-free interface.

It takes a minimalist approach to create a highly practical assistant that supports both plant care and your everyday schedule. For the full build process and configuration details, check out the complete guide on Hackster.

Plant Soil Moisture Monitor and Automated Irrigation System

After building the monitoring system, Mengdu realized that while he knew when the plant needed water, the actual watering was still manual. To “close the loop” on smart home automation, he took things a step further and built a fully automated watering system.

Building on the previous setup, he added the “muscle”: a dedicated actuator module built from a XIAO ESP32-C3, a Grove Relay, and a small water pump to listen for the “water” command and execute it precisely. The sensor detects the dry soil, Home Assistant makes the logical decision, and the actuator takes immediate action.

For a step‑by‑step breakdown of this automated build, head over to the full guide on Hackster.

By integrating the XIAO Soil Moisture Sensor into Home Assistant, you can easily set up precise, visual monitoring, even fully automated watering that you’ll never have to water your plants by hand again. 👉 Try it now!

About Author

Leave a Reply

Your email address will not be published. Required fields are marked *

Calendar

March 2026
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031