Seeeduino MEGA

The Seeeduino Mega is as small as the seeeduino which is about 2/3 of the Arduino Mega. Not only smaller but also it breakout 19 more pins than the Arduino Mega. The seeeduino Mega is also compatible to each Arduino or seeeduino shield.

 

Now the debug job is nearly finished. And the seeeduino Mega is coming soon.

About Author

3 thoughts on “Seeeduino MEGA

  1. >> This does not seem like it will accept existing shields

    Why not? Looks perfectly fine.

  2. This does not seem like it will accept existing shields. will they fit on this board? or is this not the final shape?

  3. Any plans to develop a breadboard compatible version? All of those pin headers in such a small space might make it a bit difficult to break out!

    Love the idea, hope it works well in practice…

Comments are closed.

Calendar

June 2009
M T W T F S S
1234567
891011121314
15161718192021
22232425262728
2930