Forum

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

MonthlyWrap-up November: 8 Project Tutorials, 6 Breaking News, 2 Giveaway, 2 Sponsorships, and More

For this post, we’ll cover 6 breaking news that you might want to know about, 8 awesome projects from the community, 2 stories on how to deploy IIoT Solution to solve real-world issues, 6 technical write-ups, 2 successful manufacturing case, and 2 prototyping sponsorships and 2 giveaways. Some hottest topics like XIAO BLE, RP2040, OTA, embedded Machine Learning will be covered too.

FarmBeats: Microsoft and Seeed’s AIoT Solution for Precision Agriculture and Technology Democratization for Local Farmers

In 2019, by partnering with Seeed Studio, Microsoft developed an AIoT solution for local farmers – “FarmBeats” Project. The Project has been designed to deliver Internet connectivity and to make precision farming to local farmers at affordable costs. More specifically, Seeed’s Sensor Box was developed and used for the Project to monitor various environmental conditions that affect the crop growth. As a result, agricultural productivity rate has been increased, while overall maintenance costs and human labor inputs have been minimized. FarmBeats Project has been recognized to help accelerate the UN’s SDGs 2, 9, 12, 5, 6, 7, 8, 4, 13, 17, 1 and 10.

Calendar

December 2025
M T W T F S S
1234567
891011121314
15161718192021
22232425262728
293031