DSO Quad engineering samples ready to dispatch!

Scheduled delivery:

Dec. 24th Engineering samples shipping

Jan.1st – Pioneering batch pre-order start

Jan. 20th –Pioneering batch shipping

Feb – mass production

Retail price and detailed features coming up…

Click here for more pictures of DSO Quad

Engineering Samples

We would like to send engineering samples to the community first. Allow us to thank our most active community member, DSO series can’t move forward without your insights and all the help!

–       Thanks to BenF’s super cool DSO nano firmware, which is now v3.4!

The latest one is the version 3.4 in http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1399.

You could also find the former firmware from http://www.seeedstudio.com/forum/viewforum.php?f=12

v3.3 in http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1379

v3.2 in http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1358

The new features in his firmware are listed in Revisions.txt file of the zip package.

–       Thanks to tormod and Antonio for the help migrate the project to GCC.

More details are in http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1350

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1262.

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1349.

–       Thanks to dnordenberg, Shazam, Slimfish and traugott.guenther for actively suggestions in helping us made DSO nano better!

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1406&p=4871#p4871

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1405&p=4869#p4869

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1350

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=1301.

http://www.seeedstudio.com/forum/viewtopic.php?f=12&t=676

–      Thanks to Justblair in early sharing his review of DSO Nano!

http://www.justblair.co.uk/seeed-studio-dso-nano-pocket-digital-storage-oscilloscope-review.html

Please take our sincere gratitude for the efforts and wits you guys shared with the community!

Merry Christmas and happy new year to everybody watching DSO Quad and Seeed Studio! 🙂

About Author

10 thoughts on “DSO Quad engineering samples ready to dispatch!

  1. I received the DSO Quad about one week ago but this did not include any operators manual or indtructions for installation of the battery. How can receive a manual?

  2. Have you noticed that some chinese vendors on the bay have announced a new DSO nano which is nearly identical to the quad? Are they copying your design or it is being licensed from you?

  3. Looks amazing, I’ve held out on buying a nano to wait for this baby. Just wondering, have you enlisted BenF to help write the firmware? Seems like it’s still squeezing more use out of the nano and it would be great to see that sort of skill applied to the Quad!

    I’ll put aside my pennies 😀

  4. Thanks for the mention! Just like to say that my Nano has been since I got it one of the most used tools in my box.

    I have a full 100mhz analogue scope which is now looking pretty sad.. Yes its more powerful than the Nano, but 90% of what I need a scope for is to check for signs of life. In most circuits the Nano will tell you if all is well or if the signal is mangled.

    The Quad looks like a welcome advance on an already amazing product.

  5. It’s looking fantastic! Glad to see the guys developing the v1 firmware getting some xmas presents! I can’t wait to get my hands on one… Now, tell us the price!

Comments are closed.

Calendar

December 2010
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031