MeshCore is an off-grid communication platform built on LoRa technology, designed for multi-hop text messaging in areas without internet or cellular coverage, similar to Meshtastic.
However, you might find yourself in areas with limited or no MeshCore coverage. It’s so important for more people to get involved and help grow the MeshCore network by setting up repeaters.
One comment from the community really stuck with me
A network always starts with that one person who takes the time to build a small infrastructure then gets a few buddies to test, then it starts to grow. If everyone waits for the next person to do it it will never be built.
Hope the hardware and build guide below makes it easy for you to dive in and start growing MeshCore in your area.
Recommended Hardware for MeshCore-Compatible Repeater
The SenseCAP Solar Node P1-Pro is a great device to consider as a MeshCore repeater. It is a solar-powered LoRa communication node specifically designed for areas without network coverage. With a built-in battery, it supports long-distance communication, precise positioning, and low-power operation, making it well-suited for expanding network coverage in outdoor environments.

Why You Should Choose the SenseCAP Solar Node P1-Pro as MeshCore Repeater
- Fully compatible with MeshCore
You can find firmware that supports the SenseCAP Solar Node on the official MeshCore website, as shown in the image below.

You might notice on the Seeed Studio product page that this device supports Meshtastic and wonder if it can also run MeshCore firmware. The answer is yes, it’s fully supported. As a LoRa communication node, the SenseCAP Solar Node P1-Pro is compatible with both Meshtastic and MeshCore.
- Many members of the MeshCore community have successfully deployed it in the field
The Ham Radio Tube video features the SenseCAP Solar Node P1‑Pro deployed as a MeshCore repeater, highlighting its robust power system and seamless configuration.

image source: the Ham Radio Tube
- Deployment is very simple
The SenseCAP Solar Node P1-Pro comes ready to use right out of the box. It includes the battery, antenna, and all necessary mounting accessories. All you need to do is flash the firmware, configure the device, and mount it on a pole.

- Consistent self-powered operation in all weather conditions
Equipped with a 5W solar panel and four 18650 batteries (each with a capacity of 3350 mAh), this power setup enables stable, continuous operation even in low-sunlight conditions, making it a reliable solution for outdoor deployments where a consistent power supply can be a challenge.
The Limitations
- No pre-Installed MeshCore firmware
The device comes with Meshtastic firmware by default, however, flashing MeshCore takes just a few simple steps. A pre-installed MeshCore firmware version is on the way, stay tuned!
- Sharp metal bracket edges
The metal bracket has sharp edges, which can pose a risk during installation. Be sure to wear gloves to protect your hands and avoid injury.
Buying Guide
It’s recommended to purchase directly from the official Seeed website https://www.seeedstudio.com/SenseCAP-Solar-Node-P1-Pro-for-Meshtastic-LoRa-p-6412.html (Get 5% OFF with code LWQZJ9Y5 — limited time only!)and select the warehouse closest to your location, which will help ensure faster delivery and may also reduce or eliminate import duties.
Overseas stock may vary due to high demand. If your preferred item is only available in the China warehouse, “US Direct Group Shipping” is the best option for duty-free delivery to the U.S.
If you don’t need positioning and already have batteries, it’s recommended to choose the more affordable SenseCAP Solar Node P1, about $20 less than the P1-Pro.
By the way, you can also get the T1000-E from Seeed Studio to use as a MeshCore node. This credit card-sized device is waterproof, features a built-in long-life battery, and comes with a high-performance LoRa antenna. It pairs perfectly with the MeshCore app on Android and iOS via Bluetooth.
How to Set Up a MeshCore Repeater
To support the growing MeshCore community, the Seeed Studio technical team has created a comprehensive guide for setting up the SenseCAP Solar as a MeshCore repeater. Check out the complete step-by-step guide here: https://wiki.seeedstudio.com/get_started_with_meshcore_solar_node/
Watch Ham Radio Tube’s video for a complete walkthrough from firmware flashing to outdoor deployment.
It’s crucial for more people to join in and set up MeshCore repeaters. With every new participant, the network becomes stronger and more reliable.
Build it, and the community will follow!
About Author
Liyan Gong
10 years in the IoT hardware industry. I’m here to share practical guides on Home Assistant, NVIDIA Jetson, Meshtastic/Meshcore, Raspberry Pi, LoRa, PCB/PCB Assembly and more to help bring your creative ideas to life.
Hi, thanks for the guide. I’d like to suggest one practical improvement based on field use. The mounting bracket could be shorter and more robust, because with a higher-performance antenna I noticed that the pole mount flexes quite a lot in the wind. A stiffer bracket would make the installation feel more secure and stable over time. I also replaced the stock antenna cable with a thicker, lower-loss coax cable, and it seems to reduce signal loss noticeably. This could be worth mentioning in the guide for users planning a more performance-oriented deployment
Hi Mario, thanks for the real-world insights! I’ve forwarded your suggestions about the shorter and more robust mount and the cable straight to our product team to keep in mind for future updates, and your comment there will also definitely help other Meshcore community member!
Is there any timeframe for those changes to be applied by chance? I am looking to order a P1-Pro and would rather wait for the updated revision before ordering
Hi Jake, thanks for checking in. The updated 3mm bracket should be in stock by mid-to-late April.
A quick update: we plan to upgrade the bracket thickness from 2mm to 3mm. Really appreciate your feedback!
Hi there, I’m just setting up a Meshcore network in my area. I have a repeater on top of my house but our village is in a bit of a bowl in the Black Forest highlands of Southern Germany. I’m looking to put up another repeater on the hills surrounding our village so I can get my network connected to the rest of the world. When I am up on the hills, I have my tiny T-1000E with me and I am amazed at how good it is at picking up and transmitting messages. I was wondering if you can do a solar repeater about the size of a small mobile phone which can be discreetly hidden in a tree or something tall without being easily found?
Great products from you guys, many thanks
Hi James,
So glad to hear the T‑1000E is working great for you!
We really appreciate your suggestion for a mini, discreet solar repeater, your suggestion has been noted by our product team for further evaluation. We’ll be collecting all customer feedback for a full review, and there will be more new form factor designs coming in the future, stay tuned 🙂