BeagleBadge: A High-Performance Edge HMI Platform for Specialized Industrial Solutions

Unveil the BeagleBadge: A high-performance Mobile HMI and IIoT platform powered by the Texas Instruments AM62L32. Designed for professionals tackling complex industrial challenges, it provides a production-ready foundation to validate sophisticated human-machine interaction and edge sensing in the real world. Manufactured by Seeed Studio.

In the world of wearable development, there’s an unspoken rule: “Go small or go home.” To fit onto a wrist or a lanyard, developers are usually forced to deal with cramped interfaces, wimpy processors, and the constant headache of thermal throttling.

But BeagleBoard® has never been one to follow the herd.

Live from Embedded World 2026, we are proud to unveil the BeagleBadge. It’s a full-throttle, Linux-powered powerhouse that just happens to be wearable. Whether you are a “badgelife” enthusiast looking for the ultimate hackable flagship, or a professional innovator in vertical Industrial IoT sectors seeking a robust platform to fast-track your next solution, BeagleBadge is your new mission control.

The Power Couple: Seeed Studio x BeagleBoard.org

Following the massive success of the BeagleBone Green®, Seeed Studio is thrilled to team up with BeagleBoard® once again.

As the official manufacturing partner, Seeed has poured its expertise in agile manufacturing and industrial-grade supply chain management into this project. For the community, this means a high-quality, reliable device. For professionals tackling complex field-service or industrial challenges and engineers building specialized IIoT solutions, it provides a production-ready foundation to validate sophisticated IoT use cases in the real world. We provide the heavy-lifting manufacturing support so you can focus on scaling your vision from a prototype to a full-scale deployment.

Under the Hood: The TI AM62L32 "Crossover" Power

The heart of the BeagleBadge is the Texas Instruments AM62L32—a dual-core Arm® Cortex®-A53 SoC. Usually found in industrial controllers or automotive dashboards, BeagleBoard has successfully “crossed over” this industrial beast into a portable form factor.

With 2Gb LPDDR4 RAM and 4GB eMMC storage, it doesn’t just “run” Linux—it cruises through it. This makes it the ideal platform to evaluate the TI AM62L’s performance for real-world applications like mobile HMI, edge AI, and data aggregation.

Sense Everything, Connect Everywhere

This isn’t just a “big screen” on a lanyard; it’s a mobile sensor lab.

  • Total Awareness: Integrated 6-axis accel/gyro, and ambient light.
  • Next-Gen Connectivity: Equipped with WiFi 6 and BT 5.2, plus support for Meshtastic—the gold standard for off-grid, encrypted messaging when you’re out in the wild without a cell signal.
  • Infinite Expandability: Staying true to the BB DNA, it features QWIIC, Grove, and mikroBUS headers. You can plug in hundreds of sensors instantly—turn it into an air quality monitor, a mobile medical vitals tracker, or a personal translator in seconds.

Dual-Path HMI: E-Ink Efficiency & MIPI Performance

BeagleBadge offers a versatile canvas for developing sophisticated Human-Machine Interfaces. Out of the box, BeagleBadge supports a 4.2” ePaper display for that ultra-low-power, “always-on” look. But if you’re craving something more vibrant for your UI, it also features a MIPI DSI interface, allowing you to hook up high-performance LCD screens. This dual-path display capability enables the validation of diverse HMI strategies—from simple status indicators to complex, high-resolution touch interfaces.

Ready to Build the Future of IIoT?

The hardware is ready; now we need your brainpower.

To celebrate the launch, we are officially throwing our support behind the Badge Hackathon 2026. This is the ultimate playground for “badgelife” enthusiasts and developers alike. Whether you want to design a stunning UI using LVGL, build a complex sensor-mesh network, or create the next great off-grid communication tool, this is your stage. 👉 Check out the for all the details!

Ready to Build the Future of IIoT?

The BeagleBadge is proof that the limits of hardware are defined by your imagination, not the size of your PCB. It’s the perfect blend of BeagleBoard’s innovation, Texas Instruments’ silicon power, and Seeed Studio’s manufacturing muscle.

Join the Revolution Today:

  1. Grab your BeagleBadge: Offer from Seeed Studio and be the first to start hacking.
  2. Access the Documentation: Deep dive into the open-source files at BeagleBone official website.
  3. Join the Community: Share your builds with us on social media using #BeagleBadge and #SeeedStudio.

Let’s see what you can build!

About Author

Calendar

March 2026
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031