Introducing reGoggles: Building Open Smart Goggles Together

reGoggles is an open smart goggles platform designed for industrial AI assistance, with a focus on real-world applications, extensibility, and developer flexibility.

While the core functionality is now in place, reGoggles is still under active development. We are working toward our first test units, which are expected to be available in early 2027.

We believe the most useful industrial AI wearable should be shaped by the people who will actually use it: developers, engineers, industrial teams, and technology partners. Through our upcoming Early Builder Program, we want to bring these communities into the development process early, gather real-world application requirements, explore potential use cases, and collect feedback through hands-on testing.

This article introduces what reGoggles is, where its development stands today, what comes next, and how you can get involved in shaping what it will eventually become.

What is reGoggles?

The core idea behind reGoggles is simple: let AI see what the worker actually sees. It is an AI interface built for frontline technicians and workers — worn on the job, not carried.

2.7 billion deskless workers — roughly 80% of the global workforce — still work without an AI interface built for them. That is the gap Seeed is building reGoggles to close.

Conventional industrial vision systems rely on fixed cameras observing the production environment from the outside. Much of the critical information is not in a fixed camera’s field of view — it exists at the point of operation.

reGoggles captures, records, and streams the scene in real time from a first-person perspective, and delivers the data to edge AI, cloud AI, or remote experts for analysis — enabling early warning, real-time recording, and post-event optimization.

ItemSpecification
Main PlatformAllwinner V881 + Wuqi-Micro WQ7036AX
Main Camera12MP RGB camera
IMUMain IMU 6DOF
Audio3 microphones + 2 speakers
StorageOnboard eMMC
Wireless ConnectivityWi-Fi 6 + BLE 5.4
Wired InterfacesUSB Type-C
Expansion PortsGeneral expansion port: MIPI CSI B for Additional Camera, ToF, SD Card and Custom Modules;Vision expansion port: MIPI CSI B for Additional Camera+IMU and Custom Modules.
Video & ImagingSupports 1080p video streaming and 4K still capture
PowerNeck-worn power supply (under development; users can also connect their own power devices)
Physical Buttons3 buttons on one side — 1 power/wake + 2 function keys (shutter/mode, volume); key mapping software-configurable.

The full feature list and specifications are on our landing page: www.seeedstudio.com/regoggles.

reGoggles is still in Active Development

Above is a row of 3D-printed shells from different iterations of the enclosure. We worked through many versions — structure, port layout, how it sits on the head — before it took the shape it has today.

Behind those shells sits most of the work: the chip architecture, hardware-level synchronization across the multimodal streams, a working audio/video streaming path, the expansion interfaces, the detachable lens design, and more.

reGoggles is a working device, not a concept: first-person visual capture, multimodal recording, and data transmission all run end to end. Our engineering team is still polishing the final details — appearance, specifications, and parts of the feature set. The device is not finished yet, and it will keep changing as Early Builder Program participants bring in real-world scenarios. Final details are subject to change until the official release.

Introducing Early Builder Program

We want reGoggles to stay close to the fast-evolving realities of real-world production and AI applications. The product is not perfect yet, but we would rather put it out there and co-create it with you.

At the end of November, we will officially open applications for the Early Builder Program. We invite you to bring your own work context, share your feature requirements and use-case ideas for reGoggles.

Join the community, and become:

  • Community Builders: submit your project proposal, build something with reGoggles, and explore the edges of its applications with us.
  • Beta Testers: get early samples first, use and stress-test them hard in real scenarios, and tell us what breaks.
  • KOL Reviewers: publish reviews and teardowns for your audience.

Join Now

  • Join our Discord community and connect with developers worldwide: https://discord.gg/jb5qdrnAVU
  • Subscribe to email updates on the landing page to be the first to receive development news and Early Builder application notices: www.seeedstudio.com/regoggles
  • Industrial customers or potential partners can reach us directly at: https://www.seeedstudio.com/contacts, or fill out our enterprise application form: https://docs.google.com/forms/d/e/1FAIpQLSdeWjPPHA_orgoDbsES4A_fsP4bHeOsbbtGSKGhObkvSF_pjg/viewform?usp=header

Early Feedback and Our Answers

When will it launch?

We are targeting an official launch in Q1 2027.

Is it open source, and to what extent?

The firmware running on the main chip is fully open source. The secondary chip handles audio and Bluetooth connectivity, and its firmware is not open source, but we do provide open interfaces so you can integrate it with your own applications.

What about battery life, and how is it charged?

The power design supports external power input and hot-swapping, so you can use your own charging equipment to extend capture sessions. We are also developing a neck-worn power pack for greater convenience.

Does the SDK support audio and video streaming to a phone over Wi-Fi or BLE?

The SDK supports audio and video streaming. When streaming over Wi-Fi, due to power consumption and heat generation, we recommend limiting the streaming duration and resolution.

Does it support AR?

Not in the current version. Later versions may add a display function. Whether AR will be supported is still under evaluation.

What is the main chip?

We use a dual-chip architecture: Allwinner V881 as the main chip and Wuqi-Micro WQ7036AX as the secondary chip.

Can I wear my own prescription glasses and put reGoggles on the outside?

Yes. The current structure fully supports wearing your prescription glasses underneath reGoggles.

We believe the next breakthrough in industrial AI will come from devices frontline workers can truly see through and use. reGoggles is still on its way, and we invite every interested developer, engineer, and industry partner to join us in making it a genuinely useful product.

We look forward to seeing you in the community!

About Author

Leave a Reply

Your email address will not be published. Required fields are marked *

Calendar

November 2026
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
30