Using Seeed Jetson Mate as a 4 x Jetson Xavier NX cluster for machine vision laboratory
It was incredible and so exciting to me that I have the opportunity to learn
It was incredible and so exciting to me that I have the opportunity to learn
In an effort to assist decentralization of digital education for rural children in India, Seeed donated open hardware products to Janwaar village, where the children and youth were inspired to learn coding and programming for the first time in their lives. Through embracing the learning principle of hands-on, DIY, and collaborative learning, they were self-empowered to have the ownership of technological tools, and to tackle gender inequality and casteism at village level. On this backdrop, this “Janwaar Maker Space in the Making” Project directly or indirectly accelerates the UN’s SDGs 4, 5, 10, 11, 9, 1, 17, 8 and 16.
And now, please meet the new “Seeed Studio Product Catalog 2023”: a comprehensive digital catalog for you to accurately discover, locate and explore the whole galaxy of Seeed products and services by far.
Did you know that fossil fuel air pollution is responsible for 1 in 5 deaths
Seeed Joins CAEPI as an association member to explore more collaborations with the network to apply IIoT solutions to environmental protection scenarios.
In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.
For this post, we’ll cover 6 breaking news that you might want to know about, 8 awesome projects from the community, 2 stories on how to deploy IIoT Solution to solve real-world issues, 6 technical write-ups, 2 successful manufacturing case, and 2 prototyping sponsorships and 2 giveaways. Some hottest topics like XIAO BLE, RP2040, OTA, embedded Machine Learning will be covered too.
The Challenge Brands need to understand their customers on a deeper level. Therefore, they employ
Hey community, You might also feel the trend that Machine Learning networks are getting smaller.
Breaking news just in! Seeed Studio has just released the highly anticipated addition to the
Hey community, You might notice that we’ve been giving away poster designs lately on our
In 2019, by partnering with Seeed Studio, Microsoft developed an AIoT solution for local farmers – “FarmBeats” Project. The Project has been designed to deliver Internet connectivity and to make precision farming to local farmers at affordable costs. More specifically, Seeed’s Sensor Box was developed and used for the Project to monitor various environmental conditions that affect the crop growth. As a result, agricultural productivity rate has been increased, while overall maintenance costs and human labor inputs have been minimized. FarmBeats Project has been recognized to help accelerate the UN’s SDGs 2, 9, 12, 5, 6, 7, 8, 4, 13, 17, 1 and 10.