ESP-IDF Development Basics

reTerminal Sticky is an e-paper information display designed to keep weather, schedules, notes, and lightweight data visible over long periods. With ESP-IDF, you can use its e-paper display, touchscreen, physical buttons, and onboard peripherals to build your own always-visible information pages.

This guide walks you through running the Comprehensive Development Demo (Sticky_dashboard_demo) and learning how to use ESP-IDF to drive Sticky’s display, onboard peripherals, and interaction features. The example project provides a complete reference for hardware integration and page development, which you can use to create your own pages, integrate onboard peripherals, and build your own projects with Sticky.

Note

Flashing the example project replaces the firmware currently running on Sticky. Make sure the device does not contain anything you need to keep before continuing.

Share Your Project

If you have built a project with reTerminal Sticky, we would love for you to contribute it to Sticky Playground and share your ideas with the community. We appreciate every developer who helps make the Playground better.

Open Playground Registry

Follow the contribution guide in the repository README, prepare your project, and submit a Pull Request. Once your project has been reviewed and published, other users can install and try it through Sticky Playground.

Development Environment

Before you begin, prepare the following:

  • reTerminal Sticky
  • A USB-C cable that supports data transfer
  • A Windows, Linux, or macOS computer
  • ESP-IDF v5.4

Sticky_dashboard_demo was developed and tested on hardware with ESP-IDF v5.4. If ESP-IDF is not installed yet, follow Espressif’s ESP32-S3 ESP-IDF v5.4 Getting Started Guide to install it first.

After installation, run the following command in an ESP-IDF terminal:

idf.py --version

The output should include:

ESP-IDF v5.4
Tip

A charge-only USB-C cable can power Sticky, but the computer cannot detect its serial port through that cable. If the device charges but no serial port appears, try a cable that supports data transfer.

The main Sticky development resources used in the Demo are listed below:

HardwareUse in the Demo
3.97-inch, 800 × 480 four-level grayscale e-paper displayDraw and retain page content over long periods
Capacitive touchscreenDetect left and right swipes
UP, DOWN, and AI buttonsChange pages, refresh, and enter Deep Sleep
SHT40, RTC, battery gauge, and IMUProvide environmental, time, battery, and orientation data
MicroSD and PDM microphoneRead text and capture audio
BuzzerProvide operation feedback

For complete specifications and hardware relationships, read the Hardware Overview first.

Run the Demo

This series includes two example projects:

ProjectNameBest for
Sticky_peripheral_demoMinimal Peripheral DemoClean, standalone examples for testing and reusing individual onboard peripherals
Sticky_dashboard_demoComprehensive DemoA complete example covering pages, peripherals, interaction, and low-power features used throughout this Wiki series

If you are familiar with ESP-IDF and want to work with a specific peripheral, start with Sticky_peripheral_demo. Each example is self-contained and easy to reuse in your own project.

Download Peripheral Demo

To follow this Wiki series step by step, use Sticky_dashboard_demo. All code, project structure, and page examples in the following guides are based on this Demo.

Download Dashboard Demo

Download and extract Sticky_dashboard_demo, then open an ESP-IDF v5.4 terminal in the project directory containing the top-level CMakeLists.txt.

For the first build, set the target chip:

idf.py set-target esp32s3

Build the project:

idf.py build

After you see Project build complete, connect Sticky with a USB-C data cable. Replace PORT with the device serial port, then flash the firmware and open the serial monitor:

idf.py -p PORT flash monitor

For example, if the serial port on Windows is COM5:

idf.py -p COM5 flash monitor

Linux usually uses /dev/ttyUSB0 or /dev/ttyACM0. macOS usually uses /dev/cu.usbserial-* or /dev/cu.usbmodem-*. Press Ctrl+] to exit the serial monitor.

After startup, the serial output includes:

I (...) sticky_dashboard: Starting reTerminal Sticky Dashboard Demo

The Home page appears after the first screen refresh. Use the UP/DOWN buttons or swipe left and right to view the pages in sequence:

Home -> Sensor -> Battery -> Note -> IMU -> Microphone -> Home

Home demonstrates four-level grayscale and does not display RTC time. The other five pages use monochrome images and show RTC time in the status bar.

A full e-paper refresh completes a full pixel update. When it finishes, the new content remains stable on the screen.

Project Structure

Sticky_dashboard_demo separates hardware access, application logic, and page rendering:

Sticky_dashboard_demo/
|-- components/                 External and low-level hardware components
`-- main/
    |-- main.cpp                Initialization and main event loop
    |-- pin_config.h            Pins and device addresses
    |-- board/                  Power, GPIO, and shared buses
    |-- devices/                Onboard peripheral access
    |-- app/                    State, data, events, and page navigation
    |-- pages/                  Page rendering
    `-- ui/                     Canvas, fonts, and shared status bar

When a page displays hardware data, the data follows this path:

Hardware
  ↓
devices        Read the device
  ↓
app_data       Update application data
  ↓
AppState       Store page state
  ↓
pages          Render the page
  ↓
Canvas         Produce the complete image
  ↓
display        Refresh the e-paper display

Each directory has a clear responsibility:

DirectoryResponsibility
board/Initialize board-level power and buses shared by multiple devices
devices/Initialize, read, or control specific hardware
app/Store state, update data, process events, and select pages
pages/Render pages from AppState
ui/Provide Canvas, fonts, and the shared status bar

This structure keeps hardware communication, data processing, and page rendering separate. When adding a feature, you usually only need to connect its data source, extend AppState, and create a page. You do not need to rebuild the existing display, input, or refresh framework.

Page rendering and screen refresh

A page Renderer (the page rendering function) only writes content to Canvas. After rendering, the App layer refreshes the e-paper display:

render_current_page(canvas, state);
ESP_RETURN_ON_ERROR(
    refresh_current_page(state), "app", "refresh current page");

refresh_current_page() selects the refresh method from state.current_page: Home uses a four-level grayscale full refresh, while the other pages use a monochrome full refresh. Page files therefore only draw to Canvas. The existing Device and App flow handles Display initialization and refresh.

Canvas uses 800 × 480 landscape logical coordinates with the origin at the top-left corner. Screen rotation is handled by sticky_display, so pages do not need to transform coordinates again.

Data Flow and Page Display

The Sensor page shows a complete data path: the SHT40 reads temperature and humidity, the application stores the data, and the page displays the result.

SHT40
  ↓
sticky_sht40_read()
  ↓
update_environment()
  ↓
AppState.environment
  ↓
sensor_page_render()
  ↓
Canvas

Read the sensor

main/devices/sticky_sht40.* wraps SHT40 hardware access. During initialization, it uses the sensor I2C bus already created by the Board layer:

ESP_ERROR_CHECK(sticky_sht40_init(board_sensor_i2c_bus()));

The RTC, battery gauge, and IMU also use this shared bus, so a separate I2C bus does not need to be created for each device.

Update application state

EnvironmentState in main/app/app_state.h stores the temperature, humidity, and read status needed by the page:

struct EnvironmentState {
    float temperature_c = 0.0F;
    float humidity_percent = 0.0F;
    bool valid = false;
    esp_err_t error = ESP_ERR_INVALID_STATE;
};

main/app/app_data.cpp calls the Device API and writes the result to AppState. The core relationship is:

Sht40Reading reading = {};
const esp_err_t result = sticky_sht40_read(reading);

state.environment.error = result;
state.environment.valid = result == ESP_OK;

After a successful read, the function also stores the temperature and humidity. If the read fails, valid remains false, while the error code and serial log help identify the problem.

Render sensor data

main/pages/sensor_page.cpp only reads the state. It displays the temperature when the data is valid, or N/A in the same position if the read failed:

canvas.draw_text(76, 235, "Temperature:", 3, GrayLevel::Black);
if (state.environment.valid) {
    std::snprintf(value, sizeof(value), "%.1f C",
                  static_cast<double>(state.environment.temperature_c));
    canvas.draw_text(500, 235, value, 3, GrayLevel::Black);
} else {
    canvas.draw_text(500, 235, "N/A", 3, GrayLevel::Black);
}

When the Sensor page opens, the App layer updates the data, renders the page, and refreshes the screen in sequence. The page does not read the SHT40 directly.

This path applies to most data pages: first identify the data source, then pass the data to the page through AppState. The second Wiki guide uses Battery, MicroSD, IMU, and Microphone to show different types of peripheral data.

Add the Hello Page

The following steps add a Hello page to the end of the existing page loop. It does not access hardware and is only used to complete the full page integration process.

After the change, the page order becomes:

Home -> Sensor -> Battery -> Note -> IMU -> Microphone -> Hello -> Home

Step 1: Create the page files

Create main/pages/hello_page.h:

#pragma once

class Canvas;
struct AppState;

void hello_page_render(Canvas &canvas, const AppState &state);

Create main/pages/hello_page.cpp:

#include "hello_page.h"

#include "app_state.h"
#include "canvas.h"
#include "page.h"

void hello_page_render(Canvas &canvas, const AppState &state)
{
    page_draw_layout(canvas, state, "Hello Sticky", "My First Page");
    canvas.draw_text(76, 250, "ESP-IDF Ready", 3, GrayLevel::Black);
    canvas.draw_line(76, 310, 718, 310, GrayLevel::Black);
}

page_draw_layout() draws the same border, status bar, and title used by the other monochrome pages. The Hello page only needs to add its own content.

The Demo defines only Home as a four-level grayscale page, so the new Hello page automatically uses a monochrome full refresh. Use GrayLevel::Black and GrayLevel::White for a regular new page. If a page needs four-level grayscale, also add its PageId to page_uses_gray4().

Step 2: Add the page ID

Add Hello to the end of PageId in main/app/app_state.h:

enum class PageId {
    Home,
    Sensor,
    Battery,
    Note,
    Imu,
    Microphone,
    Hello,
};

The Hello page has no new data, so AppState does not need to change. If a page displays peripheral data, follow the previous section to add the corresponding state structure and data update function.

Step 3: Register the page

Include the page header in main/app/app.cpp:

#include "hello_page.h"

Add the page name to page_name():

case PageId::Hello:
    return "Hello";

Connect the Renderer in render_current_page():

case PageId::Hello:
    renderer = hello_page_render;
    break;

Step 4: Add the page to navigation

In select_next_page(), navigate from Microphone to Hello, then from Hello back to Home:

case PageId::Microphone:
    state.current_page = PageId::Hello;
    break;
case PageId::Hello:
    state.current_page = PageId::Home;
    break;

Add the reverse relationship in select_previous_page():

case PageId::Home:
    state.current_page = PageId::Hello;
    break;
case PageId::Hello:
    state.current_page = PageId::Microphone;
    break;

Step 5: Add the page to the build system

Add the following entry to the page source list in main/CMakeLists.txt:

"pages/hello_page.cpp"

Save the changes, then build and flash the project again:

idf.py build
idf.py -p PORT flash monitor

When you open the Hello page, the screen should show My First Page and ESP-IDF Ready.

Continue to the next page to return to Home. Switching to the previous page should also follow the complete page sequence.

At this point, you have completed the full page integration process:

Create page files
  ↓
Add PageId
  ↓
Register the Renderer
  ↓
Add page navigation
  ↓
Update CMakeLists.txt
  ↓
Build and verify on the device

Application Extension Workflow

Use the following sequence when creating a new information page:

  1. Identify the data the page needs and check whether the project already provides a corresponding Device API.
  2. If no API is available, add hardware access under devices/. Otherwise, reuse the existing API.
  3. Store the page data, validity state, and error code in AppState.
  4. Read the data and update the state in app_data.
  5. Create a Page Renderer, then add the page to PageId, page routing, and the navigation order.
  6. Add the new .cpp file to main/CMakeLists.txt, build the project, and verify both the display and error states on the device.

Keep these module responsibilities separate when extending the application:

  • Pages only read AppState and draw to Canvas. They do not access hardware directly.
  • Device modules only handle hardware access. They do not draw UI.
  • Shared buses and power resources are managed by the Board layer.
  • After a page is rendered, the App layer refreshes the e-paper display.

FAQ

  1. The new page causes an undefined reference error

    The page .cpp file is missing from main/CMakeLists.txt, or the function declaration does not match its implementation. Confirm that the source file is included in SRCS, then check the function name and parameters before rebuilding.

  2. The new page builds but cannot be opened

    Adding only a PageId or Renderer is not enough. Confirm that the page is registered in render_current_page() and that its PageId is included in both forward and reverse navigation.

  3. Page content has the wrong orientation on the device

    Pages should always use the 800 × 480 logical coordinate system with the origin at the top left. The Display layer handles the 180° rotation required by the physical screen, so do not rotate coordinates again in a Page Renderer.

  4. Page text is displayed as ?

    The built-in bitmap font supports printable ASCII. Unsupported characters, such as Chinese characters and ℃, are displayed as ?. Add the required glyphs or use characters already supported by the font.

  5. The project fails to build after moving to another computer

    The build/ directory contains paths and configuration generated on the original computer. Confirm that ESP-IDF v5.4 and the ESP32-S3 target are selected. If the error remains, delete only the generated build/ directory and rebuild the project.

Next Step

This guide covered two basic development paths:

Page integration: Page files -> PageId -> Renderer -> Page navigation -> CMake

Data display: Device -> app_data -> AppState -> Page -> Canvas -> Display

The next guide continues with the same Demo and explains:

  • Reading Battery, MicroSD, IMU, and Microphone data and displaying it on pages
  • How Button and Touch trigger page changes and refreshes through AppEvent
  • How different peripherals reuse shared resources managed by the Board layer

Continue with ESP-IDF Pages and Peripherals.

Community 社区支持

Need more help? 还需要帮助?

Join our community, ask questions, or reach out to Seeed Studio technical support. 加入社区提问交流,或直接联系 Seeed Studio 技术支持。