Seeed Studio e SDC firmam parceria para expandir Soluções de Edge AI e Computação Industrial no Brasil
Shenzhen, China / São Paulo, Brasil – A Seeed Studio, provedora global de tecnologias de
Shenzhen, China / São Paulo, Brasil – A Seeed Studio, provedora global de tecnologias de
Introducing Seeed Studio XIAO nRF54LM20A (Sense): Nordic nRF54LM20A Board for Matter, Thread & Ultra-Low-Power IoT. It features Bluetooth LE 6.0, Matter, Thread, Zigbee, 28 GPIOs, 2 MB Flash, 512 KB RAM, and optional IMU and microphone for battery-powered IoT, wearables, and edge sensing applications.
ESP32-C6 has become the default choice for many ESPHome and Home Assistant projects—but where does ESP32-C5 fit? This guide compares ESP32-C5 vs ESP32-C6, explores ESPHome compatibility, and shows how XIAO ESP32-C5 can be used to build modern smart home devices.
Choosing the right M12 lens reCamera combination is critical for any AI camera project. Even
A PCB by itself is like an empty city map. The routes are there, but
On June 6, 2026, I was invited by the students of Universitas Raharja to conduct
A standard device can become a branded product with the right customization. In this case,
The reBot Arm B601-RS is now officially launched across the board, with an early bird
NVIDIA JetPack 7.2 is more than a routine software update. While JetPack 6.2 focused on
Hey community, How’s 2026 treating you so far? Welcome to the latest edition of
In many real-world scenarios, connectivity requirements can vary significantly. Whether you’re deploying sensors across remote
Since the first XIAO board landed on desks around the world, the community has done